Release Notes
25C... More information: PowerFlex® 527 Site
Version 1.008 (released 11/2017)
Catalog Number PowerFlex 527
These release notes describe version information for PowerFlex 527, version 1.008 (released 11/2017).
Corrected Anomalies in This Release
This release corrects the following anomalies.
IP Address and Gateway Address anomalies (LGX00163759/LGX00173005)
Corrected:
Known anomaly first identified as of PowerFlex 527 Drives Firmware Revision 1.006
With firmware revision 1.007 or earlier:
- It is possible to enter identical values for the IP address and gateway address by
using the keypad. This is an illegal IP address configuration for the PowerFlex
527 drive because the drive does not have the functionality or capability of an
independent router and gateway.
- It is possible to change some of the IP configuration octets on the LCD display
but, after a power cycle or after leaving and returning to the IP configuration
pages, the drive reverts to the original value for the first three octets and retains
the new value for the last octet.
With firmware revision 1.008 or later, you can change the IP configuration without any
limitations to the IP configuration octet (parameters). You must enter a valid IP
configuration and cycle power to the drive for the new IP configuration to take effect. If
an illegal IP configuration exists upon power up, for example, if the IP address and
gateway address are identical, the drive faults and exhibits INIT FLT M22 – ILLEGAL
ADDRESS on the display and the IP address configuration changes to DHCP.
Change in keypad and webpage display (LGX00200090)
Corrected:
Known anomaly first identified as of PowerFlex 527 Drives Firmware Revision 1.006
Shunt utilization data on the keypad and webpage always shows zero (0).
With firmware revision 1.008, shunt utilization is no longer shown on the keypad and
webpage. In addition, Output Current is now displayed as Output Curt 0.0 with a value
in Amps RMS. Refer to motion attribute 601 for more information.
Incorrect VelocityLockStatus bit behavior (LGX00171746)
Corrected:
Known anomaly first identified as of PowerFlex 527 Drives Firmware Revision 1.006
Once the ActualSpeed reached or surpassed the Velocity Limit, the
“Axis.VelocityLockStatus” tag / bit in Logix Designer stayed at 1 instead of changing to
0.
Intermitted M28 faults or Safe Torque Off events occur (LGX00194147,
LGX00194148, LGX00194596, LGX00201704)
Corrected:
Known anomaly first identified as of PowerFlex 527 Drives Firmware Revision 1.006
The PowerFlex 527 drive’s internal safety data integrity check leads to an unexpected
close and re-open of its safety connection.
Incorrect motor capacity decay model (LGX00194295, LGX00195436)
Corrected:
Known anomaly first identified as of PowerFlex 527 Drives Firmware Revision 1.006
The implementation of the motor capacity decay model for the PowerFlex 527 drive is
inconsistent when compared to the PowerFlex 750 Series drive.
With firmware revision 1.008, the drive’s motor capacity decay model is updated to be
in-line with the PowerFlex 750 Series drive.
Application Notes
This release has the following application notes.
Determine PowerFlex 527 Firmware Revision Level
Using Studio 5000 Logix Designer® Software
- Launch the Logix Designer software.
- Open the project for your PowerFlex® 527 drive.
- On the main screen, click
and select Go Online.

- Right-click on the PowerFlex 527 drive and select Properties.

- In the Module Properties window, select the Module Info tab to display the
firmware revision.

Update PowerFlex 527 Firmware
Using the ControlFLASH™ Software
- Install the flash kit utility for the PowerFlex 527 drive. You can download the flash
kit utility from the Product Compatibility and Download Center (PCDC) website at:
http://www.rockwellautomation.com/support/pcdc.page
- Launch the ControlFLASH software.
- On the ControlFLASH Welcome screen, click Next. The Catalog Number Dialog
box appears.

- Select the communication device you will use to update the firmware revision and
click Next. For this example, select “PowerFlex 527 via embedded dual port
Ethernet”.
- In the Select Device to Update dialog box, expand the hardware view by clicking
the “+” symbol next to the communication path you are using. For this example,
click the “+” next to “AB_ETHIP-1, Ethernet”.

- Select the entry of the PowerFlex 527 drive you are updating and click OK. The
Firmware Revision dialog box appears.

- Select the firmware revision you want to flash and click Next.
- Follow the remaining prompts to complete the flash update. When the process is
complete, the new firmware revision is displayed in the dialog box.
Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.
Copyright © 2026 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please
click here.Trademarks not belonging to Rockwell Automation are property of their respective companies.