This release corrects the following anomalies.
Fail Drive Connection on Peripheral Error (Lgx00138238)
Corrected Anomaly with Firmware Revision 21.011 and Firmware Revision 20.019
Known Anomaly First Identified as of Firmware Revision 20.011
Catalog Numbers:
If you use a PowerFlex® drive that supports automatic drive configuration (ADC) and has a peripheral that is configured to Fail Drive Connection on Peripheral Error, the controller can experience a major non-recoverable fault (MNRF) when your application is downloaded to the controller.
Local Expansion Modules Configured to Use IOT Instruction (Lgx00136059, Lgx00148390, Lgx00148392, Lgx00148394, and Lgx00148395)
Corrected Anomaly with Firmware Revision 24.011 and Firmware Revision 20.019
Known Anomaly First Identified as of Firmware Revision 20.011
Catalog Numbers:
If any local expansion modules, that is, 1769 Compact I/O™ modules, are configured to use the Immediate Output (IOT) instruction, the controller can experience a major non-recoverable fault (MNRF) at powerup.
To recover from the fault, clear the fault and redownload the project.
To work around this anomaly, configure local expansion modules so that Major Fault On Controller if Connection Fails in Run Mode is enabled.
MAJ Instruction (Lgx00136317, Lgx00150458)
Corrected Anomaly with Studio 5000® Environment Software Revision 21.011, RSLogix 5000® Software Revision 20 and Controller Firmware Revision 20.019
Known Anomaly First Identified as of Firmware Revision 20.011
Catalog Numbers:
An axis can move in the wrong direction in the following conditions:
– Profile Type = Trapezoidal
In this case, the direction on the faceplate is set to forward.
– Profile Type = S-curve
In this case, the sign of the current axis velocity of the axis being merged via the MAJ instruction and the sign of the velocity that is specified by the combination of the Direction parameter and Speed parameter on the faceplate are inconsistent.
You can complete the following tasks to work around this anomaly:
Always set the Speed parameter to +1.0.
If the current axis velocity is unknown, use a GSV instruction to obtain it.
FDU (Fault Dump Utility) (Lgx00174966)
Corrected Anomaly with Firmware Revision 20.019
Known Anomaly First Identified as of Firmware Revision 20.018
Catalog Numbers:
An anomaly was introduced in firmware revision 20.018 that would not let the FDU (Fault Dump Utility) work with the controllers. FDU is used to upload major non-recoverable fault (MNRF) data from the controller.
CompactLogix Wall Clock Time (WCT) jumps ahead by 100 years (Lgx00152701, Lgx00179778)
Corrected Anomaly with Firmware Revision 20.019
Known Anomaly First Identified as of Firmware Revision 17
Catalog Numbers:
The WCT (WallClockTime) of the controller can jump 100 years on a power cycle. This jump can be seen as a one-time 100-year jump or a 100-year jump on every power cycle.
|
Product and Series
|
Continual 100-year
jump on power cycle
|
One-time 100-year jump
on power cycle
|
|
1769-L3x/L2x
|
Yes
|
No
|
|
1768-L4x/A and B
|
No
|
No
|
|
1768-L4x/C and D
|
Yes
|
No
|
|
1756-L63/A
|
No
|
No
|
|
ControlLogix 5560
Controllers series B
|
Yes
|
No
|
|
CompactLogix 5370
|
No
|
No
|
|
1756-L7x
|
No
|
Yes
|
The continual 100-year jump occurs 2 years after a program has been downloaded to a controller after the memory had been cleared / set to default.
The one-time 100-year jump occurs if the WCT is set to a value that has the year from 1990...1999.
Reconfigure Message Instruction Causes a Major Non-Recoverable Fault (Lgx00131221)
Corrected Anomaly with Firmware Revision 20.018
Known Anomaly First Identified as of Firmware Revision 20.011
Catalog Numbers:
If a message instruction is configured to reconfigure an I/O module, it causes the Controller to Experience a major non-recoverable fault (MNRF).
See Knowledgebase document 576267.
Controller Faults When Alarm Instruction is Executed (Lgx00135333)
Corrected Anomaly with Firmware Revision 20.019
Known Anomaly First Identified as of Firmware Revision 20.011
Catalog Numbers:
If an Analog Alarm (ALMA) or Digital Alarm (ALMD) instruction has a string-type associated tag and the string has a negative length, the controller can experience a major non-recoverable fault (MNRF) when the instruction is executed.
UID and UIE Instructions in a Continuous Task (00149169, 00144170)
|
Controllers
|
First Known in
Firmware Revision
|
Corrected in
Firmware Revision
|
|
CompactLogix™ 5370
|
20.011
|
20.019, 24.011 and
later
|
|
GuardLogix® 5570
|
20.011
|
24.011 and
later
|
|
ControlLogix® 5570
|
20.011
|
20.019, 24.011 and
later
|
|
ControlLogix 5560
|
20.011
|
20.019
|
|
1768 CompactLogix L4
|
20.011
|
20.019
|
If the UID (User Interrupt Disable) and UIE (User Interrupt Enable) instructions are used in a continuous task on powerup the controller could major non-recoverable fault (MNRF).
Controller Does Not Detect I/O Module Fault (Lgx00142152, Lgx00142156, Lgx00141744, Lgx00140532)
Corrected Anomaly with Firmware Revision 24.011 and Firmware Revision 20.019
Known Anomaly First Identified as of Firmware Revision 20.011
Catalog Numbers:
In some applications, the controller does not detect I/O module faults on 1769 Compact I/O™ modules. The anomaly occurs when the modules are used as local I/O modules. In this case, the following are a result:
The controller status indicators do not indicate the existence of the fault. Instead, they appear as if the controller is communicating with modules as expected.
The controller does not experience a fault, even if the project configuration calls for a fault on the controller if an I/O fault exists. Instead, the controller continues to operate as if no fault exists.
We recommend that you monitor the controller I/O status tags for I/O module faults. If an I/O module fault occurs, cycle power to the module.
For more information on this anomaly, see Knowledgebase document 558834, CompactLogix controller does not properly handle some 1769 I/O module faults”. The article is accessible from the Rockwell Automation® Technical Support Center at http://www.rockwellautomation.com/support/overview.page.
This release has the following known anomalies.
Applications with PowerFlex drives in the I/O configuration can experience a major non-recoverable fault (MNRF) (00200734, 00200735, 00200600, 00200599)
Corrected Anomaly as of Firmware Revision 31.011 and 30.014 for these catalog numbers:
Corrected Anomaly as of Firmware Revision 31.011 and 30.013 for these catalog numbers:
Known Anomaly First Identified as of Firmware Revision 28.011 for these catalog numbers:
Known Anomaly First Identified as of Firmware Revision 20.011 for these catalog numbers:
If a controller already has an application loaded into it that contains PowerFlex drives in the I/O configuration, a MNRF (Major Non-Recoverable Fault) can occur when any of the following occurs:
For more information and workarounds, see Knowledgebase document 1067997.
These anomalies are from previous releases but are still known in this release.
PI Function Block Appears to Stop Executing
Known Anomaly First Identified as of:
The PI Function block appears to stop executing as the output does not change and instruction faults are logged.
If the PI instruction is being used in Linear mode, this floating point equation is used to calculate the ITerm.
Due to the use of the single-precision floating point values, it is possible. This possibility is dependant on on the values of WLD and KP, for the ITerm value to be small enough, less than 0.0000001, to be lost when adding to the ITermn-1.
For more information regarding the PI instruction, see the Logix5000™ Controllers Process Control and Drives Instructions User Manual, publication 1756-RM006.
Alarm Systems Timeout Changes Require New Download (00069461)
Known Anomaly First Identified as of:
Changes made to the Buffer Timeout value for FactoryTalk® Alarm subscribers do not take effect until the existing buffer has been deleted.
The FactoryTalk alarm buffer (stored in Logix controller memory) is designed to persist through power cycles. If you change the Buffer Timeout value (via the Communication Setup dialog in FactoryTalk View SE), the controller does not use the new timeout value until the existing buffer is deleted and then recreated. To force recreation of this buffer, you can either:
Cycle Power to Clear a Major Fault
Known Anomaly First Identified as of:
If a 1769 I/O fault occurs, you must cycle power to the CompactLogix™ controller after clearing the major fault. I/O communication is not restored until after the power cycle. Never use the fault handling routine to clear local I/O faults. Clear local I/O faults manually on a per case basis, and then the controller must be power cycled.
Time Synchronization Causes Controller to Become Local Master
Known Anomaly First Identified as of:
Enabling the time synchronization feature of a CompactLogix™ controller results in the controller becoming the local master. It does not result in the controller synchronizing with other wallclock times in the system.
Fault/Program States Not Supported by Using the Module Configuration
Dialog Box
Known Anomaly First Identified as of:
This anomaly applies to CompactLogix™ systems as follows:
In this description, the term I/O module refers to 1769 Compact output modules or output points on 1769 Compact combination modules.
RSLogix™ 5000 software does not support Fault/Program state action for I/O modules in CompactLogix systems. The controller cannot trigger the configured Fault/Program state action. You can configure the Fault/Program state action in RSLogix 5000 software, but the configuration does not take effect.
If either of the following conditions exists, outputs turn off, regardless of the Fault/Program state action configuration:
Additionally, RSLogix 5000 software generates configuration tags for any I/O modules in the project. Some of the tags define configuration (C) data type members that include attributes for Fault/Program states, also known as alternate output states.
Because CompactLogix systems do not support Fault/Program state action for I/O modules, do not configure the attribute tags listed in the following table.
Attribute Tags to Avoid
|
Digital Output Modules
|
Analog Output Modules
|
|
Where CHx = the channel number
|
Using Automatic Device Configuration (00129165)
Known Anomaly First Identified as of:
When using the Automatic Device Configuration (ADC) feature, the Logix controller ‘owns’ the configuration in the drive. Do not use the HIM or other external tools, such as DriveExplorer™, to change drive parameters. Doing so can cause a sequence of events to occur that results in the connection between the controller and the drive to be dropped. Also, the controller cannot re-establish the connection.
Consider using the Write Mask function (drive Parameter 888 - [Write Mask Cfg]) to prevent tools that are connected to ports other than the Embedded EtherNet/IP port from writing to the drive.
ALMA and ALMD Tag Members Mismatch (00119996)
Known Anomaly First Identified as of:
The MinDurationPRE and MinDurationACC members of ALARM_ANALOG and ALARM_DIGITAL tags are defined as DINT (signed double integer) but they are treated as UDINT (unsigned double integer) by Logix firmware. This causes negative values of the tag members to be handled as large positive numbers when they must be handled as zero.
Accept Edits Effect on Controller Log (00122622)
Known Anomaly First Identified as of:
When you accept edits in LD, ST, and FBD, the controller will log an ‘Online Edit’ entry in the controller log. Accepting edits in an SFC routine is done by performing a partial import, resulting in a ‘Transaction Commit’ entry in the controller log.
This function is confusing because you can select to mask both entries separately. Selecting only Online edits would cause the Audit Value to change only when FBD, ST, and LD edits are made. SFC online edits would change the Audit Value only if the ‘Partial Import Online Transaction Completed’ bit was set.
Maximum Simultaneous Active Reconfigure Messages (00125204)
Known Anomaly First Identified as of:
The controller only supports three active reconfigure messages at a time. If more than three are triggered at a time, they complete (DN bit goes high), but not all modules are reconfigured.
For example, if you send five reconfiguration messages simultaneously, three reconfigure messages truly complete (DN bit goes high), and the I/O modules are reconfigured. The other two reconfigure messages indicate complete (DN bit goes high), but the I/O modules is not reconfigured. In this case, the last two are supposed to have errored (ER bit), but do not.
Corrected: Logix Firmware/Studio 5000 Software 21.011
Log On to FactoryTalk Dialog Box Displays When Launching RSLogix 5000 (00124955)
Known Anomaly First Identified as of:
When launching RSLogix™ 5000 software, the Log On to FactoryTalk® dialog box can display. This dialog box can be seen when you do not have Administrator privileges on the personal computer and the current user does not exist in the FactoryTalk directory. If this dialog box is canceled, the RSLogix 5000 software is not launched. When the dialog box is displayed, entering the credentials for a user that has Administrator privileges on the personal computer allows RSLogix 5000 software to be launched.
To avoid seeing this dialog box, you can add the current user or user group to the FactoryTalk directory. Follow these steps to add a user or user group to the FactoryTalk directory.
(In some cases, to continue, you need to provide credentials for a user with Administrator privileges.)
(You can click Check Names to verify that the name was found.)
The Log On to FactoryTalk dialog box can also be displayed when you are using Remote Desktop to connect to the personal computer running RSLogix 5000 software.
This dialog box appears because FactoryTalk Security does not recognize the computer name. To enable access through Remote Desktop for a specific computer, you must add the name of the computer initiating the Remote Desktop connection to the Network\System\Computers and Groups\Computers folder in the FactoryTalk Administration Console.
To allow all computers to connect, follow these steps.
IMPORTANT: If Use single sign-on is set to disable in FactoryTalk software, then the Log On to FactoryTalk dialog box is displayed each time RSLogix 5000 software is launched. When this is launched, proper user credentials must be entered to continue. (By default, ‘Use single sign-on’ is set to enable.)
SFC Action Body Executes Erroneously (00124697)
Known Anomaly First Identified as of:
In SFCs, when using time-limited actions in steps, if the program stays on a given step for greater than 24 days (2**32 ms) the accumulator of the timer (ACC) rolls over and the action body starts to execute again.
The time-limited action initializes its timer when it starts (step is first scanned). On subsequent scans, it compares the timers PRE and ACC value. If ACC<PRE, the action body executes. If ACC >=PRE, it is not executed. When the rollover occurs, the ACC,PRE, and the action body incorrectly exectutes.
Arithmetic State Flags (00122480)
Known Anomaly First Identified as of:
Arithmetic State flags anomalies.
Logix CPU Security Tool Unavailable
Known Anomaly First Identified as of:
The Logix CPU security tool does not work with version 20 controllers.
RSLogix 5000 Clock Update Does Not Support Some Operating Systems
Known Anomaly First Identified as of:
The RSLogix 5000 Clock Update tool does not support Windows 7 or Windows Server 2008 operating systems.
Out of I/O Memory Error on Download (00148860)
Known Anomaly First Identified as of Firmware Revision 20.011
Catalog Numbers:
Download firmware, associated files, and access product release notes from the Product Compatibility and Download Center at http://www.rockwellautomation.com/rockwellautomation/support/pcdc.page.
Message Instructions in Add-On Instruction PreScan and Main Logic Routines (Lgx00152820)
Known Anomaly since Firmware Revision 16
Catalog Numbers:
If a message instruction with the same backing tag is used in an Add-On Instruction in the Prescan and Main Logic routine, the controller on a transition to Run mode does one of the following:
Or