Release Notes

Firmware Upgrade Kit containing OS501 for SLC 5/05
Version 13.000 (released 3/2016)

Catalog Number 1747-L553 

These release notes describe version information for 1747-L553, version 13.000 (released 3/2016).

Requirements

This release has the following requirements.

System Requirements

Catalog Numbers 1747-L551, 1747-L552, 1747-L553

To ControlFLASH upgrade your SLC processor, your system must be at this minimum configuration:

  

Application Notes

This release has the following application notes.

SLC 5/05 Processors Firmware/Operating System ControlFLASH Upgrade Procedure

Catalog Numbers 1747-L551, 1747-L552, 1747-L553

These instructions describe how to install the ControlFLASH utility, setup prerequisites for preparing the system for upgrade, and instructions for upgrading your processor to the latest firmware.


Prior to Running ControlFLASH

For OS501 Series C FRN 9 and later, the SNMP Server must be enabled for the upgrade to occur. The ability to disable the SNMP Server that was added in Series C FRN 9 and later, requires RSLogix 500® version 6.30 or higher.

  1. Save the current SLC™ 5/05 processor program.

IMPORTANT

The user program is cleared as part of the operating system upgrade process. You must restore your program after successfully loading the operating system upgrade.
 
  1. Note the IP address assigned to the SLC 5/05 processor. When updating the processor, use BOOTP or fixed IP address, not DHCP. The IP address may be read from the processor when you are online with RSLogix 500 software. In the Channel Configuration dialog box select the Chan. 1 – System tab. If BOOTP Enable is selected and the IP Address is 0.0.0.0, then note the Ethernet Hardware Address (located on the Ethernet Daughtercard) of the 5/05 processor, which begins with 00:00:BC).

IMPORTANT

Refer to the following Rockwell Automation publications for more information on the Ethernet Communication Protocol:
  • SLC 500 Instruction Set Reference Manual,
    publication 1747-RM001
  • SLC 500 Modular Hardware Style User Manual,
    publication number 1747-UM011
 

 


IMPORTANT

If you are not sure whether an IP address is assigned or cannot determine what the IP address is, return the 5/05 processor to initial factory conditions.
 



Return the SLC 5/05 Processors to Initial Factory Conditions


IMPORTANT

If you return the processor to the initial factory conditions, the user program and communication configurations are returned to their default settings.
 


To return the processor to initial factory conditions.


graphic

ATTENTION:  Do not remove the processor from the SLC 500 chassis until all power is removed from the SLC 500 power supply.
 
  1. Remove power from the SLC 500 power supply.
  2. Remove the processor from the chassis.
  3. Disconnect the battery by removing the battery connector from its socket.
  4. Locate the VBB and GND connections on the back of the motherboard.
  5. Place a small bladed screwdriver across the VBB and GND connections and hold for 60 seconds.

This returns the processor to the initial factory conditions.

graphic



Use ControlFLASH


graphic

ATTENTION:  Do not interrupt the flash procedure. Once you have begun to download the firmware for either the daughtercard (step 18) or the motherboard (step 24), the SLC 5/05 is put into an unrecoverable state if you lose power or communications for any reason.
 
  1. Launch the ControlFLASH application under Programs>Flash Programming Tools.
  2. Verify that the J4 jumper of the SLC 5/05 processor being upgraded is set to Protect.
    The daughtercard firmware can only be updated when the J4 jumper is set to Protect.

graphic

  1. Insert the SLC 5/05 processor into an SLC chassis.
  2. Attach an Ethernet cable to the processor from your computer (or a hub).

IMPORTANT

If you are connecting to the SLC 5/05 processor through a hub, you can use a standard Ethernet patch cable. If you are connecting directly to the SLC 5/05 processor from your computer, you need to use an Ethernet crossover cable.
 
  1. Apply power to the chassis.
  2. Verify that the SLC 5/05 processor key switch is in the PROG or REM PROG (RUN LED indicator not illuminated) mode.
    The Welcome to ControlFLASH dialog box appears.

graphic

  1. Click Next.
  2. Select the appropriate catalog number from the Catalog Number dialog box and click Next. For Series C Processors, select catalog numbers that are followed by a ‘/C’.

graphic

The AB_SNMP.DLL – Enter IP Address dialog box appears.

graphic

  1. Enter the IP address for the processor.

IMPORTANT

Use the IP address that was noted in step 2 of the section, Prior to Running ControlFLASH. If the processor has been reset to Initial Factory Conditions, use an available IP address assigned by your network administrator.
 
  1. Click the Get Info button.

If the IP address was previously configured in the processor, go to step 12.

The AB_SNMP – BOOTP Server dialog box appears, indicating that this IP address has not been configured into the processor.

graphic

  1. Enter the hardware address of the SLC 5/05 processor that is being upgraded and click OK. The hardware address is noted in step 2 of the section, Prior to Running ControlFLASH.

graphic


The AB_SNMP – BOOTP Server Running dialog box may take several seconds or minutes to appear.

graphic


You may need to wait several seconds or minutes before you are returned to the AB_SNMP.DLL – Enter IP Address dialog box. Within a few seconds, the Device Identification box displays the processor’s current revision information.

  1. Click OK.

graphic

  1. Select the appropriate revision from the Firmware Revision dialog box and click Next.

graphic


The Summary dialog box appears.

graphic

  1. Click Finish.

The ControlFLASH dialog box appears.

graphic

  1. Click Yes.

If your PC has more than one Ethernet interface installed, the following dialog box displays the assigned IP addresses of each of the listed Ethernet interfaces. Proceed to the next step. If your PC does not have more than one Ethernet interface installed, go to step 18.

graphic

  1. Highlight the IP address of the PC Ethernet interface that connects to the Ethernet network hosting the target processor.
  2. Click OK.

You may need to wait several seconds before the Progress dialog box appears. A typical sequence is shown below. While the download is in progress, the ENET LED changes

  1. from a solid green to flashing green to solid red and then turns solid green again. When he daughtercard update is complete, the ENET LED flashes green. The download process of the daughtercard firmware can take up to approximately two minutes.

graphic

graphic

graphic

  1. When the message ‘Waiting while module burns flash…’ and all progress bars are displayed, check the AB_SNMP dialog box. Open it from your taskbar if it does not appear automatically.

The AB_SNMP dialog box prompts you to turn off power, remove the processor, move the jumper to Program, re-insert the processor, and apply power.


graphic

ATTENTION:  Do not remove the processor from the SLC 500 chassis until all power is removed from the SLC 500 power supply.
 
  1. Wait for the ENET LED to turn solid green.
  2. Click OK.

graphic

  1. If your PC has more than one Ethernet interface installed, then the following dialog box displays the assigned IP addresses of each of the listed Ethernet interfaces. Proceed to the next step.

If your PC does not have more than one Ethernet interface installed, go to step 24.

graphic


Highlight the IP address of the PC Ethernet interface that connects to the Ethernet network hosting the target processor. Click OK.
  1. The AB_SNMP – BOOTP Server Running dialog box may appear.

graphic


A Progress dialog box is displayed again. A typical sequence is shown starting below. While the download is in progress, the RUN and FLT LED indicators remain off. The other four LED indicators – RS232, ENET, FORCE, and BATT – turn on and off in a walking bit sequence. When the update is complete, these four LED indicators remain on together. The download process of the firmware takes approximately 3 minutes.

graphic

graphic

graphic

  1. Open the AB_SNMP dialog box from the task bar if it does not appear automatically. Follow the dialog box prompts to do the following:

graphic

ATTENTION:  Do not remove the processor from the SLC 500 chassis until all power is removed from the SLC 500 power supply.
 
  1. Once you have re-applied power, wait for the ENET LED indicator to turn solid green. Click OK.

graphic


The AB_SNMP – BOOTP Server Running dialog box may appear.

graphic


The Update Status dialog box appears. If the update was successful, the status text box is green and has an appropriate message.

graphic


If the update was not successful, the status text box is red and has an appropriate message.

graphic

  1. Click OK and you are returned to the Welcome to ControlFLASH dialog box.

graphic

  1. You may either continue upgrading additional SLC 5/05 processors by clicking Next, or you may exit the program by clicking Cancel. If you click Cancel, you are asked to verify that you want to end the update session.

graphic



After Successfully Updating Your SLC 5/05 Processor

  1. Remove power from the SLC 500 power supply and remove the processor from the chassis.

graphic

ATTENTION:  Do not remove the processor from the SLC 500 chassis until all power is removed from the SLC 500 power supply.
 
  1. Apply the enclosed operating system upgrade label to the SLC 5/05 processor nameplate.
  2. Re-insert the processor into the chassis and apply power.
  3. Restore your program to the processor.



ControlFLASH Error Messages

There are three error messages you can receive.



Invalid Catalog Number

The following error message is displayed if:

graphic


To clear this error:

  1. Click OK.

graphic

  1. Click Cancel to go to the Catalog Number dialog box. You may either:

graphic

ATTENTION:  Do not remove the processor from the SLC 500 chassis until all power is removed from the SLC 500 power supply.
 
  1. Restart the firmware upgrade procedure in the Use ControlFLASH section.



Target Module Not in Proper State for Programming

The following dialog box appears when this error occurs:

graphic


To clear this error:
  1. Place the SLC 5/05 processor into PROG mode.
  2. Ensure that DHCP is not selected.
  3. Restart the firmware upgrade process at the beginning of the Use ControlFLASH section. If the error occurs again, power-cycle the SLC 5/05 processor and restart the firmware upgrade process.


Failed to Receive Initial TFTP Request from Target

The following dialog boxes appear in the sequence shown when this error occurs.

graphic

graphic


To clear this error:

  1. Connect the processor’s Ethernet port directly to the PC Ethernet port using a crossover cable, or disable or uninstall any firewall VPN or virus protection software running on the PC.
  2. Power-cycle the processor.
  3. Restart the firmware upgrade process.
  
Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.

Copyright © 2026 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please click here.
Trademarks not belonging to Rockwell Automation are property of their respective companies.