Release Notes

FactoryTalk View Site Edition is HMI software for monitoring and controlling applications of any size, from single computer, single user station applications to distributed server-client, multiple user applications. FACTORYTALK VIEW SE SHOULD BE DOWNLOADED USING A SERVER OR STATION SERIAL NUMBER; CLIENT SERIAL NUMBERS MAY NOT PROVIDE ACCESS TO ALL VERSIONS.
Version 8.10.00 (released 8/2015)

Catalog Number FactoryTalk View Site Edition 

These release notes describe version information for FactoryTalk View Site Edition, version 8.10.00 (released 8/2015).

Requirements

This release has the following requirements.

The following are the system requirements for FactoryTalk View SE version 8.10.00 (CPR 9 SR 8).

The hardware and software you use with FactoryTalk View Site Edition depends on the demands an application places on the system. The greater the demand, the more powerful a system you need.

For large or complex applications you should use computers with faster CPUs and more RAM. In any application, faster CPUs and more RAM will result in better performance.

In addition, there should always be sufficient disk space to provide virtual memory that is at least twice the size of the physical RAM.

Supported operating systems for running FactoryTalk View SE Client, Server, or Station

  Windows Server 2012

  • Windows Server 2012 Datacenter (64-bit)
  • Windows Server 2012 R2 Datacenter (64-bit)
  • Windows Server 2012 R2 Standard Edition (64-bit)
  • Windows Server 2012 Standard Edition (64-bit)

  Windows 8.1

  • Windows 8.1 Enterprise Edition (32-bit or 64-bit)
  • Windows 8.1 Professional (32-bit or 64-bit)

  Windows 8

  • Windows 8 Professional (32-bit or 64-bit)
  • Windows 8 Enterprise Edition (32-bit or 64-bit)

  Windows 7

  • Windows 7 Ultimate with Service Pack 1 (64-bit)
  • Windows 7 Enterprise Edition with Service Pack 1 (64-bit)
  • Windows 7 Professional with Service Pack 1 (32-bit or 64-bit)
  • Windows 7 Professional (32-bit or 64-bit)

Windows Server 2008

  • Windows Server 2008 R2 Standard Edition (64-bit)
  • Windows Server 2008 R2 Enterprise Edition with Service Pack 1 (64-bit)
  • Windows Server 2008 R2 Standard Edition with Service Pack 1 (64-bit)
  • Windows Server 2008 Standard Edition with Service Pack 2

Windows XP

  • Windows XP Professional with Service Pack 3 (32-bit)

Operating system recommendations for application servers

  Recommended FactoryTalk View SE HMI Server Operating Systems:

  • Windows Server 2012 Datacenter edition (64-bit)
  • Windows Server 2012 R2 Datacenter edition (64-bit)
  • Windows Server 2012 Standard edition (64-bit)
  • Windows Server 2012 R2 Standard edition (64-bit)
  • Windows Server 2008 Standard Edition with Service Pack 2 (32-bit or 64-bit)
  • Windows Server 2008 R2 Standard Edition with Service Pack 1 (64-bit)

  Minimum FactoryTalk View SE HMI Server Operating Systems if running fewer than 10 clients in a workgroup:

  • Windows 8.1 Professional (32-bit or 64-bit)
  • Windows 8 Professional (32-bit or 64-bit)
  • Windows 7 Professional (32-bit or 64-bit)
  • Windows XP Professional with Service Pack 3 (32-bit)

Hardware requirements for operator workstations

For computers hosting FactoryTalk View SE Clients in a network application, or for a FactoryTalk View SE Client running a local station application:

  • Recommended: Intel Core 2 Duo, 2.66 GHz or higher, and 2 GB RAM or more
  • Minimum: Intel Pentium 4,2GHz or higher, 1GB RAM or more

Hardware requirements for engineering workstations

For computers hosting FactoryTalk View Studio or FactoryTalk View SE Administration Console in a network application:

  • Recommended: Intel Core 2 Duo, 2.66 GHz or higher, and 2 GB RAM or more
  • Minimum: Intel Pentium 4, 2GHz or higher, 1GB RAM or more

Hardware requirements for application servers

For computers hosting FactoryTalk View SE HMI Server, FactoryTalk Alarms and Events Tag Server, or RSLinx Enterprise in a network application:

  • Recommended: Quad core Intel Xeon, 2.33 GHz or higher, 4 GB RAM
  • Minimum: Intel Pentium 4, dual CPU, 3GHz or higher, 2GB RAM or more

Security requirements

For information on the security considerations when using Rockwell Automation products, including

  • File extensions created by Rockwell Automation software, firewall rules, and service dependences, see Rockwell Automation Knowledgebase Answer ID 609492.
  • TCP/UDP ports used by Rockwell Automation products, see Rockwell Automation Knowledgebase Answer ID 29402.  

  Tips:

  • Some Microsoft operating system service packs and hot fixes are not compatible with FactoryTalk View Site Edition. To find out if there are any problems with a particular Microsoft update, click this link to open Answer ID 20450 (FactoryTalk View SE Operating System and Service Pack Compatibility Matrix) in the Rockwell Automation Knowledgebase.
  • FactoryTalk View Site Edition is tested on operating systems installed from original Microsoft media only.

Features

This release includes the following system features.

FactoryTalk View SE version 8.10.00 has the following new and enhanced features.

Configuration and application building

Run-time experience improvement

Alarming improvement

Other enhancements


Corrected Anomalies in This Release

This release corrects the following anomalies.

The following list identifies the anomalies corrected in FactoryTalk View SE version 8.10.00.

Known Anomalies in This Release

This release has the following known anomalies.

The following list identifies the known anomalies or limitations of FactoryTalk View SE version 8.10.00 at the time of the release.

For the latest information about the software platforms supported by FactoryTalk View SE, open Product Compatibility & Download Center or click this link to open Answer ID 42682 (Rockwell Automation Software Product Compatibility Matrix) in the Rockwell Automation Knowledgebase.

ActiveX Objects

Data logging to an ODBC data source

DeskLock hot key not disabled in Windows 7 or Windows 2008 operating system

Diagnostics logging to a remote database

Display Client

Distributed Application Manager

FactoryTalk Directory

Find and Replace

Global Objects

Graphic Displays

HMI server

HMI tags

Installation

Importing CSV files

Kepware

Memory Leak with SQL Server

PNG image support

OpenRSLogix5000 command

RSLinx Classic 2.43

String Display

TrendX

Windows operating systems

HMI project folder does not replicate to secondary HMI Server

HMI project folder does not replicate to secondary HMI Server for Windows Server 2008 or Windows 7 Professional.

This can be caused by a couple of situations. One cause could be the size of the HMI project file being larger than the maximum allowable file transfer size, the other by the replicating taking longer than the default time limit of 20 minutes.

If the project size is larger than the file transfer size lime of 500,000,000 bytes

If the total size of the project is greater than 500MB, then it is advisable to change the setting to be a little larger than the size of the project. The workaround is to go to a command line and change the size to an acceptable value.

Use an appcmd command to change the limit size:  

  1. With Windows 7 and Windows Server 2008; select Start > Programs > Accessories > Command Prompt, select Run as administrator
  2. At the command prompt, type cd /d %windir%\system32\inetsrv, and then press Enter.
  3. Type appcmd.exe set config "Default Web Site/RSViewSE/" /section:System.webServer/security/requestFiltering /
    requestLimits.maxAllowedContentLength:500000000 /commit:apphost
    , with no returns, and press Enter.
    Note: The 500000000 in the example below should be changed to at least the size of the actual project, or a little larger than the size of the project.
  4. At the command prompt, type exit and press Enter.

If the amount of time to replicate is longer than 20 minutes to complete

If the project is large, and takes longer than the default 20 minutes to complete, it may not replicate. The workaround is to set the MaxReplicationWaitTime registry key to a larger time limit value. The registry key can be set from 1 to 600 (minutes). This registry key needs to be set on both the FactoryTalk View Studio and Secondary HMI server computers.

For complete details about this topic, see Answer ID 38407 in the Rockwell Automation Knowledgebase.

Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.

Copyright © 2026 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please click here.
Trademarks not belonging to Rockwell Automation are property of their respective companies.