Release Notes

20G - Firmware versions and revisions can be found in the Versions tab above
Version 11.002 Signed (released 6/2015)

Catalog Number PowerFlex 755 (series A)

These release notes describe version information for PowerFlex 755, version 11.002 Signed (released 6/2015).

Requirements

This release has the following requirements.

Auto/Manual HIM Preload Requires New HIM Firmware

System Requirements Identified as of PowerFlex 755 Drive Firmware Revision 3.004

The new Auto/Manual HIM Preload feature requires firmware in the HIM that is newer than 1.007.

 
Customer Configurable Response to HIM Communications Loss

System Requirements Identified as of PowerFlex 755 Drive Firmware Revision 3.004

System Requirements Identified as of PowerFlex 753 Drive Firmware Revision 5.001

The Customer Configurable Response to HIM Communications Loss feature requires a new enhanced style HIM (20-HIM-A6, 20-HIM-C6S). This feature will not work with older contemporary 7-Class HIM’ s (20-HIM-A3, 20-HIM-A5, 20-HIM-C3S, 20-HIM-C5S).

 
Max Output Frequency Limited to 590Hz

System Requirement Identified as of PowerFlex 755 Drives Firmware Revision 8.001

System Requirement Identified as of PowerFlex 753 Drives Firmware Revision 9.001

This revision of drive firmware places a limit on the maximum output frequency of the drive. In previous versions of drive firmware the maximum operating frequency of the drive was 650 Hz. The new maximum output frequency limit is 590 Hz. If a previous application allows for a maximum output frequency greater than 590 Hz, the drive will ramp to the command frequency set point and once it reaches a value greater than 590 Hz for a period of time greater than 16ms the drive will trip on a Fault 31, “ Over-Freq” .
 
Implementation of Signed Firmware Files
(Replaces the previous version of this topic on the PCDC)

System Requirement Identified as of PowerFlex 755 Drives Firmware Revision 11.001

System Requirement Identified as of PowerFlex 753 Drives Firmware Revision 11.001

With this revision of drive firmware, an encryption layer with a digital signature has been attached to the drive firmware file. This encryption layer will not allow a drive firmware update with a firmware file that is not digitally signed by Rockwell Automation.

Digitally-signed firmware files have been created for previous unsigned firmware revisions. The minor revision number has been incremented to identify the signed revision. See the tables below for a list of PowerFlex 755 and PowerFlex 753 unsigned and signed firmware revisions.

You must update the unsigned firmware to revision 11.001 CONVERT to enable the secure firmware feature to read the digital signature. Once the unsigned firmware has been updated to revision 11.001 CONVERT, the drive can be updated to any desired signed firmware revision (earlier or later than 11.001).

For example, to update the drive firmware from revision 9.001 Unsigned to revision 10.003 Signed, update the drive firmware using the revision 11.001 CONVERT file to enable the secure firmware feature and read the digital signature. Then, update the drive firmware to revision 10.003 Signed. This process is true for any of the other previous unsigned firmware revisions.

Note: Use the 11.001 Signed firmware file when updating any previous signed revision of firmware to revision 11.001.

Note: If you want to update your drive firmware revision to 12.001 Signed, or later, see the ‘Update PowerFlex 75x Drive Firmware rev C’ topic in the revision 12.001 (or later) release notes.

Revisions of drive firmware that don’t have a ‘Signed’ digital signature embedded in the firmware file will display the error shown below when an update is attempted.

graphic

The following table identifies which PowerFlex 755 firmware revisions have a secure digital signature embedded in the firmware file:

Firmware Revision
Disposition
3.004
Unsigned revision
3.005
Signed revision
4.001
Unsigned revision
4.002
Signed revision
5.001
Unsigned revision
5.002
Signed revision
6.003
Unsigned revision
6.004
Unsigned revision
6.005
Signed revision
7.001
Unsigned revision
7.002
Signed revision
8.001
Unsigned revision
8.002
Signed revision
9.001
Unsigned revision
9.002
Signed revision
10.002
Unsigned revision
10.003
Signed revision

The following table identifies which PowerFlex 753 firmware revisions have a secure digital signature embedded in the firmware file:

Firmware Revision
Disposition
5.001
Unsigned revision
5.002
Signed revision
6.002
Unsigned revision
6.003
Unsigned revision
6.004
Unsigned revision
6.005
Signed revision
7.001
Unsigned revision
7.002
Signed revision
8.001
Unsigned revision
8.002
Signed revision
9.001
Unsigned revision
9.002
Signed revision
10.001
Unsigned revision
10.002
Signed revision


  

EtherNet/IP Port and 20-750-ENETR Require Quality of Service (QoS)

System Requirements Identified as of PowerFlex 755 Drive Firmware Revision 9.001

System Requirements Identified as of PowerFlex 753 Drive Firmware Revision 9.001

With this firmware revision, the EtherNet/IP port and 20-750-ENETR require the EtherNet/IP scanner to use a compatible method of specifying Quality of Service (QoS). The following table details the compatible products and firmware revisions.

 

Product
Compatible Rev. No.
DriveLogix 5730 Embedded Ethernet Port
Rev. 3.1.4
CompactLogix (1769-L2x/L3x)
Rev. 17.03
ControlLogix (1756-ENBT)
Rev. 4.005
CompactLogix (1768-ENBT)
Rev. 2.001
FlexLogix (1788-ENBT)
Rev. 2.004
ControlLogix 1756-EN2T (F)(XT)
No Update needed
SoftLogix I/O Messaging
No Update needed



  

 

Drive Firmware, Series, and Frame Size Compatibility Requirements

System Requirement Identified as of PowerFlex 755 Drive Firmware Revision 3.004

The following table identifies firmware revisions and the PowerFlex 755 drive series and frame sizes with which they are compatible:

Firmware Revision
Compatible with Drive Series
Compatible with Drive Frame Size
2.xxx
A
2…8
3.xxx…5.xxx
A
2…7
B
8 and 9
6.xxx…7.xxx
A
1…7
B
8 and 9
8.xxx and Later
A
1…7
B
8…10


  

Corrected Anomalies in This Release

This release corrects the following anomalies.

Analog Input Filter Does Not Function Properly

CORRECTED with PowerFlex 755 Drives Firmware Revision 11.002

CORRECTED with PowerFlex 753 Drives Firmware Revision 11.002

This revision of firmware corrects an anomaly associated with the Analog Input Filter function for the 120V 22-Series I/O card (20-750-2262D-2R). Prior to the fix, a change in parameters 55 [Filter Gain] and 56 [Filter Bandwidth] (excluding default values) would cause an exponential value to be populated in parameter 50 [Analog Input Value] and the Analog Input Filter did not function correctly. With the new firmware, the Analog Input Filter will perform its intended functionality.

 

Known Anomalies from Previous Releases

These anomalies are from previous releases but are still known in this release.

Feedback Selection

Known Anomaly First Identified as of PowerFlex 755 Drives Firmware Revision 3.004

Known Anomaly First Identified as of PowerFlex 753 Drives Firmware Revision 5.001

The HIM startup on the PowerFlex 755 drive includes a feedback device selection step. Depending on the option modules installed, that step may first ask the user to choose a port, then a parameter. In some situations, the list of ports incorrectly shows multiple copies of 'Port 0 - PowerFlex 755' followed by the feedback port/module.


The incorrect behavior happens only under the following conditions:

When the incorrect port list appears, it is still possible to successfully select the feedback module port by following one of these methods.

Persistent Stop Command with Profile Message Fault Action

Known Anomaly First Identified as of PowerFlex 755 Drives Firmware Revision 8.001

Known Anomaly First Identified as of PowerFlex 753 Drives Firmware Revision 8.001

In an application with the use of a PowerFlex 755 or PowerFlex 753 along with the 20-750-ENETR dual port Ethernet/IP module, a persistent stop command may appear in some cases. The action of disconnecting the Ethernet cable from the 20-750-ENETR module, which will result in the drive stopping, may follow with a nuisance fault action. This fault action previously noted is persistent communication of stop commands.

 
Saving Parameters Using DriveExplorer

Known Anomaly First Identified as of PowerFlex 755 Drives Firmware Revision 8.001

Known Anomaly First Identified as of PowerFlex 753 Drives Firmware Revision 8.001

In an application with the use of a PowerFlex 755 or PowerFlex 753 along with the 20-750-ENETR dual port Ethernet/IP module, in which a user attempts to save all parameters using DriveExplorer® in some causes the save execution does not complete. When attempting to execute the save all parameters in DriveExplorer the software tool enters an infinite loop and does not progress through the save in some instances. To exit the loop, press the cancel button and check if the text file has been saved.

 
Support for Changing Permanent Magnet Direction Test Current

Known Anomaly First Identified as of PowerFlex 755 Drive Firmware Revision 2.011

Known Anomaly First Identified as of PowerFlex 753 Drive Firmware Revision 7.001

You cannot change the level of current used during the direction test on a permanent magnet motor while in Integrated Motion on EtherNet/IP (CIP Motion) mode. It is set at 10%. If the system requires more than 10% to turn the motor, it will fail to perform the test.

 
Delta Junction Temp at Zero Speed

Known Anomaly First as of PowerFlex 755 Drive Firmware Revision 2.011

The protection algorithms in frame 8 drives create false 168 “PWM Freq Reduced” exception events when running at zero speed. These can occur when the drive is first energizing the motor and establishing motor flux.

 
Diagnostic Item and Parameter Values Affected by Flash from Version 1 to Version 6

Known Anomaly First Identified as of PowerFlex 755 Drive Firmware Revision 3.004

Known Anomaly First Identified as of PowerFlex 753 Drive Firmware Revision 5.001

The following internal diagnostic items may contain incorrect data after upgrading a PowerFlex 755 from revision 1 to revision 6 firmware: 2 [PBLT Pwrup Time], 3 [PBLT GatesOnTime], 4 [PBLT Mtr MW Hrs], 5 [PBLT Rgn MW Hrs] and 67 [PwrBd Pwr Cycles].

The following parameters may contain incorrect data after upgrading a PowerFlex 755 from revision 1 to revision 6 firmware: 13[Elapsed MWH], 14 [Elapsed kWH], 15 [Elapsed Run Time], 16 [Elpsd Mtr MWHrs], 17 [Elpsd Rgn MWHrs], 18 [Elpsd Mtr kWHrs], 19 [Elpsd Rgn kWHrs], 490 [HSFan ElpsdLife], 497 [InFan ElpsdLife], 503 [MtrBrngElpsdLife], 508 [MtrLubeElpsdHrs], 512 [MchBrngElpsdLife] and 517 [MchLubeElpsdHrs].

These values will affect the associated calculated “ remaining life ” parameter values and predictive maintenance events.

 
Missing Error When Drive NV Selected in Integrated Motion Mode

Known Anomaly First Identified As of PowerFlex 755 Drive Firmware Revision 3.004

This anomaly affected customers using Integrated Motion on EtherNet/IP (CIP Motion). If you attempted to use Drive NV when configuring the motor on a motion axis with a PowerFlex 755, the drive would not return the appropriate error. This feature is not currently supported in the PowerFlex 755.

 
CIP Motion Axis Inhibit F927 Event

Known Anomaly First Identified as of PowerFlex 755 Drive Firmware Revision 8.001

The drive may throw an F927 fault when an axis is inhibited. If this occurs, the drive will shut down allowing the motor to coast. The status LED will blink 27 times, pause, then repeat. If this occurs, cycle power to the drive to clear the fault.

 
F918 Exception Events

Known Anomaly First Identified as of PowerFlex 755 Drive Firmware Revision 6.004

Known Anomaly First Identified as of PowerFlex 753 Drive Firmware Revision 6.004

When running in Flux Vector open loop mode for induction motor or Interior Permanent Magnet (IPM) motor mode, the drive may experience an F918 exception event when the motor accelerates through a 7 Hz operating frequency due to the simultaneous transition from a 2 to 4 KHz carrier frequency. This exception can be avoided by setting parameter 40 [Mtr Options Cfg] bit 9 – PWM FreqLock], which will keep the carrier frequency at 4 KHz.

 

Application Notes

This release has the following application notes.

Determine PowerFlex 755 Drive Firmware Revision Level

Application Notes


Use the Drive LCD HIM

  1. Access the Status screen, which is displayed on HIM power up.

graphic

  1. Use the graphic or graphic key to scroll to Port 00 for the Host Drive.
  2. Press the graphic key to display its last-viewed folder.
  3. Use the graphic or graphic key to scroll to the DIAGNOSTIC folder.
  4. Use the graphic or graphic key to select Device Version.
  5. Press the graphic (Enter) key to display device version information.

FW Revision is listed under – Main Control Board.

graphic


Use DriveExplorer Lite/Full

Important: You need DriveExplorer version 6.01 or later to interface with the PowerFlex 755 drive. To obtain the latest version, visit the Allen-Bradley Web Updates site located at http://www.ab.com/support/abdrives/webupdate

 

  1. Launch DriveExplorer and go online with the PowerFlex 755 drive. To connect to the drive, use a 1203-USB converter, a 1203-SSS converter, or an EtherNet/IP network connection.
  2. In the Devices hardware view, select the PowerFlex 755 drive.

Once selected, information regarding the PowerFlex 755 drive is shown in the right panel including the current firmware revision number.

graphic


Use DriveExecutive

Important: You need DriveExecutive version 5.01 or later to interface with the PowerFlex 755 drive. To obtain the latest version, visit the Allen- Bradley Web Updates site located at http://www.ab.com/support/abdrives/webupdate

 

  1. Launch DriveExecutive and go online with the PowerFlex 755 drive. To connect to the drive, use a 1203-USB converter, a 1203-SSS converter, or an EtherNet/IP network connection.
  2. In the Drives hardware view, select the PowerFlex 755 drive (graphic).
  3. Click the information icon (graphic) to display the drive’ s Properties dialog box.

In the Properties dialog box the “ Revision:” field (graphic ) will show the drive ’s current firmware revision number.

graphic

 

Update PowerFlex 755 Drive Firmware

Product Updates and Replacements


Flashing can be performed using a 1203-USB or 1203-SSS converter. For information on connecting either converter to your drive, refer to the 1203-USB USB Converter User Manual, publication DRIVES-UM001, or 1203-SSS Smart Self-powered Serial Converter User Manual, publication 20COMM-UM001.

Note: Images are shown for example only. They are not intended to identify the exact firmware version to which you are updating. Therefore, do not use the data in the images as input or selections for your update.


Frame 8 and Larger Drives

When a Frame 8 or larger drive is flashed with firmware earlier than V4, a F361 “Rerate See Manual” fault will result.

  1. Confirm the drive's current configuration by viewing Port 10, P21 [Effctv I Rating].
  2. Save the current parameter settings using the Human Interface Module (HIM), DriveExecutive, or DriveExplorer.
  3. Perform the flash update.

When concluded, an F361 “Rerate See Manual” fault is indicated.

  1. Set Port 10, P20 [Recfg Acknowledg ] to 1 “Acknowledge” to accept the reconfiguration.

Important: Drive parameters are set to factory defaults when the reconfiguration is acknowledged. If a condition exists that does not allow the drive parameters to be set to factory defaults, setting P20 to 1 “Acknowledge” will not be accepted. Such conditions include the drive is currently running, DeviceLogix is currently running, or the drive is communicating with a PLC.

  1. Download the saved drive configuration.
  2. Confirm the motor and drive ratings before running the drive.


Install the Flash Kit

  1. Install the flash kit utility for the PowerFlex 755 drive, which includes the latest version of the ControlFLASH utility and deploys firmware files for using HyperTerminal on your computer.
  2. You are now ready to use DriveExplorer, DriveExecutive, ControlFLASH or HyperTerminal to update the drive.


Use DriveExplorer Lite/Full to Flash Update

  1. With the Flash Kit installed (see “Install the Flash Kit”), launch DriveExplorer and go online (via a 1203-USB or 1203-SSS converter) with the PowerFlex 755 drive.
  2. In the Devices hardware view, select the PowerFlex 755 drive (graphic).
  3. Click the information icon (graphic)to display the drive’s Properties dialog box.
  4. In the Properties dialog box, click the Component Details tab (graphic).

graphic

  1. With the Main Control Board selected, click Flash Update.

graphic

Important: Flash updating the device firmware may cause the device to load defaults. It is recommended that you save the setting to your PC before proceeding.

  1. From the list of available updates, select the desired firmware revision and click Next >.

graphic

  1. Follow the remaining prompts until the flash update procedure completes and displays the new firmware revision.

Use DriveExecutive to Flash Update

  1. With the Flash Kit installed, launch DriveExecutive and go online (via a 1203-USB or 1203-SSS converter) with the PowerFlex 755 drive.
  2. In the Drives hardware view, select the PowerFlex 755 drive (graphic).
  3. Click the information icon (graphic)to display the drive’s Properties dialog box.
  4. In the Properties dialog box, click the Component Details tab (graphic).

graphic

  1. With the PowerFlex 755 drive selected, click Flash Update.

graphic

  1. From the list of available devices, select the PowerFlex 755 drive and click Next >.

graphic

Important: Flash updating the device firmware may cause the device to load defaults. It is recommended that you save the setting to your PC before proceeding.

  1. From the list of available updates, select the desired firmware revision and click Next >.

graphic

  1. Follow the remaining screen prompts until the flash update procedure completes and displays the new firmware revision.


Use ControlFLASH to Flash Update

  1. With the Flash Kit installed, launch ControlFLASH by selecting Start > (All) Programs > Flash Programming Tools > ControlFLASH.
  2. On the ControlFLASH Welcome screen, click Next >.

graphic

  1. The Catalog Number dialog box appears. From the list, choose the communication device you will use to update the PowerFlex 755 drive. In the figure below, the embedded EtherNet device is selected.

Once the appropriate communication device is selected, click Next >.

graphic

  1. Now that the correct communication device has been selected, you must select which device is being updated. With the Select the PowerFlex… dialog box displayed, follow these steps.
    1. Expand the hardware view for the communication path you are using (graphic).
    2. Select the drive icon that represents the PowerFlex 755 drive you are updating (graphic).
    3. Click OK (graphic).

graphic

  1. In the Multiple Assemblies Found display box, select “Port x-PowerFlex 755” from the list and click OK.

graphic

  1. In the Firmware Revision dialog box, select the desired firmware revision from the list of available updates and click Next >.

graphic

  1. Follow the remaining prompts until the flash procedure completes and displays the new firmware revision.


Use HyperTerminal to Flash Update

Important: The HyperTerminal process takes at least one hour to complete.

  1. With the Flash Kit installed, access and launch HyperTerminal as shown below.

graphic

  1. A New Connection dialog box appears.
    1. Enter the connection device name in the Name field or select an icon from the library.
    2. Click OK once you have finished.

graphic

  1. A Connect To dialog box appears.
    1. Use the “Connect using:” drop-down menu to select the appropriate connection device.
    2. Click OK once you have finished.

graphic

  1. A Properties dialog box will appear for the selected connection device.
    1. Use any of the drop-down menus to change the various port settings.
    2. Click OK once you have finished.

graphic

  1. After you click OK, you will get a blank screen.

Press Enter on your computer keyboard so the following test screen appears.

graphic

  1. From the Main Menu, select the flash upgrade (graphic) by pressing the number 3 key on your computer keyboard.
  2. Additional text appears. From the Flash Upgrade menu, select the PowerFlex 775 drive (graphic) by pressing the number 0 key on your computer keyboard.
  3. Additional text appears. After reading the conditions, select Yes (graphic) to proceed by pressing the letter Y key on your computer keyboard.

graphic

The terminal program will start displaying the letter “C”. This signals the XMODEM protocol that the download may proceed.

graphic

Important: You have one minute to complete steps 9…14 or HyperTerminal will return to step 5, where you must repeat steps 5…8.

Tip: To cancel the flash update at any time, press CTRL-X.

  1. Select Transfer > Send File to display the Send File dialog box.

graphic

  1. Click Browse and navigate to one of the following locations:
  1. Search within the appropriate subfolder until the “PF755_LP_App_vxx_xxx_xxx.dpi” file appears in the Select File to Send list.
  2. With the file name highlighted, click Open so it appears in the Filename data field in the Send File dialog box.

graphic

  1. In the Protocol box, select “Xmodem.”
  2. Click Send.

A dialog box appears and reports the update progress, which takes about one hour for HyperTerminal to complete. When it is complete, the message “Flash Complete” appears.

graphic

  1. Press any key to continue.
  2. Press the Enter key to return to the main menu.

Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.

Copyright © 2026 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please click here.
Trademarks not belonging to Rockwell Automation are property of their respective companies.