Release Notes

CompactLogix L35E controller
Version 20.014 (released 8/2014)

Catalog Number 1769-L35E (series A)

These release notes describe version information for 1769-L35E, version 20.014 (released 8/2014).

Security

This release includes security enhancements as a part of our ongoing efforts to improve security. For information regarding Rockwell Automation's vulnerability disclosure process, please reference the Rockwell Automation Vulnerability Policy.

Access Denied dialog box does not appear when users without FactoryTalk Security access attempt to modify Motion Configuration (Lgx00184951)

Studio 5000 Logix Designer v29.00

Corrected Anomaly with Studio Logix Designer v30.00

When a user without Motion: Modify Configuration security credentials attempts to modify the motion configuration, an Access Denied dialog box does not appear.

Requirements

This release has the following requirements.

Firmware Requirements – 1769 CompactLogix Controllers

Catalog Numbers 1769-L31, 1769-L32C, 1769-L32E, 1769-L35CR, 1769-L35E

Consider the following before upgrading the firmware on your 1769 CompactLogix controller:

Consideration
Description
Avoid Interrupting the Firmware Upgrade
 
When upgrading your controller firmware, it is extremely important to allow the upgrade to complete without interruption.
If you interrupt the firmware upgrade either in the software or by disturbing the physical media, you may render the controller inoperable.
During an upgrade of the CompactLogix firmware, the ControlFLASH™ utility displays various progress dialog boxes. The progress dialog boxes contain these status statements:
  • Transmitting block…
  • Polling for power-up…
It is crucial that you do not interrupt the firmware upgrade while these progress statements are displayed. Once the Update Status dialog box indicates that the firmware upgrade is complete, you may adjust your controller’s network connection, make changes using controller-related software, or cycle controller power.
End Cap Needed for Firmware Upgrade
Attempting a firmware upgrade without the controller end cap attached does not complete.
When upgrading your controller firmware, verify that your end cap is properly attached and locked. If you attempt to upgrade without the end cap attached, your firmware upgrade may not complete successfully.

 

Controller Memory Limits
If your controller is close to its memory limit and this firmware revision requires more project memory, you can upgrade to a controller that has more memory.
Avoid Loss of Communication During Firmware Upgrade
Loss of communication or power during a controller firmware upgrade may result in the controller’s rejection of the new firmware. If the controller firmware upgrade fails due to those conditions described, the following corrective actions may be required.
  • Cycle controller power with the battery disconnected for 2…3 minutes, then successfully complete the flash upgrade.
  • If a nonrecoverable fault occurs, contact Rockwell Automation Technical Support for a ticket number and return the controller for factory repair.
Disconnect Controller from DH-485 Network Before Firmware Upgrade
If your controller is connected to a DH-485 network, disconnect it from the DH-485 network before you update the firmware of the controller. If you update the firmware of a controller while it is connected to a DH-485 network, communication on the network may stop.
Firmware Upgrade on 1769-L32E or 1769-L35E Controller
IMPORTANT: This consideration applies only to 1769-L32E and 1769-L35E controllers.
We recommend that you complete the following tasks before attempting a firmware upgrade on a 1769-L32E or 1769-L35E:
  1. Check the status of the MS (module status) status indicator next to the Ethernet port. If it is flashing red before you begin the upgrade, additional action may be required. Contact Rockwell Automation Technical Support for more information.
  2. Modify the Port Configuration for the Ethernet card so that the Network Configuration Type is set to Static and assign a valid IP address.
  3. If RSWho is actively browsing the controller through an Ethernet or serial connection, close the RSWho window to stop the browse.
  4. If other controllers are messaging to the 1769-L32E or 1769-L35E controller, take the other controllers off the network or put them in Program mode.
  5. If there are controllers consuming tags from the 1769-L32E or 1769-L35E controller, remove them from the network.
  6. If there are HMI devices connected to the controller, disconnect them from the network or shut them down.
IMPORTANT: If you cannot perform the tasks listed above before attempting a controller firmware upgrade, Ethernet traffic on the controller’s Ethernet port may cause the ControlFLASH utility to timeout during the firmware upgrade. If the timeout condition is not handled properly, you may render the Ethernet port on the controller inoperable, requiring you to return the controller to Rockwell Automation for repair.
In the event that a ControlFLASH timeout occurs, the software displays an error dialog indicating that the ‘Target Device failed to report the new revision number’, or that the upgrade ‘Failed to begin update to the target device’.
If the error dialog boxes display, check the MS status indicator. If the indicator is flashing red, the upgrade is still in progress and should not be interrupted. Do not cycle power to the controller while the status indicator is flashing red.
If the upgrade completes, the controller power cycles itself and indicates the upgrade is complete with a solid green MS status indicator. The time required to complete the upgrade is dependent on the level of Ethernet traffic.
If the controller does not complete the upgrade, the MS status indicator continues flashing red. In this case, contact Rockwell Automation Services and Support.
Use of ControlFLASH software, Version 9 (CPR9 SR3) with Firmware Revision 19
IMPORTANT: This consideration applies only when you are using firmware revision 19.
Consider the following before you install the ControlFLASH software, version 9:
  • We recommend you install RSLinx communication software, version 2.057, before you install ControlFLASH software, version 9 (CPR9 SR3).
  • If you install RSLinx communication software, version 2.057, before you install ControlFLASH software, version 9, you can enable or disable the FactoryTalk Security platform during ControlFLASH software, version 9, installation. However, to disable the FactoryTalk Security platform, you must first uninstall ControlFLASH software, version 9, then reinstall it.
  • If the FactoryTalk Security platform is enabled during ControlFLASH software, version 9, installation, the software opens with a Select FactoryTalk Directory dialog box. At that dialog box, click the following:
    • Network
    • Local
    • Cancel - If you click Cancel, you must select a directory.
  • ControlFLASH software, version 9, only integrates the FactoryTalk Security platform in the FactoryTalk Services Platform, version 2.030 or later.

 

 

Corrected Anomalies in This Release

This release corrects the following anomalies.

Corrected: Logix Firmware 20.014

Controller Logs Minor Fault Code 3 Type 93 (00129124, 00129117)

Known Anomaly

Cat. No.
Identified As Of
1769-L23E-QB1B, 1769-L23E-QBFC1B, 1769-L23-QBFC1B
Firmware Revision 20.011/RSLogix 5000 Software Version 20
1769-L31, 1769-L32C, 1769-L32E,1769-L35CR, 1769-L35E
Firmware Revision 20.011/RSLogix 5000 Software Version 20

Regardless of how you configure the RPIs for the I/O on the local CompactBus, the controller logs a minor fault Code 3 Type 93. If you clear this error, the fault will occur again in 35…40 minutes.

If this minor error is appearing more frequently, you have an application issue that needs to be corrected; for example, RPIs are set too fast, there are user tasks at or above priority 6, the controller is performing high-speed trending.

 

Tag Incorrectly Identified as Being on Scan (Lgx00148404)

Corrected as of:

Known Anomaly First Identified as of:

Catalog Numbers:


If you use RSLinx® Enterprise software for HMI communication and you try to modify or delete a controller tag online or try to modify an I/O module configuration, you can get the error 'Failed to modify properties. Tag is actively being read by one or more clients.' The controller improperly determines that a tag is on scan when it is not.

Known Anomalies in This Release

This release has the following known anomalies.

Applications with PowerFlex drives in the I/O configuration can experience a major non-recoverable fault (MNRF) (00200734, 00200735, 00200600, 00200599)

Corrected Anomaly as of Firmware Revision 31.011 and 30.014 for these catalog numbers:

Corrected Anomaly as of Firmware Revision 31.011 and 30.013 for these catalog numbers:

Known Anomaly First Identified as of Firmware Revision 28.011 for these catalog numbers:

Known Anomaly First Identified as of Firmware Revision 20.011 for these catalog numbers:

If a controller already has an application loaded into it that contains PowerFlex drives in the I/O configuration, a MNRF (Major Non-Recoverable Fault) can occur when any of the following occurs:

For more information and workarounds, see Knowledgebase document 1067997.



Known Anomalies from Previous Releases

These anomalies are from previous releases but are still known in this release.

PI Function Block Appears to Stop Executing

Known Anomaly First Identified as of:

The PI Function block appears to stop executing as the output does not change and instruction faults are logged.

If the PI instruction is being used in Linear mode, this floating point equation is used to calculate the ITerm.

graphic

Due to the use of the single-precision floating point values, it is possible. This possibility is dependant on on the values of WLD and KP, for the ITerm value to be small enough, less than 0.0000001, to be lost when adding to the ITermn-1.

For more information regarding the PI instruction, see the Logix5000™ Controllers Process Control and Drives Instructions User Manual, publication 1756-RM006.



Alarm Systems Timeout Changes Require New Download (00069461)

Known Anomaly First Identified as of:

Changes made to the Buffer Timeout value for FactoryTalk® Alarm subscribers do not take effect until the existing buffer has been deleted.

The FactoryTalk alarm buffer (stored in Logix controller memory) is designed to persist through power cycles. If you change the Buffer Timeout value (via the Communication Setup dialog in FactoryTalk View SE), the controller does not use the new timeout value until the existing buffer is deleted and then recreated. To force recreation of this buffer, you can either:


Cycle Power to Clear a Major Fault

Known Anomaly First Identified as of:

If a 1769 I/O fault occurs, you must cycle power to the CompactLogix™ controller after clearing the major fault. I/O communication is not restored until after the power cycle. Never use the fault handling routine to clear local I/O faults. Clear local I/O faults manually on a per case basis, and then the controller must be power cycled.

Time Synchronization Causes Controller to Become Local Master

Known Anomaly First Identified as of:

Enabling the time synchronization feature of a CompactLogix™ controller results in the controller becoming the local master. It does not result in the controller synchronizing with other wallclock times in the system.


Fault/Program States Not Supported by Using the Module Configuration
Dialog Box

Known Anomaly First Identified as of:

This anomaly applies to CompactLogix™ systems as follows:

In this description, the term I/O module refers to 1769 Compact output modules or output points on 1769 Compact combination modules.

RSLogix™ 5000 software does not support Fault/Program state action for I/O modules in CompactLogix systems. The controller cannot trigger the configured Fault/Program state action. You can configure the Fault/Program state action in RSLogix 5000 software, but the configuration does not take effect.

If either of the following conditions exists, outputs turn off, regardless of the Fault/Program state action configuration:

Additionally, RSLogix 5000 software generates configuration tags for any I/O modules in the project. Some of the tags define configuration (C) data type members that include attributes for Fault/Program states, also known as alternate output states.

Because CompactLogix systems do not support Fault/Program state action for I/O modules, do not configure the attribute tags listed in the following table.

Attribute Tags to Avoid

Digital Output Modules
Analog Output Modules
  • ProgToFaultEn
  • ProgMode
  • ProgValue
  • FaultMode
  • FaultValue
  • CHxProgToFaultEn
  • CHxProgMode
  • CHxFaultMode
Where CHx = the channel number

Using Automatic Device Configuration (00129165)

Known Anomaly First Identified as of:

When using the Automatic Device Configuration (ADC) feature, the Logix controller ‘owns’ the configuration in the drive. Do not use the HIM or other external tools, such as DriveExplorer™, to change drive parameters. Doing so can cause a sequence of events to occur that results in the connection between the controller and the drive to be dropped. Also, the controller cannot re-establish the connection.

Consider using the Write Mask function (drive Parameter 888 - [Write Mask Cfg]) to prevent tools that are connected to ports other than the Embedded EtherNet/IP port from writing to the drive.


ALMA and ALMD Tag Members Mismatch (00119996)

Known Anomaly First Identified as of:

The MinDurationPRE and MinDurationACC members of ALARM_ANALOG and ALARM_DIGITAL tags are defined as DINT (signed double integer) but they are treated as UDINT (unsigned double integer) by Logix firmware. This causes negative values of the tag members to be handled as large positive numbers when they must be handled as zero.


Accept Edits Effect on Controller Log (00122622)

Known Anomaly First Identified as of:

When you accept edits in LD, ST, and FBD, the controller will log an ‘Online Edit’ entry in the controller log. Accepting edits in an SFC routine is done by performing a partial import, resulting in a ‘Transaction Commit’ entry in the controller log.

This function is confusing because you can select to mask both entries separately. Selecting only Online edits would cause the Audit Value to change only when FBD, ST, and LD edits are made. SFC online edits would change the Audit Value only if the ‘Partial Import Online Transaction Completed’ bit was set.


Maximum Simultaneous Active Reconfigure Messages (00125204)

Known Anomaly First Identified as of:

The controller only supports three active reconfigure messages at a time. If more than three are triggered at a time, they complete (DN bit goes high), but not all modules are reconfigured.

For example, if you send five reconfiguration messages simultaneously, three reconfigure messages truly complete (DN bit goes high), and the I/O modules are reconfigured. The other two reconfigure messages indicate complete (DN bit goes high), but the I/O modules is not reconfigured. In this case, the last two are supposed to have errored (ER bit), but do not.


Corrected: Logix Firmware/Studio 5000 Software 21.011

Log On to FactoryTalk Dialog Box Displays When Launching RSLogix 5000 (00124955)

Known Anomaly First Identified as of:

When launching RSLogix™ 5000 software, the Log On to FactoryTalk® dialog box can display. This dialog box can be seen when you do not have Administrator privileges on the personal computer and the current user does not exist in the FactoryTalk directory. If this dialog box is canceled, the RSLogix 5000 software is not launched. When the dialog box is displayed, entering the credentials for a user that has Administrator privileges on the personal computer allows RSLogix 5000 software to be launched.

To avoid seeing this dialog box, you can add the current user or user group to the FactoryTalk directory. Follow these steps to add a user or user group to the FactoryTalk directory.

  1. Launch the FactoryTalk Administration Console (available from the Start menu).
  2. Select the Network directory when prompted.

(In some cases, to continue, you need to provide credentials for a user with Administrator privileges.)

  1. To allow access for a particular user, navigate to Network\System\Users and Groups\Users, right-click the Users folder and choose New>Windows Linked User.
  2. Click Add and provide the domain\logon name for the desired user.

(You can click Check Names to verify that the name was found.)

  1. To allow access for all authenticated users, navigate to Network\System\Users and Groups\User Groups, right-click the User Groups folder and choose New>Windows Linked User Group.
  2. Click Add and type the name of the user group, Authenticated Users.

The Log On to FactoryTalk dialog box can also be displayed when you are using Remote Desktop to connect to the personal computer running RSLogix 5000 software.

This dialog box appears because FactoryTalk Security does not recognize the computer name. To enable access through Remote Desktop for a specific computer, you must add the name of the computer initiating the Remote Desktop connection to the Network\System\Computers and Groups\Computers folder in the FactoryTalk Administration Console.

To allow all computers to connect, follow these steps.

  1. Open the FactoryTalk Administration Console and log in to the Network directory with your domain credentials.
  2. Navigate to Network\System\Security Policy. In the Computer Policy Settings section, set Identify terminal server clients with the name of to Server Computer.

IMPORTANT: If Use single sign-on is set to disable in FactoryTalk software, then the Log On to FactoryTalk dialog box is displayed each time RSLogix 5000 software is launched. When this is launched, proper user credentials must be entered to continue. (By default, ‘Use single sign-on’ is set to enable.)


SFC Action Body Executes Erroneously (00124697)

Known Anomaly First Identified as of:

In SFCs, when using time-limited actions in steps, if the program stays on a given step for greater than 24 days (2**32 ms) the accumulator of the timer (ACC) rolls over and the action body starts to execute again.

The time-limited action initializes its timer when it starts (step is first scanned). On subsequent scans, it compares the timers PRE and ACC value. If ACC<PRE, the action body executes. If ACC >=PRE, it is not executed. When the rollover occurs, the ACC,PRE, and the action body incorrectly exectutes.


Arithmetic State Flags (00122480)

Known Anomaly First Identified as of:

Arithmetic State flags anomalies.

  1. When dealing with floating point numbers, the controller does not truncate denormalized values or -0.0…0.0.
  2. For an integer divide, when the denominator is 0, the S:N and S:Z are not set.
  3. For the MOD instruction, the S:V is not set if an overflow occurred during the calculation.

Logix CPU Security Tool Unavailable

Known Anomaly First Identified as of:

The Logix CPU security tool does not work with version 20 controllers.


RSLogix 5000 Clock Update Does Not Support Some Operating Systems

Known Anomaly First Identified as of:

The RSLogix 5000 Clock Update tool does not support Windows 7 or Windows Server 2008 operating systems.


Fail Drive Connection on Peripheral Error (Lgx00138238)

Corrected Anomaly with Firmware Revision 21.011 and Firmware Revision 20.019

Known Anomaly First Identified as of Firmware Revision 20.011

Catalog Numbers:

If you use a PowerFlex® drive that supports automatic drive configuration (ADC) and has a peripheral that is configured to Fail Drive Connection on Peripheral Error, the controller can experience a major non-recoverable fault (MNRF) when your application is downloaded to the controller.




Local Expansion Modules Configured to Use IOT Instruction (Lgx00136059, Lgx00148390, Lgx00148392, Lgx00148394, and Lgx00148395)

Corrected Anomaly with Firmware Revision 24.011 and Firmware Revision 20.019

Known Anomaly First Identified as of Firmware Revision 20.011

Catalog Numbers:

If any local expansion modules, that is, 1769 Compact I/O™ modules, are configured to use the Immediate Output (IOT) instruction, the controller can experience a major non-recoverable fault (MNRF) at powerup.

To recover from the fault, clear the fault and redownload the project.

To work around this anomaly, configure local expansion modules so that Major Fault On Controller if Connection Fails in Run Mode is enabled.




MAJ Instruction (Lgx00136317, Lgx00150458)

Corrected Anomaly with Studio 5000® Environment Software Revision 21.011, RSLogix 5000® Software Revision 20 and Controller Firmware Revision 20.019

Known Anomaly First Identified as of Firmware Revision 20.011

Catalog Numbers:

An axis can move in the wrong direction in the following conditions:

– Profile Type = Trapezoidal

In this case, the direction on the faceplate is set to forward.

– Profile Type = S-curve

In this case, the sign of the current axis velocity of the axis being merged via the MAJ instruction and the sign of the velocity that is specified by the combination of the Direction parameter and Speed parameter on the faceplate are inconsistent.

You can complete the following tasks to work around this anomaly:

Always set the Speed parameter to +1.0.

If the current axis velocity is unknown, use a GSV instruction to obtain it.



CompactLogix Wall Clock Time (WCT) jumps ahead by 100 years (Lgx00152701, Lgx00179778)

Corrected Anomaly with Firmware Revision 20.019

Known Anomaly First Identified as of Firmware Revision 17

Catalog Numbers:

The WCT (WallClockTime) of the controller can jump 100 years on a power cycle. This jump can be seen as a one-time 100-year jump or a 100-year jump on every power cycle.

Product and Series
Continual 100-year jump on power cycle
One-time 100-year jump on power cycle
1769-L3x/L2x
Yes
No
1768-L4x/A and B
No
No
1768-L4x/C and D
Yes
No
1756-L63/A
No
No
ControlLogix 5560 Controllers series B
Yes
No
CompactLogix 5370
No
No
1756-L7x
No
Yes

The continual 100-year jump occurs 2 years after a program has been downloaded to a controller after the memory had been cleared / set to default.

The one-time 100-year jump occurs if the WCT is set to a value that has the year from 1990...1999.


Reconfigure Message Instruction Causes a Major Non-Recoverable Fault (Lgx00131221)

Corrected Anomaly with Firmware Revision 20.018

Known Anomaly First Identified as of Firmware Revision 20.011

Catalog Numbers:

If a message instruction is configured to reconfigure an I/O module, it causes the Controller to Experience a major non-recoverable fault (MNRF).

See Knowledgebase document 576267.




Controller Faults When Alarm Instruction is Executed (Lgx00135333)

Corrected Anomaly with Firmware Revision 20.019

Known Anomaly First Identified as of Firmware Revision 20.011

Catalog Numbers:

If an Analog Alarm (ALMA) or Digital Alarm (ALMD) instruction has a string-type associated tag and the string has a negative length, the controller can experience a major non-recoverable fault (MNRF) when the instruction is executed.





Message Instructions in Add-On Instruction PreScan and Main Logic Routines (Lgx00152820)

Known Anomaly since Firmware Revision 16

Catalog Numbers:

If a message instruction with the same backing tag is used in an Add-On Instruction in the Prescan and Main Logic routine, the controller on a transition to Run mode does one of the following:

Or



  

UID and UIE Instructions in a Continuous Task (00149169, 00144170)

Controllers
First Known in Firmware Revision
Corrected in Firmware Revision
CompactLogix™ 5370
20.011
20.019, 24.011 and later
GuardLogix® 5570
20.011
24.011 and later
ControlLogix® 5570
20.011
20.019, 24.011 and later
ControlLogix 5560
20.011
20.019
1768 CompactLogix L4
20.011
20.019


If the UID (User Interrupt Disable) and UIE (User Interrupt Enable) instructions are used in a continuous task on powerup the controller could major non-recoverable fault (MNRF).






  

Controller Does Not Detect I/O Module Fault (Lgx00142152, Lgx00142156, Lgx00141744, Lgx00140532)

Corrected Anomaly with Firmware Revision 24.011 and Firmware Revision 20.019

Known Anomaly First Identified as of Firmware Revision 20.011

Catalog Numbers:

In some applications, the controller does not detect I/O module faults on 1769 Compact I/O™ modules. The anomaly occurs when the modules are used as local I/O modules. In this case, the following are a result:

The controller status indicators do not indicate the existence of the fault. Instead, they appear as if the controller is communicating with modules as expected.

The controller does not experience a fault, even if the project configuration calls for a fault on the controller if an I/O fault exists. Instead, the controller continues to operate as if no fault exists.

We recommend that you monitor the controller I/O status tags for I/O module faults. If an I/O module fault occurs, cycle power to the module.

For more information on this anomaly, see Knowledgebase document 558834, CompactLogix controller does not properly handle some 1769 I/O module faults”. The article is accessible from the Rockwell Automation® Technical Support Center at http://www.rockwellautomation.com/support/overview.page.




Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.

Copyright © 2026 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please click here.
Trademarks not belonging to Rockwell Automation are property of their respective companies.