Release Notes

More information: PowerFlex® 525 Site
Version 1.005 (released 6/2014)

Catalog Number PowerFlex 525 (series A)

These release notes describe version information for PowerFlex 525, version 1.005 (released 6/2014).

Corrected Anomalies in This Release

This release corrects the following anomalies.

Clearing Fault Using Drive Keypad can take Multiple Attempts (LGX00143382)

Corrected: PowerFlex 525 Drives Firmware Revision 1.005

When a fault occurs, using the “Stop” key on the drive keypad to clear the fault may take more than one attempt.

 
Drive LCD Display Unable to Show Turkish, Polish, or Czech Languages (LGX00140760)

Corrected: PowerFlex 525 Drives Firmware Revision 1.005

The drive LCD display is unable to show Turkish, Polish, or Czech languages.

Important: This anomaly has been fixed in this firmware revision. However, due to a limitation of the LCD display, some of the characters for Turkish, Polish, and Czech languages will be modified.

 
Drive Sometimes Unresponsive to Start Command Sent Using EtherNet/IP (LGX00141783)

Corrected: PowerFlex 525 Drives Firmware Revision 1.005

When a “Start” command is sent to a drive using EtherNet/IP, sometimes the drive does not respond and the command needs to be resent.

 
DSI Comms Through 1203-USB Becomes Unresponsive After Resetting Communication Adapter (LGX00143529)

Corrected: PowerFlex 525 Drives Firmware Revision 1.005

If a Bulletin 1203-USB converter is used to interface with the DSI port on a drive that has an attached communication adapter, resetting the communication adapter using Connected Components Workbench™ software causes DSI comms to become unresponsive.

 
Firmware of Attached 25-COMM-E2P Cannot be Flashed Through the Drive

Corrected: PowerFlex 525 Drives Firmware Revision 1.005

The firmware of an attached PowerFlex® 25-COMM-E2P adapter cannot be flashed through the drive.

 
Parameter P053 Command Sent from Controller to Drive Using 25-COMM-E2P in Multi-drive Mode can Cause Fault F081 DSI Comm Loss (LGX00141166)

Corrected: PowerFlex 525 Drives Firmware Revision 1.005

This anomaly applies to drives using the PowerFlex 25-COMM-E2P adapter in Multi-drive mode.

When the controller sends the parameter P053 [Reset to Defalts] command to the drive through the adapter, fault F081 “DSI Comm Loss ” can occur.

 
Resetting Fault F083 EN Comm Loss can Cause Fault F114 uC Failure" (LGX00139755)

Corrected: PowerFlex 525 Drives Firmware Revision 1.005

When a drive is disconnected from EtherNet/IP and faults on F083 “EN Comm Loss”, resetting this fault can cause fault F114 “uC Failure ” to occur.

 

Known Anomalies in This Release

This release has the following known anomalies.

Drive Runs Immediately Following Removal of Stop Condition While Start or Jog Bit via Comms Remains Active (1) (LGX00152681)

Corrected: PowerFlex 525 Drives Firmware Revision 2.003

Corrected: PowerFlex 523 Drives Firmware Revision 2.002

Known Anomaly Identified as of PowerFlex 525 Drives Firmware Revision 1.005

If the user's controller program holds the Start or Jog command bit active (1) in the drive’s logic command word, asserting a "Stop condition" will result in the drive stopping as expected. However, when the "Stop condition” is removed, the drive will run immediately if the Start or Jog command bit is still active (1).

PowerFlex 525 drive firmware revision 2.003 and PowerFlex 523 drive firmware revision 2.002 corrects this behavior. The removal of the Stop condition will no longer cause the drive to run (with Start or Jog bit active). A transition of the Start or Jog bit must now be initiated for the drive to run.

See Knowledge Base ID 603580 – Product Notice 2014-06-001 – PowerFlex 523/525 Start and Jog Bit Logic (201406001) for more details.

 
Resetting Faults when Drive is Powering Down can Cause Fault F105 C Connect Err (LGX00144194)

Corrected: PowerFlex 525 Drives Firmware Revision 2.002

Known Anomaly Identified as of PowerFlex 525 Drive Firmware Revision 1.005

When power is shut off, the drive will discharge any remaining power. During this period, resetting a drive fault may cause fault F105  C Connect Err ” to occur.

 
Drive Faults on F105 C Connect Err After Clearing Faults and Cycling Power (LGX00150140)

Corrected: PowerFlex 525 Drives Firmware Revision 2.003

When a fault is cleared by setting parameter A551 [Fault Clear] to 2 “Clear Buffer” or comm logic command 2002H Bit 3 to 1 “Clear Faults”, fault F105 “C Connect Err” occurs after the drive is power cycled.

This anomaly exists in firmware revision 1.005 and 2.002. It will cause the drive to not trigger fault F004 “UnderVoltage” before power off and causes fault F105 “C Connect Err” to occur after power up.

Firmware revision 2.003 corrects this anomaly so that when the drive is power cycled, fault F004 “UnderVoltage” should trigger before power off and no fault should occur after power up.

 

Known Anomalies from Previous Releases

These anomalies are from previous releases but are still known in this release.

Security Vulnerability in PowerFlex 525 AC Drives with Embedded EtherNet/IP (152230)


Corrected Anomaly with PowerFlex® 525 Drives Firmware Revision 5.002

Known Anomaly First Identified as of PowerFlex 525 Drives Firmware Revision 1.003

Catalog Number: 25B


This product release remediates a security vulnerability in the firmware. This vulnerability may affect the availability of network communications to this product due to resource exhaustion and/or memory corruption. An affected product would require manual intervention to recover. For complete details on the vulnerability and recommended mitigations, refer to KnowledgeBase article 1082684.

  

Application Notes

This release has the following application notes.

Determine PowerFlex 525 Firmware Revision Level

Application Notes


Using Connected Components Workbench Software

  1. Launch the Connected Components Workbench software.
  2. Open the project for your PowerFlex 525 drive.
  3. On the main screen, click graphic to go online.
  4. graphicgraphicThe firmware revision is displayed on the screen as shown in this example. graphic


Using Studio 5000 Logix Designer Software

  1. Launch the Logix Designer software.
  2. Open the project for your PowerFlex 525 drive.
  3. On the main screen, click graphic and select Go Online.

graphic

  1. Right-click on the PowerFlex 525 drive and select Properties.

graphic

  1. In the Module Properties window, select the Module Info tab to display the firmware revision.

graphicgraphicgraphic


Using the Drive LCD Display and Keypad

Step
Key(s)
Example Display
1.
When power is applied, the last user-selected Basic Display Group parameter number is briefly displayed with flashing characters. The display then defaults to that parameter’ s current value.
(Example shows the value of b001 [Output Freq] with the drive stopped.)
 
graphic
2.
Press Esc to display the Basic Display Group parameter number shown on power-up. The parameter number will flash.
graphic
graphic
3.
Press the Up Arrow or Down Arrow to scroll to parameter b029 [Control SW Ver].
graphic
or
graphic
graphic
4.
Press Enter to display the drive’ s firmware revision.
graphic
graphic

 

Update PowerFlex 525 Firmware


Product Updates and Replacements

Using the USB Utility Application

  1. Separate the Control Module from the Power Module.

 

TIP
For more information on how to separate the Control Module from the Power Module, see the PowerFlex® 520-Series Adjustable Frequency AC Drive User Manual, publication 520-UM001.
  1. Connect one end of a USB cable to the USB port on the back of the Control Module.
  2. Connect the other end to the PC. A Windows® Explorer window appears.

graphic

  1. Launch the PF52XUSB utility application. The PowerFlex 520-Series USB Application window appears.

graphic

  1. Click Flash and select the firmware with which you want to update the module.
  2. Click Yes. The Confirm Flash Update dialog box appears. It displays the current firmware revision and the new revision to be flashed.

graphic

  1. Click Flash.
  2. When the process is complete, click OK.
  3. Close the application and disconnect the Control Module from the PC.
  4. Connect the Control Module to the Power Module and power cycle the drive.
  5. During the boot-up sequence, the following commands are displayed on the drive’ s LCD display: BOOT > COPY1 > COPY2 > ERASE > BOOT
  6. When fault F105 “C Connect Err” occurs, clear the fault to complete the flash update.
  7. The LCD display shows the drive data and current firmware revision.
    Alternatively, you can verify the firmware revision by checking parameter b029 [Control SW Ver].

  
TIP
If the firmware revision did not update properly, you may need to reset the drive to default and cycle drive power.

Using the ControlFLASH™ Software

  1. Install the flash kit utility for the PowerFlex 525 drive. You can download the flash kit utility from the Allen-Bradley Web Updates site at: http://www.ab.com/support/abdrives/webupdate/
  2. Launch the ControlFLASH software.
  3. On the ControlFLASH Welcome screen, click Next. The Catalog Number dialog box appears.

graphic

  1. Select the communication device you will use to update the firmware revision and click Next. For this example, select “PowerFlex 525 via PowerFlex 520-Series Comms” .
  2. In the Select Device to Update dialog box, expand the hardware view by clicking the “+” symbol next to the communication path you are using. For this example, click the “+” next to “AB_ETHIP-1, Ethernet ”.

graphic

  1. Select the entry of the PowerFlex 525 drive you are updating and click OK. The Firmware Revision dialog box appears.

graphic

  1. Select the firmware revision you want to flash and click Next.
  2. Follow the remaining prompts to complete the flash update. When the process is complete, the new firmware revision is displayed in the dialog box.

Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.

Copyright © 2026 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please click here.
Trademarks not belonging to Rockwell Automation are property of their respective companies.