Release Notes
Kinetix 5500 Servo Drives: (2198-Hxxx)
Version 2.003 (released 6/2014)
Catalog Number Kinetix 5500 (2198-Hxxx) (series A)
These release notes describe version information for Kinetix 5500 (2198-Hxxx), version 2.003 (released 6/2014).
Features
This release includes the following system features.
Kinetix 5500 Servo Drives Version 2.003 Enhancement
Catalog Numbers:
2198-H003-ERS2
2198-H008-ERS2
2198-H015-ERS2
2198-H025-ERS2
2198-H040-ERS2
2198-H070-ERS2
Added support for Kinetix 5500 servo drives with integrated safety over the EtherNet/IP network. With integrated safety, the GuardLogix safety controller issues the safe torque-off (STO) command over the EtherNet/IP network and the 2198-Hxxx-ERS2 servo drive executes the command.
Corrected Anomalies in This Release
This release corrects the following anomalies.
Corrected: Version 2.003
Kinetix 5500 Servo Drives Version 2.003 Corrected Anomaly
Catalog Numbers:
2198-H003-ERS, 2198-H003-ERS2
2198-H008-ERS, 2198-H008-ERS2
2198-H015-ERS, 2198-H015-ERS2
2198-H025-ERS, 2198-H025-ERS2
2198-H040-ERS, 2198-H040-ERS2
2198-H070-ERS, 2198-H070-ERS2
Nuisance precharge failure faults when cycling control power with residual voltage on the DC bus.
(Lgx00150715)
Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.
Copyright © 2026 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please
click here.Trademarks not belonging to Rockwell Automation are property of their respective companies.