Release Notes
1789-Lx Controller
Version 23.00.00 (released 5/2014)
Catalog Number SoftLogix 5800
These release notes describe version information for SoftLogix 5800, version 23.00.00 (released 5/2014).
Security
This release includes security enhancements as a part of our ongoing efforts to improve security. For information regarding Rockwell Automation's vulnerability disclosure process, please reference the Rockwell Automation Vulnerability Policy.
Access Denied dialog box does not appear when users without FactoryTalk
Security access attempt to modify Motion Configuration (Lgx00184951)
Studio 5000 Logix Designer v29.00
Corrected Anomaly with Studio Logix Designer v30.00
When a user without Motion: Modify Configuration security credentials attempts to
modify the motion configuration, an Access Denied dialog box does not appear.
Requirements
This release has the following requirements.
SoftLogix Version 23 Compatible Software
Requirements First Identified as of Version 23
Catalog Numbers 1789-L10, 1789-L30, 1789-L60
Compatible software for SoftLogix 5800, version 23.00.00
|
FactoryTalk Services Platform |
2.61.00 (CPR9, SR6.1) |
|
FactoryTalk Activation Manager |
3.60.01 (CPR9, SR6.0) |
|
RSLinx Classic |
3.61.00 (CPR9, SR6.1) |
|
RSLinx Enterprise |
5.61.00 (CPR9, SR6.1) |
|
Studio 5000 with Logix Designer |
23.00.00 (CPR9, SR6.0) |
SoftLogix Version 23 System Requirements
Requirements
Catalog Numbers 1789-L10, 1789-L30, 1789-L60
Important: Treat the computer that is running the SoftLogix 5800 controller like
an industrial controller, not a personal computer. The SoftLogix 5800 controller
executes real-time operations. If you use other programs or applications on the
computer when the SoftLogix 5800 controller is executing real-time operations,
those operations may be disrupted.
Important: SoftLogix 5800 controllers and software do not support Integrated
Motion on the EtherNet/IP network. ControlNet and DeviceNet are supported in
SoftLogix 5800 controller, Version 20.00.00 and earlier.
When using a SoftLogix 5800 controller on a Microsoft Windows 7 operating
system, an Ethernet network is the only communication network supported. No
other communication modules are supported or should be used.
There are no drivers for Allen-Bradley PCI-based cards beyond the Windows XP operating system.
SoftLogix 5800, version 23
|
Category
|
Description
|
|
Personal computer
|
IBM-compatible Pentium 4 1.6 GHz or later
Other requirements include the following:
- FactoryTalk Activation Manager if you are currently using
Factory Activation software.
- A hard disk that supports bus mastering.
- The need for bus-mastering drivers for the personal
computer's chip set; for Intel motherboards, this software is called Application Accelerator.
- Applications that are resource-intensive, including
applications that use sequential, motion, and other local
applications running on the computer, may require a dual
CPU to achieve performance requirements.
- The Studio 5000 with Logix Designer application is not
required.
The SoftLogix 5800 controller has been tested and qualified
only on genuine Intel processors.
|
|
Operating systems
|
- Microsoft Windows 7 Professional (64-bit) with Service
Pack 1
- Microsoft Windows 7 Professional (32-bit) with Service Pack 1
- Microsoft Windows 7 Home Premium (64-bit) with Service
Pack 1
- Microsoft Windows 7 Home Premium (32-bit) with Service
Pack 1
- Microsoft Windows Server 2008 R2 Standard Edition with
Service Pack 1
The SoftLogix controller is not supported in virtualized environments. It is required that the SoftLogix controller be installed on a computer that is hosting one physical instance of the Windows operating system Do not install virtualization software on the same computer as the controller. Virtualization software affects computer timing which can result in unstable controller operation.
Important: When SoftLogix software is installed, the following
modules will be available in the Chassis Monitor:
- SoftLogix controller
- Soft ENBT
- Input/output simulator module
Important: Motion, ControlNet, and DeviceNet modules are
not supported in SoftLogix 5800 controllers, version 23.
|
|
RAM
|
1 GB, min
|
|
Hard disk space
|
64 MB of free hard disk space per controller instance (or more
based on application requirements)
|
|
Network
|
Supports EtherNet/IP via the Ethernet port of the personal
computer.
Third-party networks are supported through the Rockwell
Automation Encompass program.
|
|
Video
|
16-color VGA graphics adapter 640 x 480, or later resolution
(256-color, 800 x 600 min, for optimal resolution)
|
Known Anomalies in This Release
This release has the following known anomalies.
SoftLogix Version 23 Known Anomalies
Catalog Numbers 1789-L10, 1789-L30, 1789-L60
(Lgx00118782, Lgx00127537)
No Arithmetic Overflow Minor fault is seen in the SoftLogix software, but is seen in
a hard controller if you are passing parameters to an Add-On Instruction and the
source value exceeds the range of Add-On Instruction’
s parameter. For example,
if the Add-On Instruction input parameter type is SINT, and the source value
passed to the Add-On Instruction is 99999 (99999 exceeds the range of SINT, which is (-128 to 127), in a hard controller, you will see the overflow minor fault but
will not see the fault in the SoftLogix controller.
(Lgx00126929)
Repeated power cycling or resetting the Ethernet switch that connects the
Softlogix I/O module to the control system may cause the SoftLogix Ethernet
connections to not be re-established. Resolving this condition requires removing
the SoftLogix Ethernet module from the Chassis Monitor, and then re-insert the
Softlogix Ethernet module once the power to the Ethernet switch has been
restored.
(Lgx00136977)
When the MCR zone is disabled, all rungs inside the MCR zone are expected to
be disabled.
However, if the LBL instruction is used in a rung inside the disabled MCR zone, the
instructions after LBL in that rung will be enabled, which is incorrect.
(Lgx00114013)
SoftLogix 5800 controllers operate differently in integer calculations involving
XPY. Operands in XPY are converted to REAL before executing XPY.
Multiplication, however, is treated as an integer operation. The increased
precision in XPY may lead to discrepancy in behavior compared to using
multiplication.
(Lgx00107669, Lgx00107451)
The use of Windows Vista or Server operating systems does not result in an
expected EtherNet/IP configuration error.
If you are using the Windows XP operating system and have two EtherNet/IP
modules in the same chassis configured with the same IP address, an error is
indicated by a red X on top of the last EtherNet/IP module added to the SoftLogix
chassis configuration. This is the expected behavior for such a configuration
when any of the operating systems are used.
However, if you are using Windows Vista or Server operating systems, you can
configure two EtherNet/IP modules in one SoftLogix chassis with identical IP
addresses. This configuration should result in an error, but does not.
SoftLogix Version 23 Restrictions
Catalog Numbers 1789-L10, 1789-L30, 1789-L60
Using Alarms in SoftLogix (Lgx00136426)
Depending on the number of alarms in the program and the performance of the computer, if you request the computer to shut down, the SoftLogix controller may delay the shut down
process (3 minutes or longer for each controller in the virtual chassis) to save alarms information. During that time, the computer displays a `Shutting Down’
message.
If an improper computer shut down is performed, the integrity of the alarm records
cannot be guaranteed.
Known Anomalies from Previous Releases
These anomalies are from previous releases but are still known in this release.
PI Function Block (Lgx00070832)
Known Anomaly First Identified as of:
- 1756 ControlLogix® L6 Firmware Revision 16
- 1756 ControlLogix L7 Firmware Revision 19
- 1756 GuardLogix L6 Firmware Revision 16
- 1756 GuardLogix® L7 Firmware Revision 19
- 5370 CompactLogix™ L1 Firmware Revision 20
- 5370 CompactLogix L2 Firmware Revision 20
- 5370 CompactLogix L3 Firmware Revision 20
- 1789 SoftLogix™ Firmware Revision 20
The PI Function block appears to stop executing as the output does not change and instruction faults are logged.
If the PI instruction is being used in Linear mode, this floating-point equation is used to calculate the ITerm.
Due to the use of the single-precision floating point values, it may be possible, depending on the values of WLD and KP, for the ITerm value to be small enough, less than 0.0000001, to be lost when adding to the ITermn-1.
For more information regarding the PI
instruction, see the Logix5000™ Controllers Advanced Process Control and Drives
Instructions User Manual, publication 1756-RM006.
Logix CPU Security Tool
Known Anomaly First Identified as of Firmware Revision 20.011
RSLogix 5000™ Version 20.00
Studio 5000 Logix Designer™ First Identified as of Version 21.00
Catalog numbers:
- 1756 ControlLogix® L6
- 1756 ControlLogix L7
- 1756 GuardLogix L6
- 1756 GuardLogix® L7
- 5370 CompactLogix™ L1
- 5370 CompactLogix L2
- 5370 CompactLogix L3
- 1789 SoftLogix™
Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.
Copyright © 2026 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please
click here.Trademarks not belonging to Rockwell Automation are property of their respective companies.