This release includes security enhancements as a part of our ongoing efforts to improve security. For information regarding Rockwell Automation's vulnerability disclosure process, please reference the Rockwell Automation Vulnerability Policy.
Improved Product Resiliency for Firmware Revision 12.001
Product improvements have been made to increase product resiliency to potentially disruptive activities. These enhancements have been verified not to affect product safety, performance, expected life, configuration, or operation of the product. Rockwell Automation recommends that you follow good Industrial Control System (ICS) security practices that include regular product updates. To maintain authenticity, obtain product updates and new releases directly from Rockwell Automation.
This release includes the following system features.
How Logix Ethernet Modules Handle Leading Zeros in IP Addresses
Product Updates and Replacements
When entering IP addresses, if you enter leading zeros in the module configuration screen or message configuration screen of the Logix programming software, they are removed by the software. However, the leading zeros are not removed if they are typed into an L5K import file or if they are typed directly into the message path string. Different versions of the Logix Ethernet module treat the leading zeros differently.
Leading zeros show in the I/O tree with the mouse tool tip when imported from an L5K file.
Leading zeros can be entered directly into the message path string tag.
These leading zeros cause some modules to interpret those numbers as octal. For example, 192.168.001.013 is interpreted as 192.168.1.11 (1 octal is equal to 1 decimal, and 13 octal is 11 decimal). This causes the connection attempt to be made to IP 192.168.1.11 instead of 192.168.1.13. If 192.168.1.11 is not there, then the result is a 16#0204 timeout error.
If the IP address is 192.168.001.090, for example, the Ethernet module returns an error 16#0312 Invalid Link Address instead because 90 is not a valid octal number.
The same goes for message instructions. A message instruction attempts to connect to the equivalent octal node. If the node is not there, a timeout error is generated. If the value is not a valid octal value (such as 090), a return error 16#0001 with extended error 16#0312 is generated.
The following modules interpret a leading 0 to mean an octal value.
The following modules ignore the leading zero and interpret the values as decimal.
The leading zeros can be removed to force decimal interpretation.
For more information and for how other Ethernet modules handle leading zeroes, see KB 623220.
Product Resiliency Improvement
System Feature Identified as of:
This release includes enhancements that are intended to improve product resiliency to potentially disruptive activities. These enhancements do not affect product safety, performance, expected life, configuration, or operation of the product. Rockwell Automation advises customers to follow good Industrial Control System (ICS®) security practices that include regular product updates. To be sure of authenticity, obtain product updates and new releases directly from Rockwell Automation.
Improved Messaging Performance
System Feature Identified as of:
With these modules, message performance has been improved over earlier versions.
This release corrects the following anomalies.
TCP Window Size (Lgx00145648)
Known Anomaly Identified as of:
If the application software that communicates with the module indicates a TCP window size of 0 when establishing the TCP connection, the module does not open the TCP connection.
This issue does not generally occur with standard software packages, but can occur when using MSG instructions and the open sockets feature of the module.
Replace Remote Module (Lgx00149145)
Corrected: Firmware Revision 10.007
Known Anomaly as of Firmware Revision 10.006
Catalog Number 1756-EN2T, 1756-EN2T, 1756-EN2TXT Series D
When you replace a 1756-EN2T module in a remote chassis (there is no controller in the chassis that communicates through the 1756-EN2T), the module does not respond to requests. This lack of response is because the Ethernet switch does not recognize that another MAC ID is on the port of the switch.
Cycle power to the switch to correct the issue.
This release has the following known anomalies.
Connection drop between controller and 1756 Ethernet module during cable break
Corrected Anomaly with Firmware Revision 10.010
Known Anomaly First Identified as of Firmware Revision 10.007
Catalog Numbers:
Following a cable break and reconnection of the CompactLogix™ 5370 controller, it cannot communicate with the 1756 Ethernet module (Lgx00210701). Workaround is to cycle power or manually disconnect and reconnect the controller to re-establish communication.
Rack-optimized Connections Can Cause an Ethernet Module to Assert (1186272, 1186282, 942336)
|
Communication Modules
|
First Known in Firmware Revision
|
Corrected in Firmware Revision
|
|
1756-EN2T, 1756-EN2TR
|
10.007
|
12.001 and later
|
|
1756-EN3TR
|
10.007
|
12.001 and later
|
|
1756-EN4TR,
1756-EN4TRK,
1756-EN4TRXT |
2.001
|
4.001
|
Five or more rack-optimized connections that are targeted to an Ethernet module cause the module to assert immediately. The module status display shows ‘RackInput.cpp LineXXX’ information in the assert message.
These anomalies are from previous releases but are still known in this release.
Known Anomaly Identified as of:
When a Cisco switch with IP Device Tracking enabled (Cisco IOS firmware that is released after August 2013) is used within the layer 2 broadcast domain, the following can occur:
For more information, see Tech Note 568750. The Tech Note is available at https://rockwellautomation.custhelp.com/app/answers/detail/a_id/568750. A separate login is required.
By default, Stratix™ Ethernet switches do not exhibit this behavior.
Corrected: Revision 10.010
When you install RSLinx® Classic software, the EDS files for these modules are not necessarily available. You can use RSLinx Classic software to upload EDS files from the module or download EDS files from the Product Compatibility and Download Center website, http://www.rockwellautomation.com/global/support/pcdc.page.
Corrected: Revision 10.010
You can get an error if you use a MSG instruction to send emails through the module when communicating with a SMTP server. If an error occurs, the error string that is reported in the MSG instruction is missing the first four characters.
Not Valid Device Error
Known Anomaly Identified as of:
In the Studio 5000 Logix Designer® application, a Not Valid Device error can occur. This error occurs when you change the module type from one of the previously listed modules to any of the other listed modules in the Change Type dialog box.
|
Device
|
First Known in
Firmware Revision
|
Corrected in Firmware Revision
|
|
CompactLogix® 5380
|
28.011
|
34.014, 35.013, 36.011 and later
|
|
Compact GuardLogix® 5380 SIL 2
|
31.011
|
34.014, 35.013, 36.011 and later
|
|
Compact GuardLogix 5380 SIL 3
|
32.013
|
34.014, 35.013, 36.011 and later
|
|
CompactLogix 5380 Process
|
33.011
|
34.014, 35.013, 36.011 and later
|
|
CompactLogix 5480
|
32.011
|
34.014, 35.013, 36.011 and later
|
|
ControlLogix® 5580
|
28.011
|
34.014, 35.013, 36.011 and later
|
|
GuardLogix 5580
|
31.011
|
34.014, 35.013, 36.011 and later
|
|
ControlLogix 5580 Process
|
33.011
|
34.014, 35.013, 36.011 and later
|
|
1756-EN4TR
|
2.001
|
6.001 and later
|
|
1756-EN3TR/B, 1756-EN2TR/C
|
10.007
|
12.001 and later
|
|
1756-EN2TP
|
10.020
|
12.001 and later
|
|
1756-EN2T/D
|
10.006
|
12.001 and later
|
|
1756-EN2F/C
|
10.009
|
12.001 and later
|
|
Module
|
First Known in
Firmware Revision
|
Corrected in
Firmware Revision
|
|
1756-EN4TR, 1756-EN4TRXT
|
4.001
|
8.011 and later
|
|
1756-EN2T, 1756-EN2TXT, 1756-EN2TR
|
2.007
|
—
|
CPU Utilization Error (00179391)
Corrected Anomaly with Firmware Revision 11.001
Known Anomaly First Identified in Catalog Numbers:
When accessing Web pages, CPU utilization is 100%.
Increased ICMP message per second capacity (00191724)
Corrected Anomaly with Firmware Revision 11.001
Known Anomaly First Identified in Catalog Numbers:
ICMP message per second capacity increased.
Ethernet module sends incorrect ARP at switchover (00194847)
Corrected Anomaly with Firmware Revision 11.001
Known Anomaly First Identified in Catalog Numbers:
Ethernet module sends Address Resolution Protocol (ARP) to gateway address with source IP 0.0.0.0 at ControlLogix Redundancy switchover.
GoAhead Web Server Vulnerabilities – EtherNet/IP Communication Devices (1693483)
|
Product
|
First Known in Firmware Revision
|
Corrected in Firmware Revision
|
|
1747-AENTR
|
2.002
|
--
|
|
1769-AENTR
|
1.001
|
1.003 and later
|
|
1756-EN2T/D
|
10.006
|
11.002 and later
|
|
1756-EN2TR/C
|
10.007
|
11.002 and later
|
|
1756-EN2TSC/B (discontinued)
|
10.01
|
--
|
|
5069-AEN2TR (discontinued)
|
3.011
|
--
|
|
Product
|
First Known in Firmware Revision
|
Corrected in Firmware Revision
|
|
1747-AENTR
|
2.002
|
--
|
|
1769-AENTR
|
1.001
|
1.003 and later
|
|
1756-EN2F/C
|
11.001
|
11.002 and later
|
|
1756-EN2T/D
|
11.001
|
11.002 and later
|
|
1756-EN2TP
|
11.001
|
11.002 and later
|
|
1756-EN2TR/C
|
11.001
|
11.002 and later
|
|
1756-EN2TSC/B (discontinued)
|
10.01
|
--
|
|
5069-AEN2TR (discontinued)
|
3.011
|
--
|
|
1756-EN3TR/B
|
11.001
|
11.002 and later
|
For a full list of the potentially affected Rockwell Automation products and a description of the vulnerabilities and additional mitigations, see Knowledgebase Product Notice, CVE-2019-5096 and CVE 2019-5097 Vulnerabilities Impact Multiple Products.
MNRF/Assert can Occur on a Module After RCP Switchover (1955194)
|
Communication Modules
|
First Known in Firmware Revision
|
Corrected in Firmware Revision
|
|
1756-EN2T/D
|
10.006
|
12.001 and later
|
|
1756-EN2TR/C
|
10.007
|
12.001 and later
|
|
1756-EN3TR/B
|
10.007
|
12.001 and later
|
|
1756-EN2F/C
|
10.009
|
12.001 and later
|
|
1756-EN2TP/A
|
10.020
|
12.001 and later
|
After a switchover due to a cable break, the redundant system may not recover to a synchronized state. This can lead to the module experiencing a major nonrecoverable fault/assert.
A ReadSocket Service Request of the TCP/IP Socket Object Returns Incorrect Values (3096193)
|
Communication Modules
|
First Known in Firmware Revision
|
Corrected in Firmware Revision
|
|
1756-EN2T/D
|
10.006
|
12.001 and later
|
|
1756-EN2TR/C
|
10.007
|
12.001 and later
|
|
1756-EN3TR/B
|
10.007
|
12.001 and later
|
|
1756-EN2F/C
|
10.009
|
12.001 and later
|
|
1756-EN2TP/A
|
10.020
|
12.001 and later
|
When a Socket Object instance is used for a TCP connection, the response to a ReadSocket service request returns 0 for the Family, Port, and IP address.
Incorrect Product Type String in EDS files (3297343)
|
Communication Modules
|
First Known in Firmware Revision
|
Corrected in Firmware Revision
|
|
1756-EN2T/D
|
10.006
|
12.001 and later
|
|
1756-EN2TR/C
|
10.007
|
12.001 and later
|
|
1756-EN3TR/B
|
10.007
|
12.001 and later
|
|
1756-EN2F/C
|
10.009
|
12.001 and later
|
|
1756-EN2TP/A
|
10.020
|
12.001 and later
|
The ProdTypeStr keyword in EDS files had the incorrect value of ‘Communication Module’. The correct value is ‘Communications Module’.
Module does not get IP Address Assigned from a DHCP Server (2188094, 2233611)
|
Modules
|
First Known in Firmware
Revision
|
Corrected in Firmware
Revision
|
|
CompactLogix™ 5370
|
20.011
|
36.011
|
|
Compact GuardLogix®
5370
|
28.011
|
36.011
|
|
1756-EN2F
|
5.028 (Signed)
2.005 (Unsigned)
|
12.001 and later
|
|
1756-EN2T
|
5.028 (Signed)
|
12.001 and later
|
|
1756-EN2TP
|
10.020
|
12.001 and later
|
|
1756-EN2TR
|
5.028 (Signed)
1.003 (Unsigned)
|
12.001 and later
|
|
1756-EN3TR
|
5.028 (Signed)
3.004 (Unsigned)
|
12.001 and later
|
|
1756-ENBT
|
1.061
|
—
|
|
1768-ENBT
|
1.003
|
—
|
This anomaly was due to a change in the Dynamic Host Configuration Protocol (DHCP) standard, RFC 6842. This anomaly results in the module not being able to obtain an IP address through DHCP with some Stratix® switches that follow the updated standard.
For more information, see Knowledgebase Technote Some Ethernet devices do not obtain DHCP lease from Stratix 5800 as DHCP Server.
IP Address is Manually Configurable in DHCP Mode (1665460)
|
Communication Modules
|
First Known in Firmware Revision
|
Corrected in Firmware Revision
|
|
1756-EN2T/D
|
10.006
|
12.001 and later
|
|
1756-EN2TR/C
|
10.007
|
12.001 and later
|
|
1756-EN3TR/B
|
10.007
|
12.001 and later
|
|
1756-EN2F/C
|
10.009
|
12.001 and later
|
|
1756-EN2TP/A
|
10.020
|
12.001 and later
|
When a module is in DHCP mode, attempts to change the IP address manually are accepted, but the actual address remains the same.
Incorrect Delay Before Sending a Response to a Broadcast ListIdentity Request (1592443)
|
Communication Modules
|
First Known in Firmware Revision
|
Corrected in Firmware Revision
|
|
1756-EN2T/D
|
10.006
|
12.001 and later
|
|
1756-EN2TR/C
|
10.007
|
12.001 and later
|
|
1756-EN3TR/B
|
10.007
|
12.001 and later
|
|
1756-EN2F/C
|
10.009
|
12.001 and later
|
|
1756-EN2TP/A
|
10.020
|
12.001 and later
|
A module responds immediately to broadcast ListIdentity requests instead of delaying for a random period before responding.
PTP Announce Messages Have Incorrect PTP_TIMESCALE Value (1428782)
|
Communication Modules
|
First Known in Firmware Revision
|
Corrected in Firmware Revision
|
|
1756-EN2T/D
|
10.006
|
12.001 and later
|
|
1756-EN2TR/C
|
10.007
|
12.001 and later
|
|
1756-EN3TR/B
|
10.007
|
12.001 and later
|
|
1756-EN2F/C
|
10.009
|
12.001 and later
|
|
1756-EN2TP/A
|
10.020
|
12.001 and later
|
When a module is in the same chassis as the PTP Grandmaster, it sends PTP Announce Messages with an incorrect value for PTP_TIMESCALE.
Invalid IP Subnet Mask Allowed on Module (1418381)
|
Communication Modules
|
First Known in Firmware Revision
|
Corrected in Firmware Revision
|
|
1756-EN2T/D
|
10.006
|
12.001 and later
|
|
1756-EN2TR/C
|
10.007
|
12.001 and later
|
|
1756-EN3TR/B
|
10.007
|
12.001 and later
|
|
1756-EN2F/C
|
10.009
|
12.001 and later
|
|
1756-EN2TP/A
|
10.020
|
12.001 and later
|
The module does not check the validity of the subnet mask; therefore, an invalid subnet mask can be set on the module.
This release has the following functional changes from the previous release.
Functional Change Identified as of:
·Firmware Version 10.006, 1756-EN2T, 1756-EN2TXTSeries D
·Firmware Version 10.007, 1756-EN2TR, 1756-EN2TRXT Series C
·Firmware Version 10.007, 1756-EN3TRSeries B
·Firmware Version 10.009,1756-EN2F Series C
With these modules,when the switches are set to 888 to do an out-of-box reset, the module does not become active on the backplane, and other modules do not recognize when the module has been inserted.
Also, when these moduleswith switches set to 888are inserted in the primary chassis of a qualified redundant chassis pair, a switchover does not occur.
Exact Match Keying and Firmware Supervisor
Functional Change Identified asof:
·FirmwareVersion 10.006, 1756-EN2T, 1756-EN2TXTSeries D
·FirmwareVersion 10.007, 1756-EN2TR, 1756-EN2TRXT Series C
·FirmwareVersion 10.007, 1756-EN3TRSeries B
·FirmwareVersion 10.009,1756-EN2F Series C
Functional Change Identified as of Redundancy Bundle Versions 16.081 Enhanced
Firmware Versions 2.007,1756-EN2T, 1756-EN2TXT
Important: Series D modules come with firmware version 10.006, and cannot be used with earlier firmware versions.
When you use rotary switches for setting an IP address, modules with firmware version 2.007 default to gateway address 0.0.0.0. When you use the series D module, firmware version 10.006, the default gateway address is 192.168.1.1. This change impacts redundant systems. For more information, refer to ControlLogix Enhanced Redundancy System User Manual, publication 1756-UM535.
I/O in Redundancy Bundle Version 16.081
Functional Change Identified as of: Redundancy Bundle, Version 16.081
Firmware Version 10.006,1756-EN2T, 1756-EN2TXT Series D
Important: Series D modules come with firmware version 10.006, and cannot be used with earlier firmware versions.
Using the Series Dmodule to control I/O with redundancy bundle 16.081 is not supported or tested.
Functional Change Identified as of Firmware Version 10.006
Catalog Number 1756-EN2T, 1756-EN2TXT Series D
Important: Series D modules come with firmware version 10.006, and cannot be used with earlier firmware versions.
The existingmodule specification sheet does list the module as SIL2 certified; however, new polices put in place by TUV require that only the 1756-EN2TR modules be used for SIL2 applications as part of the safety loop.
For more information on configurations for SIL2 applications, refer to Using ControlLogix in SIL 2 Applications Reference Manual, publication 1756-RM001.
Functional Change Identified as of Firmware Version 10.006
Catalog Number 1756-EN2T, 1756-EN2TXT Series D
Important: Series D modules come with firmware version 10.006, and cannot be used with earlier firmware versions.
Firmwareversion 2.007 defaults to having PTP enabled. All later versions default to disabled. If youreplaceversion 2.007 withversion 10.006, PTP will be disabled, which may affect the application.
Functional Change Identified as of Firmware Version 10.006
Catalog Number 1756-EN2T, 1756-EN2TXT Series D
Important: Series D modules come with firmware version 10.006, and cannot be used with earlier firmware versions.
The module, firmware version 2.007, uses PTP version 1 on the backplane, while the series D module, firmware version 10.006, uses PTP version 2. These versions are incompatible on the backplane. When you replace a module at firmware version 2.007 in a chassis, replace all other modules in the backplane at firmware version 2.xxx.
Functional Change Identified as of:
·Firmware Version 10.006, 1756-EN2T, 1756-EN2TXTSeries D
·Firmware Version 10.007, 1756-EN2TR, 1756-EN2TRXT Series C
·Firmware Version 10.009,1756-EN2F Series C
These modules are not supported in all redundancy bundles. See the Product Compatibility and Download Center for updated information on which redundancy bundles include these modules.
RSLogix 5000 Software Support
Functional Change Identified as of:
·Firmware Version 10.006, 1756-EN2T, 1756-EN2TXTSeries D
·Firmware Version 10.007, 1756-EN2TR, 1756-EN2TRXT Series C
·Firmware Version 10.007, 1756-EN3TRSeries B
·Firmware Version 10.009,1756-EN2F Series C
When using RSLogix 5000 software, version 16.00, choose Compatible Keying when you are using redundant modules.
See the table below for RSLogix 5000 software version support information, including Add-on Profile information.
|
Catalog Number
|
Minimum RSLogix 5000
Software Version
Supported
|
Minimum RSLogix 5000 Software
Version With Add-on Profile
Supported
|
| 1756-EN2T/D
1756-EN2F/C
|
15.00
|
18.00
|
|
1756-EN2TR/C
|
17.00
|
17.00 (versions 17.00 or earlier do
not have RSNetWorx software
integrated. Versions 18.00 and later
have RSNetWorx softwareintegrated)
|
|
1756-EN3TR/B
|
18.00
|
18.00 (supports RSNetWorx software
integration in all releases)
|