This release has the following requirements.
Hardware Requirements v21
The personal computer must meet these minimum requirements. Using a computer meeting the recommended characteristics will improve performance.
|
Characteristic
|
Minimum Required
|
Recommended
|
|
Processor
|
Pentium 4
|
Intel Core i5
|
|
Speed
|
2.8 GHz
|
2.8 GHz
|
|
RAM Memory
|
2 GB
|
8 GB
|
|
Hard Disk Space
|
16 GB free
|
20 GB free
|
|
Graphics Device
|
DirectX 9, with WDDM
1.0 or higher driver
|
DirectX 9, with WDDM
1.0 or higher driver
|
Installation Notes
Review these notes before attempting to install this version of the Studio 5000 Engineering and Design Environment.
Prior to Installation
Keep the following considerations in mind before you install the Studio 5000 Engineering and Design Environment:
Installing one of the following software versions:
· Logix Designer application v21
· RSNetWorx v21
· RSLinx v3.51
· Add-On Profiles using Core 9.0
· DeviceNet Tag Generator
will cause prior versions of RSNetWorx and the DeviceNet Tag Generator to become inoperable.
Important: During the installation of Logix Designer application, version 21.03, the installation stops and a dialog box opens if an incompatible version of RSNetWorx software is detected on the PC. Upgrade RSNetWorx software to version 21 or uninstall it from your PC, and restart the Studio 5000 Engineering and Design Environment installation.
Installing the Software
Follow these steps to install the Studio 5000 Engineering and Design Environment.
The DVD-ROM should auto-start. If it does not auto-start, run Setup.exe from the root of the DVD.
The Studio 5000 Engineering and Design Environment supports multiple versions of the programming software on a single personal computer. With version 10 and later of the application, you may install as many of the later major versions as needed plus one version earlier than version 10 (for example, version 8.02).
Note that the Studio 5000 Engineering and Design Environment version 21 may need to update several system files early in the installation process. These updates will likely require you to restart your personal computer. Be sure to close all other applications before clicking OK to initiate this reboot.
When prompted for a serial number, enter the 10-digit serial number identifying your software license; otherwise, enter any sequence of characters, not longer than 10 characters.
Important: The 10-digit serial number is used to determine what functionality to enable while in Grace Period mode. Entering an invalid serial number will result in the application operating in Service Edition mode, upload and download only, while in Grace Period mode.
Important: When a valid activation cannot be located by the application, the application will enter a seven-day activation grace period, during which you will be able to run the application with full functionality. If this seven-day grace period ends before a valid activation has been found, you will no longer be able to start the Logix Designer application.
When the setup utility finishes, an entry for the Studio 5000 Engineering and Design Environment appears in the program list in the Rockwell Software group.
Starting the Studio 5000 Engineering and Design Environment
To start the Studio 5000 Engineering and Design Environment, from the Start menu, choose All Programs>Rockwell Software>Studio 5000 from the menu.
If Studio 5000 Engineering and Design Environment does not start up or run properly, keep the following in mind:
Uninstalling the Software
Follow these steps to uninstall the software when using the default Start menu on the Windows 7 or Windows Server 2008 operating system.
(for Windows 7, Windows Server 2008 R2) From the Programs category, choose Uninstall a program.
(for Windows Server 2008 – Control Panel Home) From the Programs category, choose Uninstall a program.
(for Windows Server 2008 – Classic View) Double-click Programs and Features.
Note: This will uninstall only the Studio 5000 Engineering and Design Environment. Other components that were installed with the Studio 5000 Engineering and Design Environment (such as Start Page Media, Online Books, or RSLinx) must be uninstalled separately.
Software Requirements Product Considerations v21
Software Requirements v21
Operating system and service pack compatibility:
This release includes the following system features.
Kinetix 5500 CIP-Motion Servo Drives
Software Feature
Firmware Revision/ Software Version 21
Kinetix 6000M Integrated Drive-Motor systems
Software Feature
Firmware Revision/ Software Version 21
Studio 5000 Engineering and Design Environment and Logix Designer Application
Software Feature
Firmware Revision/ Software Version 21
Version 21 of the application is the first release that re-brands RSLogix 5000 software to Logix Designer application, and embeds the Logix Designer application as a key component of Studio 5000 Engineering and Design Environment. The Studio 5000 Engineering and Design Environment is the new launch point for components of the integrated architecture, providing the infrastructure to share data, share design time components, and share runtime components between traditionally independent automation development tasks.
Project Documentation Stored in Controller
System Feature
Firmware Revision/ Software Version 21.011
Catalog Numbers 1769-L16ER-BB1B, 1769-L18ER-BB1B, 1769-L18ERM-BB1B, 1769-L24ER-QB1B, 1769-24ER-QBFC1B, 1769-L27ERM-QBFC1B, 1769-L30ER, 1769-L30ERM, 1769-L30ER-NSE, 1769-L33ER, 1769-L33ERM, 1769-L36ERM
CIP-Sync Enabled Logix (1756) and Armor-Block (1732E), SOE-Input and Scheduled-Output Modules
Software Feature
Firmware Revision/ Software Version 21
Pre-scan of Add-On Instruction Behavior
System Feature
Firmware Revision/ Software Version 21.011
Catalog Numbers 1769-L16ER-BB1B, 1769-L18ER-BB1B, 1769-L18ERM-BB1B, 1769-L24ER-QB1B, 1769-24ER-QBFC1B, 1769-L27ERM-QBFC1B, 1769-L30ER, 1769-L30ERM, 1769-L30ER-NSE, 1769-L33ER, 1769-L33ERM, 1769-L36ERM
You can access the Rockwell Automation Knowledgebase at: http://www.rockwellautomation.com/rockwellautomation/support/overview.page?
HMI Connectivity and Performance Improvements
System Feature
Firmware Revision/ Software Version 21.011
Catalog Numbers 1769-L16ER-BB1B, 1769-L18ER-BB1B, 1769-L18ERM-BB1B, 1769-L24ER-QB1B, 1769-24ER-QBFC1B, 1769-L27ERM-QBFC1B, 1769-L30ER, 1769-L30ERM, 1769-L30ER-NSE, 1769-L33ER, 1769-L33ERM, 1769-L36ERM
For more information, see the Logix5000™ Data Access Programming Manual, publication 1756-PM020.
Extended Tag Properties
System Feature
Firmware Revision/ Software Version 21.011
Catalog Numbers 1769-L16ER-BB1B, 1769-L18ER-BB1B, 1769-L18ERM-BB1B, 1769-L24ER-QB1B, 1769-24ER-QBFC1B, 1769-L27ERM-QBFC1B, 1769-L30ER, 1769-L30ERM, 1769-L30ER-NSE, 1769-L33ER, 1769-L33ERM, 1769-L36ERM
This release corrects the following anomalies.
Corrected: Studio 5000 21.03
Anomaly
Studio 5000 21.00
During the installation of Studio 5000 Engineering and Design Environment, an error occurs when you enter an alpha numeric serial number.
Corrected: Logix Designer 21.03
Anomaly
Logix Designer 21.00
Logix Designer application, version 21, has optimized the EDS subsystem, which causes a compatibility issue with early versions of RSNetWorx software. During the installation of Logix Designer application, the installation stops and a dialog box opens if an incompatible version of RSNetWorx software is detected on the PC. You need to upgrade RSNetWorx software to version 21 or uninstall it from your PC, and then restart the Studio 5000 Engineering and Design Environment installation.
Corrected: Logix Designer 21.03
Anomaly
Logix Designer 21.00
When downloading a project with nested Add On Instruction routines, an "Invalid data type. Argument must match parameter data type" error occurs when Logix Designer application attempts to link the routines. This occurs when one of the Add On Instructions has a Function Block IREF element that contains a tag with a boolean member that is an alias to a user defined data type's boolean member.
These anomalies are from previous releases but are still known in this release.
Corrected: Logix Firmware/RSLogix 5000 Software 19.11
Watchdog Fault During Prescan (Lgx00113376, Lgx00112413)
Anomaly
Logix Firmware/RSLogix 5000 Software 18.11
Catalog Numbers 1756-L61, 1756-L61S, 1756-L62, 1756-L62S, 1756-L63, 1756-L63S, 1756-L63XT, 1756-L64, 1756-L65, 1756-L72, 1756-L73, 1756-L74, 1756-L75
A watchdog fault occurs during prescan on a transition from Program mode to Run mode.
In large applications that include elements, such as many Add-On Instructions, Add-On Instructions with defined prescan routines, and complex Structured Text routines, the prescan could exceed 60 seconds. Because 60 seconds was the prescan watchdog setting, the controller experienced a major recoverable fault.
To correct this anomaly, the prescan watchdog has been changed to 300 seconds.
IMPORTANT: You cannot configure the prescan watchdog value.
Corrected
Blank Primary Window (Lgx0039239)
Anomaly
RSLogix 5000 Software 16.x
If you have a primary help window displayed and you open a help topic which displays a secondary window, the primary window may become blank. This is the result of a problem with the Windows Help compiler. To display the original topic, click Help Topics and re-select the original topic.
Project Re-Verification Operations (Lgx00033403)
Corrected Anomaly
RSLogix 5000 Software 16.x
If you perform an operation that requires re-verification of the entire project (e.g. changing the controller type, compacting the database, or importing) the operation will complete successfully but may take an extended amount of time. Projects with FBD routines with large blocks (many visible parameters) and numerous input and output references are particularly sensitive to this re-verification time. The amount of time will vary depending on the complexity and size of the project.
Unicode Characters, Does Not Display (Lgx00063773)
Anomaly
RSLogix 5000 Software 16.x
When the description of a task, program, routine, module, trend, etc. is edited, any audit records displayed using RSMACC Audit will not properly display Unicode characters.
Inserting Unicode Characters (Lgx00059649, Lgx00059650, Lgx00059825)
Anomaly
RSLogix 5000 Software 16.x
RSLogix 5000 employs a feature which allows the user to position the caret on an edit control and, without explicitly opening the edit control, to begin entering character data from the keyboard. This action will cause RSLogix 5000 to automatically open that edit control as character data entry continues. For many of the edit controls in RSLogix 5000, using this auto-open feature when inputting Unicode characters using an Input Method Editor (IME) will result in unexpected behavior or in a Fatal Error.
To avoid this Fatal Error when entering Unicode characters, the edit control should be explicitly opened before beginning to enter character data from the keyboard. In most cases, pressing [Enter] on the keyboard will open the edit control which has the caret. In other cases, a single click or double click of the mouse is required.
When using an IME to input Unicode characters, if the small IME character input dialog appears in the upper left corner of the display, then you have started to input a Unicode character string with no edit control opened. When this occurs, you can press [Esc] on the keyboard to cancel the input and then open the desired edit control before entering the Unicode character string.
Hardware Overtravel Fault (x66998)
Anomaly
RSLogix 5000 Software 16.x
For Kinetix 6000 axes configured in RSLogix 5000, if you have both Soft Overtravel and Hardware Overtravel Limits enabled, and you configure the Soft Overtravel Fault Action as "Status Only", be aware that a Hardware Overtravel Fault Action configured for "Stop Motion" may not "Stop Motion" due to the two faults existing together and the first fault action being set to "Status Only". For more information refer to Technical Note: ID=36709 "2094 Kinetix 6000; Soft Overtravel triggers first then sequential hard overtravel does not stop motion", and Technical Note: ID=21500 "How do I get off a Soft Overtravel?"
Unable to Enable Security (x107466)
Anomaly
RSLogix 5000 18.x
The SetSecKeys tool included with RSLogix 5000 software version 17 and earlier do not work with User Account Control (UAC) turned on. When a SetSecKeys tool earlier than file version 18.0.0.0 is executed with UAC turned on, security appears to be enabled, yet security remains disabled in RSLogix 5000 software. If a version of SetSecKeys earlier than file version 18.0.0.0 is used inadvertently, SetSecKeys file versions 18.0.0.0 and later can still be used to enable security. (Note that depending on the operating system, the file version of SetSecKeys.exe can be viewed on either the Details tab or the Version tab of the File Properties dialog box.)
References In Program Logic Will Not Update (x125220)
Anomaly
RSLogix 5000 20.x
If a project for a CompactLogix controller that is no longer supported is imported as a controller that has expansion I/O, any expansion I/O modules from the original controller are properly moved to the correct expansion slot; however, the references in program logic will not be correspondingly updated. This does not necessarily result in the program failing to verify. Instead, the logic may now be referencing the embedded modules for this controller. This is a problem only when opening a L5K or L5X project file. The references are properly adjusted when opening an ACD file.
Windows 7 Operating Systems (x111504, x113166, v124864)
Anomaly
RSLogix 5000 19.x
There are a number of issues related to compatibility of RSLogix 5000 software with the Windows 7 operating system. The most significant of these includes the following:
New EDS File Not Displayed (Lgx00124959)
Anomaly
RSLogix 5000 20.x
When a new EDS file is registered from outside RSLogix 5000 software, when RSLogix 5000 software is not running and RSLinx Classic software is running as an application (as opposed to as a service), then the newly registered device will not be available in the Select Module Type dialog box. Note that there is no problem with display of the device when registered outside of RSLogix 5000 software, provided that you first exit the RSLogix 5000 application and shut down the RSLinx Classic application. There is also no problem with display of the device when registered from within the RSLogix 5000 application (such as when using the “ Tools>EDS Hardware Installation Tool” menu). So, if the registered module is not displayed, you can use the “ Tools>EDS Hardware Installation Tool” menu to register the device again.
XML Full Project (x114197)
Anomaly
RSLogix 5000 20.x
Unable to Open Full Project XML Format File (.L5X) for Project File of Later Version of RSLogix 5000 Software than is Being Executed.
When attempting to open a full project xml format file (.L5X), an error may be reported indicating "Controller Revision not supported". This will occur when the major revision of the xml format file being opened is later than the revision of RSLogix 5000 software being executed.
For example, when executing RSLogix 5000 software version 19, an attempt to open an xml format file for version 20 will report the error. However, when executing RSLogix 5000 software version 20, an attempt to open an xml format file for version 19 will not exhibit the problem. When this error is observed, first switch to the RSLogix 5000 software version for the xml format file, and then open the file. This problem does not affect L5K or ACD files. (x114197)
"Log On to FactoryTalk" Displayed (Lgx00124955)
Corrected Anomaly with Studio 5000 Logix Designer 24.01
Known Anomaly First Identified as of RSLogix 5000 20.x
When launching RSLogix 5000 software, the "Log On to FactoryTalk" dialog box may be displayed.
This dialog box may be seen when you do not have Administrator privileges on the personal computer and the current user does not exist in the FactoryTalk directory. If this dialog box is cancelled, the RSLogix 5000 software will not be launched. When the dialog box is displayed, entering the credentials for a user that exists in the FactoryTalk Directory will allow RSLogix 5000 software to be launched. Administrator accounts are included in the FactoryTalk Directory by default.
To avoid seeing this dialog box, you can add the current user or user group to the FactoryTalk directory. Follow these steps to add a user or user group to the FactoryTalk directory:
The "Log On to FactoryTalk" dialog bax may also be displayed when using Remote Desktop to connect to the personal computer that is running RSLogix 5000 software. This is due to FactoryTalk Security not recognizing the computer name. To enable access through Remote Desktop for a specific computer, you should add the name of the computer that is initiating the Remote Desktop connection to the "Network\System\Computers and Groups\Computers" folder in the FactoryTalk Administration Console. To allow remote computers to connect using the name of the host computer, open the FactoryTalk Administration Console and log in to the Network directory using your domain credentials. Then navigate to "Network\System\Policies\Security Policy". In the "Computer Policy Settings" section, set "Identify terminal server clients using the name of" to "Server Computer". To allow all computers to connect, set the value of "Require Computer accounts for all client machines" to disabled.
Note that if "Use single sign-on" is set to "disable" in FactoryTalk software, then the "Log on to FactoryTalk" dialog box will be displayed each time RSLogix 5000 software is launched and proper user credentials must be entered in order to continue. (By default, "Use single sign-on" is set to "enable".)
Slow Launch Times (x125369)
Anomaly
RSLogix 5000 Software 20.x
When RSLogix 5000 software is launched for the first time after restarting your personal computer, it may take 1 to 3 minutes for RSLogix 5000 software to be available for use. This behavior is also exhibited when launching FactoryTalk Administration Console or any other product that uses FactoryTalk Services Platform. Note that subsequent launches of these applications will not experience this behavior. This is only observed on the first launch of the application after a restart of the personal computer. If you experience launch times significantly longer than 3 minutes, refer to the firewall configuration settings in Tech Note #29402
Corrected: Logix Firmware/RSLogix 5000 Software 17.02 and 17.06
Analog or Digital Alarm InAlarmUnack Tag (Lgx00081999)
Anomaly
Logix Firmware/RSLogix 5000 Software 16.x
Catalog Numbers 1756-L61, 1756-L61S, 1756-L62, 1756-L62S, 1756-L63, 1756-L63S, 1756-L64
Acknowledging an analog or digital alarm does not clear the alarm's unacknowledged (InAlarmUnack) tag. If an alarm has an active status (InAlarm tag is true) and is unacknowledged (InAlarmUnack is true), acknowledging the alarm does not reset the alarm's unacknowledged tag (that is, even after being acknowledged, the InAlarmUnack continues to be true).
This anomalous behavior occurs with both digital (ALMD) and analog (ALMA) alarms.
Logix CPU Security Tool
Known Anomaly First Identified as of Firmware Revision 20.011
RSLogix 5000™ Version 20.00
Studio 5000 Logix Designer™ First Identified as of Version 21.00
Catalog numbers:
Corrected
Studio 5000 Logix Designer 21.00
An anomaly is present for tracking the change date of an Add-On Instruction that contains a user-defined data type (UDT). In Prior releases, when this embedded UDT had a modification of the UDT name, the Add-On Instruction it was embedded in would update its change date. In this current release, this has been noted to account for changes in individual members within the UDT as well as the description or comments for each member of the UDT. Now for any modification of the embedded UDT, the Add-On Instruction change date will reflect this modification and update its change date value. This anomaly is limited to the first nested layer of a UDT only. If a nested UDT is modified, then this modification will not be captured as a change date for the Add-On Instruction at this time.
This release has the following functional changes from the previous release.
Generic Ethernet Module Extensions
Software Enhancement
Firmware Revision/ Software Version 16
With version 16 of RSLogix 5000, the Generic Ethernet Module support that is used to interface Logix5000 to 3rd party devices via EtherNet/IP has been extended in a number of ways.
These extensions provide greater flexibility when using this configuration option and expand the functionality so that 3rd party devices can interact more readily with Logix5000.
Software Enhancement
Firmware Revision/ Software Version 21
This release has the following application notes.
Application Notes RSLinx Software v21
Logix Designer 21.x
Data access control compatibility with RSLinx software
In version 18 and later of the application, there is an External Access tag attribute, which defines how an external application can access a tag. This functionality is fully supported by RSLinx Classic software version 2.56 and RSLinx Enterprise software version 5.21. Version 18 and later of the application can be used with earlier versions of RSLinx Classic software to go online to a controller; however, earlier versions of RSLinx Classic or RSLinx Enterprise software should not be used as a data server with a controller running firmware revision 18 or later. Unexpected results will be observed when using an earlier version of RSLinx Classic or RSLinx Enterprise software as a data server with a controller running firmware revision 18 or later.
Please see Rockwell Automation Knowledgebase Tech Note #67071 (https://rockwellautomation.custhelp.com/app/answers/list).
Configuring the Ethernet port on a CompactLogix5532E controller
You are sometimes prevented from configuring the Ethernet Port of a CompactLogix5532E controller (catalog number 1769-L32E) via Channel 0 using RSLinx software. To work around the anomaly, use the Logix Designer application to configure the port (if the 1769-L32E controller is at revision 13) or use the BootP utility (which is enabled for a 1769-L32E controller at revision 1).
RSLinx Classic software Professional activation
Beginning with RSLinx Classic software version 2.31.00, the Logix Designer application Professional activation will also enable the RSLinx Classic Professional (RSLinx Classic OEM with version 16 and higher) version features. Only one professional activation is required for both products. The Logix Designer application Professional Activation must be installed on the personal computer hard disk in order to activate RSLinx Classic Professional (RSLinx Classic OEM with version 16 and higher).
Configuring drivers for the 1756-ENET, 1756-ENBT, and 1756-EWEB modules
You configure a driver for communicating from the workstation through the 1756-ENET, 1756-ENBT, or 1756-EWEB module by selecting Configure Drivers from the RSLinx Communications menu. In the dialog box, select Ethernet devices in the list of available driver types and click the Add New button.
If you are using RSLinx software version 2.40 or later, you can use the EtherNet/IP driver. This driver will automatically browse for all EtherNet/IP-capable devices on the local or configured remote subnet. See RSLinx Help for information on this driver. Note that 1756-ENET/A and 1756-ENET/B modules will not respond to the browse commands. You must use a different driver for these modules.
Configuring DF1 drivers
For DF1 point-to-point communications, choose RS232 DF1 Devices from the list of available drivers in RSLinx software. Then choose Logix5550 Serial Port for DeviceType. Rockwell Automation recommends that you do not use the DF1 Polling Master Driver or the DF1 Slave Driver with the Logix Designer application. You may be able to download successfully, but there are anomalies accessing information from I/O modules.
Offline tag and UDT Changes causing RSLinx software to halt communication
RSLinx software maintains knowledge of the memory layout of a Logix5000 controller in order to optimize the data access performance when accessing the data in these controllers. However, changes made to an offline project that are then downloaded can result in RSLinx software attempting to access tag information that is no longer present. When this occurs, RSLinx software halts the communications to the controller.
To recover, both RSLinx software and the software requesting tags from RSLinx software must be restarted. To avoid this anomaly, use caution when making offline changes to a project and then downloading to a Logix5000 controller. In particular:
Note that RSLinx Enterprise Series software is able to accommodate these changes without requiring a restart.
Third-party software with Logix Designer application
Data access control compatibility with third-party software
Some third-party data servers use un-tested data access methods not published in the Logix5000 Data Access manual. To assure controller integrity and overall system performance and reliably, Version 18 of RSLogix 5000 software only supported documented published methods for writes. Starting in Version 21 of the Logix Designer application, Logix controllers will only support published communications methods for both reads and writes. As a result, some third party data access packages may need to re-write or re-design their drivers to use a published communications method. Please see Rockwell Automation knowledgebase technical note 67071.
Application Notes v21
Logix Designer 21.x
The following information is provided to help you better understand the behavior of the Logix Designer in particular applications or under certain circumstances.
Product Resiliency Improvement
This release includes enhancements intended to improve product resiliency to potentially disruptive activities. These enhancements have been verified to not affect prodcut safety, performance, expected life, configuration, or operation of the product. Rockwell Automation advises customers to follow good Industrial Control System (ICS) security practices that include regular product updates. To ensure authenticity, obtain product updates and new releases directly from Rockwell Automation. Product resiliency includes, but is not limited to, security topics related to tamper prevention and detection, intellectual property management and source protection, and user authentication and authorization.
Offline interactions between minor versions
Starting with version 21.03, ACD projects converted to version 21.03 and later cannot be opened in prior versions.
Onlne interactions between controller and application
Starting with version 21.03,
Support of minor versions
The Logix Designer application only supports the installation of a single minor release of the application on a computer. Therefore, version 21.03 or later versions of the application CANNOT run on the same computer as Logix Designer application version 21.00.
In order to support a system that runs version 21.03 and version 21.00, leverage the use of separate computers or use virtualization.
Required to re-register EDS files after upgrading to version 20 or version 21 of the application
If the product described by the EDS file is to be used in the I/O configuration using EDS AOP, any EDS files that have been registered for RSLogix 5000 software version 19 and earlier must be re-registered after the installation of RSLogix 5000 software version 20 or later.
Resources cannot be found in the Online Books section of the Start Page
The Release History and Vendor Sample Project .pdf file will not display until http://localhost is added to the list of Trusted Sites in Internet Explorer.
Application crashes after importing the 1734-IB8 module
If you import the 1734-IB8 module into version 15 and later of the application, the application crashes. The workaround is to not import the 1734-IB8 module into the application. (x122918)
OpenRSLogix5000 command generates an error when trying to select Routine name
When you select a routine using the OpenRSLogix5000 command in FactoryTalk View, an error displays that tells you that RSLogix 5000 is not installed. To fix this issue, contact Technical Support to obtain a new revision directory dll.
Opening or creating data types causes the application to crash with older version of FTA
If FactoryTalk Activation version 4.0 or earlier is installed on your computer, opening or creating data types from the Controller Organizer causes the Logix Designer application to crash. To prevent this from happening, use FactoryTalk Activation version 4.1 with Logix Designer application version 21.
Download Project Documentation and Extended Properties
Your Logix Designer application project will not download in the following conditions:
To work around this restriction, check the Download Project Documentation and Extended Properties check box when configuring the project.
Download duration is slow for certain projects
Storing your project comments and tag descriptions in the controller increases upload/download times.
Be aware of the following:
To work around this restriction, clear the Download Project Documentation and Extended Properties check box when downloading the project.
IMPORTANT: Be aware that a restriction applies to clearing the Download Project Documentation and Extended Properties check box in a multi-workstation development application. (x135928)
Fatal error occur when attempt to go online with the controller
A false time stamp in the controller caused a fatal error to occur when you attempt to go online with the controller. Additionally, the application is not processing dates that are out of range when attempting to convert them to string format, which causes the application to crash.
Use the following workaround to correct the controller's time stamp.
Use the following workaround to correct the out of range dates.
It is critical to get the controller's time fixed. Otherwise, any new faults that are generated will also have false time stamps and will cause the controller to crash.
This will clear any major faults that exist. DO NOT attempt to do this from the Major Faults tab of the Controller Properties dialog box.
DO NOT attempt to clear minor faults from the Minor Faults tab of the Controller Properties dialog box.
At this point, the controller's time stamp should be corrected and all faults that captured false time stamps should be cleared or purged.
Note that there is also the option to remove the batteries and power cycle the controllers. This will likely reset the controller's time stamp back to Jan. 1, 1998. This solution requires you to take the controller offline.
Rockwell Automation suggests that you investigate how the controller's time is getting a false value so that the problem does not repeat itself. (x135741)
Indirect addressing within Add-On Instruction logic
If your project uses indirect addressing in an Add-On Instruction, you need to be aware of two compatibility items when using RSLogix 5000 software version 20.01 and Logix5000 controller firmware revision 20.012.
First, you should consider RSLogix 5000 software version 20.01 and Logix5000 controller firmware revision 20.012 to be lock stepped. This means that you should not use the following:
EvRSI replaced by FactoryTalk Activation Manager
Beginning with RSLogix 5000 software version 20, EvRSI activation has been replaced by the FactoryTalk Activation Manager utility. EvRSI activation will not be able to activate the Logix Designer application. If you are using EvRSI activation, please contact your local Rockwell Automation Sales office or Rockwell Automation Services & Support for information on migrating your activations to FactoryTalk Activation.
1769-L2y controllers cannot be properly configured
For 1769-L2y controller types, which were released in RSLogix 5000 software version 20, the Embedded Counters module cannot be properly configured for Pulse External Direction. This anomaly was corrected in version 20.01. 1769-L2y controllers can be properly configured by using the Logix Designer application. However, 1769-L2y projects created by using RSLogix 5000 software version 20.00 will continue to be configured incorrectly.
To correct the configuration, the controller must be recreated in the Logix Designer application. A convenient way to do this import is to use the File > Import Component feature of the Logix Designer application to import your logic from the version 20.00 project to the new version project. This affects the following controller types:
Out-of-Box CIP Axis Position Loop Gain values adjusted with Load Observer
With the introduction of the CIP Motion Load Observer enhancement in version 19 of RSLogix 5000 software, the out-of-box calculations for several CIP Axis attributes were impacted. In particular, the Position Loop Bandwidth attribute and the Position Error Tolerance attribute will be automatically adjusted when the Load Coupling is change from Rigid to Compliant and Use Load Ratio is enabled.
When a change to the Load Coupling is applied, the out-of-box Position Loop Bandwidth will be reduced by 90% and the out-of-box Position Error Tolerance will be increased by 90%. This has the effect of loosening the out-of-box Position Gains so that the Motion Load Observer loop response can be tightened.
Time Synchronization replaces CST Time Mastership
RSLogix 5000 software version 18 has replaced the concept of Coordinated System Time (CST) Mastership with the more comprehensive notion of Time Synchronization, also referred to as CIP Sync Time Coordination. The Date/Time page of the controller properties has been modified to reflect this change.
For projects created with RSLogix 5000 software version 17 or earlier, if Coordinated System Time Master (CST) is enabled, then the converted project will have the Time Synchronization setting enabled. For more information about time synchronization using CIP Sync Time Coordination, refer to the Integrated Architecture and CIP Sync Configuration Application Technique, publication IA-AT003.
Attribute Value not Settable reported using AutoFLASH from Logix firmware revision 20 to an earlier revision
When attempting to download a project by using RSLogix 5000 software version 19 or earlier, if the controller firmware is at revision 20 or later and the controller is in Remote Run mode, then the version 19 software will not be able to change the controller mode in order to AutoFLASH the controller with revision 19 firmware. In this case, the controller mode must be changed either by using the keyswitch or by using version 20 or later of the application. (x123924)
CIP Generic writes to controller objects that originate from another controller failing
In RSLogix 5000 software version 20, there are enhanced security restrictions to controller CIP objects. Because of this, some CIP Generic messages that are used to write directly to controller object attributes sometimes do not function. Any CIP generic object write that originates external to the controller sometimes fail in version 20 or later of the application. CIP Generic writes that are executed in the controller’ s own user program will operate normally.
Security permissions changed for program creation
In version 17 of RSLogix 5000 software, the FactoryTalk Security permissions required for creating scheduled programs have changed slightly. As before, to create an unscheduled program, you need permission for the Program: Create action. To create a program scheduled in a task, however, you now need permission for both the Program: Create and the Task: Modify Properties actions. To create a program scheduled in the Power-Up Handler or Controller Fault Handler, you now need permission for both the Program: Create and the Controller: Modify Properties actions. (x77816, x77817)
Testing SFC online edits no longer always requires chart to reset
With RSLogix 5000 software version 17 and earlier, when performing online editing operations in a Sequential Function Chart (SFC), switching the executing logic from the original programming to the test edits version (or vice versa) resets the chart to the initial step and resets all stored actions. Beginning with version 18.00 of RSLogix 5000 software, many SFC online edits no longer result in this reset. In general, only edits that alter the logic structure of the chart will require the SFC routine to be reset.
In cases when a reset is required, you can force the transition with the initial step to false, wait for the routine to execute to the initial step, and then perform the test/un-test operation followed by removal of the force. Also, you can leverage the SFC Reset (SFR) instruction to reposition the chart back to the desired step. (x36331, x43482)
Cannot create, view, or edit modules based on Classic Profile after McAfee QuickClean
McAfee virus software version 8.0 ships with a Quick Registry Cleaner component that cleans the registry on a periodic basis. Upon cleaning the registry, the McAfee software removes all existence of the application's classic profiles from the registry. Once this has occurred, you can no longer create, view, or edit any classic profile based module.
This anomaly will also prevent the creation and importing of projects. When this condition is encountered, it is necessary to uninstall and reinstall the application. A way to avoid the anomaly is to remove the registry cleaner from any QuickClean manual and scheduled scans or delete all scheduled QuickClean tasks from the McAfee SecurityCenter UI. (x81691)
L5X file list not filtered on Windows 7 operating system
When performing a Partial Import online, the list of files displayed on the Import dialog box is filtered to show only files of the selected component type (for example, program, routine, data type, equipment phase). This filtering is not supported by the Windows 7 operating system. The Import dialog box will therefore show all .L5X format files when running the Logix Designer application on a Windows 7 operating system. The icon and ToolTip for the component file will identify the file type. (x105789, x112515, x113267)
Adobe Reader error selecting Online Books from the Tools menu
After installing RSLogix 5000 software version 19, you may see the Tools>Online Books menu item. If this menu item is selected, Adobe Reader will report that "This file cannot be found." This error occurs when using version 19 or later of the application if RSLogix 5000 software version 18 had also been installed on the same personal computer.
The Online Books installed with version 18 software were accessed by using the Custom Tools Menu (Tools>Online Books). The Online Books installed with version 19 and later access the Online Books by using the Start Page Resource Center. With version 19 installed, the Custom Tools Menu item for version 18 Online Books remains on the Tools menu, but is no longer used. Once RSLogix 5000 software version 19 has been installed, the unused Online Books Custom Tools Menu item can be manually removed by:
Unknown URL attempting to access Online Books or Vendor Sample Projects from Start Page
If your personal computer is not configured as part of a domain, you sometimes receive the error message "Unknown URL" when attempting to access Online Books or Vendor Sample Projects from the Start Page. This is the result of security enhancements to the Internet Explorer browser.
If Logix Designer application was installed by using the default installation path, the Online Books can be accessed from links provided in the file C:\Program Files\Rockwell Software\RSLogix 5000\Common\<language>\Docs\top level linking.pdf or C:\Program Files (x86)\Rockwell Software\RSLogix 5000\Common\<language>\Docs\top level linking.pdf, and the Vendor Sample Projects can be accessed from links provided in the file C:\RSLogix 5000\Projects\Samples\<language>\<version>\Third Party Products\Vendor Sample Projects.pdf. Access to Online Books and Vendor Sample Projects can be allowed by adding localhost’ to the allowed Local Internet sites. (x89165)
Help from 32-bit .hlp files is not displayed
The Windows Help (WinHlp32.exe) program is used to display Help that is provided in 32-bit .hlp files. The Microsoft Corporation stopped including this 32-bit Help file viewer in Windows releases beginning with Windows Vista and Windows Server 2008 operating systems. Version 18 and later of the application display Help in HTML format and does not require this Windows Help program. However, some module profiles may continue to display Help by using 32-bit .hlp files.
To properly display Help that is provided in 32-bit .hlp files on a Windows Vista or later operating system, you need to install the Windows Help program. This application is available for download from the Microsoft Download Center. For additional information on downloading and installing the Windows Help program, refer to the Microsoft Knowledgebase article I cannot open Help files that require the Windows Help (WinHlp32.exe).
Start Pages will not work if version 16.00 is installed after other versions
If version 16.00 of RSLogix 5000 software is installed after version 17.00 or later, Start Pages will fail to load and the message "Server Startup Failure physicalPath=… " will be displayed. In order to restore Start Page functionality, it is necessary to re-install the version 17.00 or later. Note that this anomaly will not be observed for version 16.03 and later. (x76424)
Function Block Diagram (FBD) ActiveX Faceplates not compatible with Windows Vista or later
The FBD ActiveX faceplates are not compatible with Microsoft Windows Vista or later operating systems. Instead, use FactoryTalk View SE/ME FBD Global Objects, available with FactoryTalk View SE/ME software version 5.1 or later.
Overflow checking improved for Immediate Operand values
In RSLogix 5000 software version 20, overflow checking for immediate operand values has been extended to all radix formats. Earlier versions of RSLogix 5000 software checked Octal values (that is, 8#nnn) for overflow into a 32-bit integer. Starting with RSLogix 5000 software version 20, immediate operand values of any integer-type radix (Hexadecimal, Decimal, Octal, or Binary) are checked for overflow into a 32-bit integer. The overflow conditions are indicated as errors during the verification process. (x116816)
First use of Drive profile when Add-On Profiles not installed requires media access
When a drive profile is first accessed, any user other than the user who installed the Drives Add-On Profiles version 4.02 or earlier will need access to the install media. When accessing the drive profile either by importing a project or by creating a drive in the I/O configuration tree, the user will be prompted with the following: "Enter an alternate path to a folder containing the installation package „RADrives_PF7.msi ”. ” The user must then provide the path on the installation media to ...\ENU\MP\RADrives\RADrives_PF7.msi. These Add-On Profiles may have been installed either separately or as part of the installation of RSLogix 5000 software version 20.01. (x128249)
Manual Tune fields active when Servo disabled
In version 20 or later, the Manual Tune parameters are enabled and editable when online for either the On or Off setting for the Servo parameter of a CIP_AXIS_DRIVE axis type. (x122492)
Motion instruction error for Stop_All or MGS Active and Pending Motion instruction
A new motion instruction error has been incorporated in version 17 of RSLogix 5000 software: error code 78 - Not Allowed While Stopping. In addition, an expanded meaning has been incorporated for error code 7 - Shutdown State Error. These errors will now be generated whenever an MGS, MAS=All, or MCS=All is active and a second motion instruction is then executed in sequence while one of these is still active. The second instruction will now report either an error 78 or an error 7. The user must allow the initial MGS, MAS=All, or MCS=All to complete before initiating another motion instruction. (x83819, x85559)
Kinetix 6000 S0 and S1 Safety Drive with Digital Inputs configuration
The hardwired digital inputs on the Kinetix 6000 S0 Enhanced Safe Torque-off Drive and S1 Advanced Safety Drive are now populated via 4 hardwired connections representing 7 selectable inputs. With the introduction of these profiles in version 17 of RSLogix 5000 software, users must develop application logic to map these inputs. This must be done via the MSG command, Read_IDN, Write_IDN to SERCOS Identification Number P-0-52, 53, 54, and 55. This data must be rewritten at each power-up of the SERCOS Ring. The user’s application must be written to make proper use of these digital inputs within the context of the associated motion instructions.
Event task names can conflict with Microsoft Windows Event names
Creation of an event task for a SoftLogix controller will result in the creation of a Microsoft Windows event with the same name. Because Windows events are globally scoped among all applications running on the same workstation, names of the event tasks must be chosen carefully so as not to conflict with other Windows events.
Versions 18 and later require updates to Custom Motion Database
If you currently use a Custom RSLogix 5000 Motion Database in RSLogix 5000 software version 12 through 17, you will need an updated motion database to work with versions 18 or later. The following table lists the motion database revisions that are used with these application versions.
* Before a Custom Motor can be used in version 18 or later, any Custom Motor currently in a motion database file at revision 5 or earlier (Motion.db format) must be converted to the newer Motion.mdb format.
To initiate the process of getting the database updated, please email your request to raeptechsupport@ra.rockwell.com. Please include any prior tech support case number if your current database includes non-Rockwell motors.
|
Version of Application |
Motion Database Revision |
|
21.03 / 21.00 20.03 / 20.01 |
9.8.0 [ Motion.mdb format ] 8.12.0 [ Motion.mdb format ] |
|
20.00 |
8.9.0 [ Motion.mdb format ] |
|
19.01 / 19.00 |
7.5.0 [ Motion.mdb format ] |
|
18.02 / 18.01 / 18.00 |
6.9.0 [ Motion.mdb format ] |
|
17.01 / 17.00 |
5.3.0 [ *Motion.md format ] |
|
16.04 / 16.03 / 16.00 |
4.2.0 [ *Motion.md format ] |
|
15.03 / 15.02 / 15.01 / 15.00 |
3.24.0 [ *Motion.md format ] |
|
14.01 / 14.00 |
3.12.0 [ *Motion.md format ] |
|
13.04 / 13.03 / 13.02 / 13.01 / 13.00 |
3.12.0 [ *Motion.md format ] |
|
12.06 / 12.05 / 12.04 / 12.03 / 12.02 / 12.01 / 12.00 |
3.3.0 [ *Motion.md format ] |
Error sometimes displayed when attempting to print to Adobe PDF
When Adobe Reader 6.0 and Adobe Acrobat 6.0 or 7.0 are both installed on the same workstation, attempting to print reports from the Logix Designer application sometimes result in a dialog box being displayed with the message "Unable to find Adobe PDF resource files. Do you want to run the installer in repair mode?‟ This issue is documented in the Adobe Knowledgebase article http://helpx.adobe.com/acrobat/kb/error-unable-create-pdf-resource.html, which also describes the recommended procedure for installing Adobe Acrobat Reader 6.0 and 7.0 on the same workstation.
A temporary workaround for printing reports is:
GSV of PositionFeedback1 attribute reports verification error
In version 20 and later, the PositionFeedback1 is now an integer value. When configuring a GSV of the PositionFeedback1 attribute, a destination tag value of type DINT is now required. (x123873)
Superimposed motion shifts path
Beginning with RSLogix 5000 software version 20, the superimposed motion behavior has changed. In Absolute mode, when Superimposed mode is programmed, the path is shifted by the superimposed motion, except for moves in the following conditions: (1) Sequence of moves using any termination type other than TT0 or TT1, (2) a merge, or (3) when the queue becomes empty.
This change allows for the capability of any path that is drawn on a table moving in either the X or Y direction as a result of superimposed motion to look exactly the same as if it were drawn on a stationary table. In RSLogix 5000 software version 19, the path was not shifted when Superimposed mode is programmed and this was not achievable. (x122482)
Enhancements to Motion Planner may affect motion profiles
The performance of the Rockwell Automation Integrated Motion’ s motion planner has been improved in the controller firmware associated with version 16.03 of RSLogix 5000 software. As a consequence, there can be minor differences in the velocity profile and the path profiles in some blended and merged moves. The majority of these minor differences manifest themselves in velocity limited moves and in moves programmed using an S-curve velocity profile. There can also be minor differences in Trapezoidal velocity profiles. Please refer to the Motion Planner, Version 16.03 Application Solution, publication RA-AP031, for additional details.
Kinematics transformations, additional native geometry support compatibility issues
The Kinematics transformation motion control capabilities of ControlLogix that were introduced with firmware revision 16.20 (included with RSLogix 5000 software version 16.03) should only be used with version 16.03 or greater of the application. If RSLogix 5000 software version 16.00 is used to upload a project containing one of the four new native geometries from a controller flashed with revision 16.20 firmware or later, then any of these four non-supported geometries will be converted to the default Coordinate System Type of Cartesian. The message attribute list error will be displayed during the download attempt of an RSLogix 5000 software version 16.03 project containing one of the four new native geometries to a controller flashed with a firmware revision earlier than revision 16.20. (x75769)
Version 17 installation does not automatically uninstall version 17 Beta versions
For users who have Beta software for version 17 of RSLogix 5000 software installed on their workstation, the version 17 install will not offer to uninstall any previous installations of version 17 software. Before installing the released version 17 software, it is necessary to first uninstall the version 17 Beta software using Add/Remove Programs.
Using Security with version 16 and CPR 7 FactoryTalk Network Directory Server
This applies only if you are using security with version 16 of RSLogix 5000 software. In order for CPR 7 FactoryTalk Network Directory clients to take advantage of new security actions added in version 16 of RSLogix 5000 software, a utility needs to be run on the CPR 7 FactoryTalk Network Directory Server. This utility is automatically run when version 16 of RSLogix 5000 software is installed.
However, if you will not be installing version 16 of RSLogix 5000 software on the FactoryTalk Network Directory Server, it is strongly recommended that you run the utility manually on the server prior to installing or running version 16 of RSLogix 5000 software on other workstations. The utility, named UpdateActionsInSchema.exe, can be found in the System\SecuritySchemaUpdate\ directory on the RSLogix 5000 DVD. Note that upon execution, the utility will provide further instructions.
SFCRESTART attribute removed for GSV/SSV
In version 16, the SFCRESTART attribute has been removed from the PROGRAM class for the GSV and SSV instructions. This attribute was not used in earlier versions of Logix5000, and it will now report a verification error if present.
Migrating to FactoryTalk Security (from RSI Security Server)
Existing RSI Security Server installations can be migrated to FactoryTalk Security. The FactoryTalk Security server is provided with the FactoryTalk Services Platform, which can be found on the DVD. See the FactoryTalk Security installation instructions for further migration information.
Removal of built-in action groups for Security
In version 16, the built-in action groups have been removed from RSLogix 5000 software (for example, Full Access, Maintain Project, Go Online, and View Project). If you are upgrading to RSLogix 5000 software version 16 and continue to use RSI Security Server for Logix security rather than migrating to FactoryTalk, a set of predefined action groups can be found in the RSLogix5000Security.bak file and are for use with version 16. These new action groups for the RSI Security Server are:
Tag Modify Properties required to update Configuration dialog boxes with Tag tab
When making changes to a configuration dialog box that contains a Tag tab, you sometimes see an error message indicating that Tag: Modify Properties is not granted. Allowed configuration changes to tabs other than the Tag tab are still committed, and this error can be ignored. (x72089)
FactoryTalk Security resource and action groups and FactoryTalk CPR 9 release
The release and update of FactoryTalk Security is independent of the release of the Logix Designer application. FactoryTalk Security in CPR 9 will support resource groups and action groups. This feature will allow you to conveniently group resources, like ControlLogix controllers, and actions, like Tag Create, for easier security administration.
Ramp/Soak (RMPS) results appear to be in error
Due to the operation of single precision floating point arithmetic processing in the controller, intermediate results shown in the Soak time left of the Ramp/Soak (RMPS) instruction may appear to be inaccurate during the execution of the instruction. This does not cause improper execution of the instruction. (x72583)
Opening pre-version 17 project with Axis and Axis Performance Verification
Some motor parameter value settings have been changed in the version 17 Motion Database for the following motor types:
A project created in a version earlier than version 17 of RSLogix 5000 software that contains an AXIS_SERVO_DRIVE type axis configured with one of these motors will have its related axis parameters converted when opened in version 17 of RSLogix 5000 software. When this occurs, the following warning message will be displayed: "Axis <tag_name> Warning: Parameters for the associated motor have changed, which may have caused changes to some axis parameters. Please verify the axis performance.”
When this warning is encountered, you should verify that the axis parameters pertaining to rated current are configured for proper axis operation. You should also validate that the axis is properly configured for your application. As an alternative, you can re-associate the motor to the axis, but in this case, all motor parameters will be reset to default motion database values, canceling any previously tuned and saved non-default axis values.
File import of Axis with MPx motors and Axis Performance Verification
In the Motion Database earlier than version 16 of RSLogix 5000 software, the Maximum Rated Current (I-rated) value for certain MPF, MPG, MPL, and TL motors were defined with settings from 1% to 7% higher than rated. If a project created in version 15 or earlier contains an AXIS_SERVE_DRIVE type axis configured with one of these motors, then when this project is imported (.L5K format project file) into RSLogix 5000 software version 16, the following warning will be generated: "Warning: During conversion of Axis <tag name> – Parameters for the associated motor have change, which may have caused changes to some axis parameters. Please verify the axis performance.‟
When this warning is encountered, you should verify that the Axis Parameters pertaining to Rated Current are configured for proper axis operation. As an alternative, you can re-associate the motor to the axis, but in this case, all motor parameters will be reset to default Motion database values, canceling many previously tuned and saved axis values.
This issue does not exist with database conversion of an .ACD format project file. The motors that are affected are:
LINT time stamp values not shown with FactoryTalk View SE Utility
A new 64-bit Long INTeger data type (LINT) was introduced in version 16 of RSLogix 5000 software. This data type is currently used only for date and time stamps for the analog and digital alarm instructions (ALMA and ALMD). In the CPR 9 release of FactoryTalk View SE, these LINT time stamp values can be seen only on the Alarm Summary, Alarm Banner, and Alarm Log. LINT time stamps cannot be seen on custom FactoryTalk View SE graphics. Support of LINT time stamp values on custom graphics will be added to a future release of FactoryTalk SE.
Controller time object changed in version 16
The Controller time object was modified in version 16 of RSLogix 5000 software to support future alarms and events functionality. Time stamps now use Universal Coordinated Time (UTC), also referred to as Greenwich Mean Time (GMT). If the logic in your application reads or sets the controller clock by using the GSV/SSV attribute DateTime, then this logic should be updated to use the new attribute LocalDateTime. You may also need to make other modifications to your application as a result of this change. (x72073, x72238)
Use new Clock Update Tool with Logix5000 version 16 and later
A Logix5000 Clock Update Tool is included on the DVD. Only revision 2.2.5 or later of this tool should be used with Logix5000 version 16 and later. Older revisions sometimes do not properly synchronize workstation time and controller time.
Firmware update required for 1734 and 1738 Ethernet Point adapters
When using a 1734-AENT or a 1738-AENT that is configured in one of the following two cases, you need to upgrade the firmware in the adapter module in order for both controllers to make a connection. The two scenarios are:
The required firmware for the 1734-AENT module is revision 2.003.4 or later, and the required firmware for the 1738-AENT module is revision 2.003.4 or later.
Non-Unicode character fonts
Rockwell Automation recommended that the Microsoft Windows operating system's Language for non-Unicode programs (System Locale) be configured to match the localized language. This is especially true for the Chinese, Japanese, and Korean editions. Not configuring the PC’ s operating system's System Locale to match the language of the application sometimes results in the inability of the application to show certain fonts.
If the Microsoft Windows operating system is not configured with the recommended System Locale, a warning will be displayed when the application is started. Clicking Change on this warning dialog box will navigate to the operating system dialog box from which you can adjust the System Locale.
The System Locale can then be changed by selecting a new Language for non-Unicode programs (System Locale) on the Advanced tab of the Regional and Language Options (accessed from Microsoft Windows Control Panel). For example, if you are running the Chinese version of the application (9324-RLD300ZHE), you should select Chinese (PRC) for the System Locale.
CTree errors opening projects with McAfee VirusScan running
With McAfee VirusScan Enterprise Edition 7.1 running, unexpected CTree errors are sometimes seen when project files are opened. This is caused by files in the temporary folders, AB_xxxx, being modified by the McAfee VirusScan software. McAfee VirusScan software should be configured to ignore the contents of the AB_xxxx folders.
Starting with RSLogix 5000 software version 14, the directory structure for temporary folders has been modified so that all AB_xxxx folders now reside within a single folder named RSLogix 5000.Temp located under the Temp directory (C:\Users\<username>\AppData\Local\Temp for Windows Server 2008 and Windows 7 operating systems.
To prevent the CTree errors from occurring, the McAfee VirusScan software settings can be configured to ignore the contents of the RSLogix5000.Temp folder. (x51417, x85503)
MOTION_INSTRUCTION data type change
The MOTION_INSTRUCTION data type changed in version 12 and later and the size increased from 12 bytes to 16 bytes. If you have created User-Defined data types that include members of type MOTION_INSTRUCTION, you will lose tag initial values when you convert your project files from earlier versions.
To work around this anomaly, export your project using a version earlier than version 12 of the application and then import the project in version 12.02 or later. If you have written logic that relies on the old 12-byte size (for example by doing a COP of a MOTION_INSTRUCTION tag) you will need to verify that your logic is still correct.
The new MOTION_INSTRUCTION data type structure is:
|
FLAGS |
DINT |
|
EN |
BOOL |
|
DN |
BOOL |
|
ER |
BOOL |
|
PC |
BOOL |
|
IP |
BOOL |
|
AC |
BOOL |
|
ACCEL |
BOOL |
|
DECEL |
BOOL |
|
ERR |
INT |
|
STATUS |
SINT |
|
STATE |
SINT |
|
SEGMENT |
DINT |
|
EXERR |
SINT |
Note the addition of a new flag AC and a new element EXERR. (x36228, x34556, x33393)
Extra digit of precision shown for REAL data type
The REAL data type now shows a 32-bit (4-byte) IEEE floating-point value with the following range:
The REAL data type also stores ±infinity, ±NAN, and -IND, but what the application shows differs based on the format.
The application also stores and shows the IEEE subnormal range:
|
Format: |
Equivalent: | |
|
Real |
+infinite
- infinite
+NAN
-NAN
-indefinite |
1.$
-1.$
1.#QNAN
-1.#QNAN
-1.#IND |
|
Exponential |
+infinite
- infinite
+NAN
-NAN
-indefinite |
1.#INF000e+000
-1.#INF000e+000
1.#QNAN00e+000
-1.#QNAN00e+000
-1.#IND0000e+000 |
Application appears to lock up when RSMACC connection broken
If RSAudit message logging is enabled and the workstation is unable to connect to the FactoryTalk AssetCentre (RSMACC) server to log messages, the Logix Designer application experiences intermittent freezes while it is waiting for the message requests to time out. This might cause the application to appear as though it has locked up, but if you wait about one minute, it will begin responding again.
To resolve this anomaly, either restore the connection to the FactoryTalk AssetCentre (RSMACC) server or disable the RSAudit message logging. Once a connection has been restored, cached messages will be logged to the server and the application will resume normal operation. (x36127)
Save sometimes results in large project .ACD file
During a file save operation, the Logix Designer application attempts to compress the contents of a project so that the resulting file (.ACD) requires less disk space. When opening a project, this process is reversed and the contents of the .ACD file are de-compressed. In some instances, the application is not able to compress the information within the .ACD file.
In order to prevent the loss of project information, the Logix Designer application will perform the save without the compression. When this occurs, your .ACD file sometimes become abnormally large, but it is still usable. That is, you can continue to work with the file as you would normally. However, if you contact Rockwell Automation Services & Support and provide a copy of your project file, this could help the Logix Designer application development team to locate the source of the compression failure.
Activation error running multiple versions simultaneously
If you have version 10.00 or later and also an earlier version of the application installed on your computer, you will observe an activation error if you run the version 10.00 or later version first and then attempt to run the earlier version simultaneously. To work around this anomaly, always run the earlier version first and then run the 10.00 or later version.
Default project directory
Be careful when performing operations with project files that depend on the default project directory. The Windows operating system controls and retains the default directory for the Open, Save As, and New Controller dialog boxes. Be sure to check that the folder selected is the one you wish to use when performing these operations to avoid mistakenly overwriting your project files. The Project Directory setting in the Tools Options dialog box is normally used unless you navigate to a different directory within the Open, Save As, or New Controller dialog boxes. (x28475, x27886)
FBD routine localized feedback wiring errors
In releases earlier than version 10.00, if you had a Function Block Diagram routine that contained nested feedback loops (outer and inner) you could download the project to a controller but sometimes encounter an error when uploading the project. This anomaly was caused by selecting multiple localized feedback wires in the outside feedback loop. In this release, this condition will be detected as a verification error in the routine. To correct this anomaly, select a feedback wire in the inner loop to be the localized feedback wire that is not also in the outer loop. (x28963, x27712)
FBD routine order of execution for unwired blocks
If you have a Function Block Diagram routine with function blocks that are not wired together, the execution order is not deterministic. Operations such as Verify Routine or Export/Import sometimes change the execution order unexpectedly for unwired blocks. To define the execution order, you must wire function blocks together. See the Function Block Attributes Order of Execution topic in the Help or the Logix5000 Process Control Drives Instructions Reference Manual, publication no. 1756-RM006 for more information. (x28703, x28681)
Describing a full circle using the MCCM instruction
In order to describe a full circle in a system with 2 axes in a coordinate system, the Direction flag in the MCCM instruction should be programmed using a code of 2 (CWF - Clockwise Full) or 3 (CCWF - Counterclockwise Full). Due to internal round-off in the floating point calculations, using a Direction flag of 0 (CW) or 1 (CCW ) with the start and end point being equal (or nearly equal) sometimes results in a small arc of nearly 0 degrees, instead of a full circle of nearly 360 degrees. (x56812)
Motion module Servo Update Period changed
The Servo Update Period for the 1756-M02AE 2 Axis Analog/Encoder Servo module has been changed from 200 microseconds to 250 microseconds. The servo update period is displayed on the Module Properties dialog box Associated Axes tab. This change in the Servo Update Period will have no effect on the behavior of existing motion control applications or on the overall performance of the motion control system. (x28647)
Motion Group Fault no longer produces Major Fault in Program mode
In version 12.01 and later, a motion group that is configured as General Fault Type: Major Fault, will no longer produce a Major Fault in program mode but will produce a Major Fault if the controller is in Run or Remote Run mode. In versions earlier than version 12.01, the motion group could produce a major fault while the controller was in Program or Remote program mode. For example, a store to nonvolatile memory interrupts the execution of the motion planner, which produces a fault. (x36957)
Phase Loss Fault-action for AM versus IAM on Kinetix 2000 & 6000 drives
With the new Phase Loss Fault-action, added in version 16, if the Integrated Axis Module (IAM) detects a phase loss fault, the motor attached to that IAM will respond with respect to the phase loss fault action setting as configured in the application without any user logic being written. However, if you expect the motor on the AM to perform in the same manner as does the IAM, a Kinetix Axis Module (AM) on the same power rail will require logic to be written.
This logic should monitor the IAM‟ s phase loss status bit, and based on the value of this bit, cause the motor attached to the AM to respond in the same manner as the IAM in regards to axis and drive stopping action. The AM cannot have the Power Loss Fault-action configured; only the IAM can. For more detail see also Kinetix Drive Firmware Release Notes. (x71448, x71717)
Motion Axis Fault reset MAFR timing changed on Kinetix drives
The Fault Reset timing for Kinetix based SERCOS Drives has changed in Drive firmware revision 1.85. The change accommodates new checks for reset of the motor commutation angle on the reset of certain drive faults, in particular E05 (IPM), E18 (Overspeed), and E19 (Following Error). Average timing changes observed were 20ms in version 13 associated drive firmware. Now up to 400ms, in RSLogix 5000 software version 15 and later, associated drive firmware for Motion Fault Reset MAFR instruction average timing changes can be observed to complete for clearing the above listed faults. For more detail see also Kinetix Drive Firmware Release Notes. (x55240)
ControlFLASH update of Rockwell Automation SERCOS Drives via SERCOS Ring
Version 13 of RSLogix 5000 software added the capability to use either RSLinx, RSWho, or RSLogix 5000 Who Active dialog boxes to browse to Rockwell Automation SERCOS drives. In version 15, support was added to allow direct firmware update of the Rockwell Automation SERCOS drives via ControlFLASH. The SERCOS Ring must be connected and able to reach Phase 2 to use ControlFLASH for firmware update. The ControlFLASH via Sercos will 1st transition the Ring to Phase-0, then re-establish Phase-2, and finally establish Phase-5 on the drive that ControlFLASH will be updating. ControlFLASH of the drives on the Ring must be done one drive node at a time.
Specific firmware revisions must exist on both the Logix MxxSE Sercos Interface motion modules and on the Rockwell Automation SERCOS Drives to support ControlFLASH via SERCOS. The Logix MxxSE module must have at minimum revision 15.06, the Rockwell Automation Kinetix Sercos drives must have revision 1.85 or higher, and the Rockwell Automation Ultra SERCOS drives must have revision 1.50 or higher. Also required is RSLinx software version 2.42 or later, and if using a 1784-PCICS card for the communication routing, the PCICS card should have current firmware and driver version 2.7 or later. (x51766)
Updating controller firmware in a DH485 network
If you update the firmware of a controller while it is connected to a DH485 network, communications on the network sometimes stops. To prevent this, disconnect the controller from the DH-485 network before you update the firmware of the controller. (x28491)
Online disconnection after non-volatile store or load operation
When using any of the controllers with nonvolatile memory, the memory store and memory load operations will take between 30 seconds and approximately 3 minutes to complete. During these operations the Logix Designer application will be taken offline and will require you to manually reconnect.
Any other workstations connected to the controller will also be taken offline. If you performed a store operation, or a load operation where your project did not have any online changes, you will be able to go back online immediately and the project will need to be saved. If you performed a load operation, and your project included online changes that you saved since the last store operation, you will be prompted to upload or download before going online.
I/O module list appears empty
If the list of modules appears empty in the Select Module Type dialog box when you attempt to create a new module, there could be an anomaly with system DLL files on your computer. Make sure that the version of files on your computer matches the compatible version listed in the table below. (x19891, x18680, x06823)
|
DLL Name |
Compatible Versions | |
|
Comcat.dll |
4.71 |
5.0 |
|
Ole32.dll |
4.0 |
4.71 or later |
Configuring CRC error detection
The Logix Designer application is configured to use BCC error detection by default when using DF1 serial port communication. CRC error detection can be configured instead of BCC by following these two steps.
CRC Error Detection must be selected on the Controller Properties dialog box System Protocol tab.
The RSLinx DF1 Communications Device Driver must be Auto-Configured so that the driver's Error Checking will be set to CRC to match the Logix5000 controller. The process is simplified if non-DF1 communications is used to select CRC Error Detection in the Logix5000 controller.
To change the error detection:
If you are using DF1 communications, there will be a short delay and then the information dialog box will display the error: "Failed to modify the DF1 Protocol configuration. Communications timed out.‟ This is expected and normal for this operation.
The other protocols will not display the error.
This DF1 driver will now communicate only with Logix5000 controllers that are set up to use CRC Error Detection.
Fatal error handling
There is a log file generated that records abnormal events and that can be delivered to Rockwell Automation Services & Support so that the anomaly can be recorded, diagnosed, and fixed. An abnormal termination of the Logix Designer application will result in a short period of program unresponsiveness followed by the appearance of a dialog box that identifies the fatal error. The dialog box contains specific details about the cause of the error. In addition, this information is appended to the file fatal error log file.
In order to more effectively address software error conditions, starting with version 14.00, the Fatal Error information will be stored in a file named RSLogix 5000 Fatal Error.Dmp. This file, containing the exact memory image at the time the error occurred, greatly extends our ability to determine the cause of the Fatal Error and to address product anomalies if those were the case. The new file will be large. If it must be sent to Rockwell Automation Services & Support, it can be either (a) copied to a CD or (b) posted onto our public FTP site (ftp://ftp.rockwellautomation.com/pub/). if it is not needed, the RSLogix 5000 Fatal Error.Dmp file can also be deleted.
Starting with RSLogix 5000 software version 17.00, these diagnostic files are located in C:\Users\Public\Public Documents\Rockwell Automation\RSLogix 5000\Logs for Windows Vista, Windows Server 2008, and Windows 7 operating systems, or in C:\Documents and Settings\All Users\Documents\Rockwell Automation\RSLogix 5000\Logs for Windows XP, Windows Server 2003, and Windows 2000 operating systems. For RSLogix 5000 software versions earlier than version 17.00, these diagnostic files are located in the directory C:\Documents and Settings\<username>\Local Settings\Temp (for all operating systems).
Destination operands for GSV commands
Caution should be used in selecting the proper data type for the destination operand of a GSV instruction. Use of mismatched operand data types sometimes result in unexpected results. Refer to the Instruction Set reference manual or the Help instructions to determine the proper data types.
Downloading controllers that use more memory than available
If a controller utilizing more memory than is available in the physical controller is downloaded, you will receive an appropriate error message. However, in some instances, the serial port will become inoperative. It is recommended that in this case, the controller memory be cleared (power turned off and the battery removed).
Multiple owners or listeners of 1756 analog modules
When using multiple owners or listeners of 1756 analog modules, set the Requested Packet Interval (RPI) for all connections to the same value. If different RPIs are used, connections sometimes will not recover correctly in a power-up situation.
Configuring the DHRIO module
When online with the controller, if the DHRIO module is configured for DH+ only, this module continuously displays Faulted as its Status on the Module Properties dialog box, even when normal communications exist. To avoid this erroneous fault condition, include the DHRIO module in the I/O configuration only if the application uses the Remote I/O features.
If the Logix5000 controller is not located in the default slot (slot 0) of the ControlLogix chassis, you must use RSLinx software version 2.20 or later, or the ControlLogix Gateway Configuration Tool (1756-GTWY) to setup a controller slot for the 1756-DHRIO module.
User disk memory utilization
If a Logix Designer application session is terminated abnormally, some large temporary files could be left on the hard drive. You should periodically delete old folders named AB_xxxx from your temporary directory. Smaller files with .SEM and .WRK suffixes could be left in your project directory after an abnormal termination and can also be deleted.
AB_xxxx folders reside within a single folder named "RSLogix 5000.Temp‟ located under the Temp directory (C:\Users\<username>\AppData\Local\Temp for Windows Vista, Windows Server 2008, and Windows 7 operating systems, or C:\Documents and Settings\<username>\Local Settings\Temp for Windows XP, Windows Server 2003, and Windows 2000 operating systems).