Release Notes

( 9324-RLDx ) Studio 5000 programming software. All you need for discrete, process, batch, motion, safety etc.
Version 21.00.00 (released 12/2012)

Catalog Number Studio 5000 Logix Designer 

These release notes describe version information for Studio 5000 Logix Designer, version 21.00.00 (released 12/2012).

Requirements

This release has the following requirements.

Hardware Requirements v21

System Requirements
Logix Designer 21.x

The personal computer must meet these minimum requirements. Using a computer meeting the recommended characteristics will improve performance.

 

Characteristic
Minimum Required
Recommended
Processor
Pentium 4
Intel Core i5
Speed
2.8 GHz
2.8 GHz
RAM Memory
2 GB
8 GB
Hard Disk Space
16 GB free
20 GB free
Graphics Device
DirectX 9, with WDDM 1.0 or higher driver
DirectX 9, with WDDM 1.0 or higher driver
  

Installation Notes

Logix Designer 21.x

Review these notes before attempting to install this version of the Studio 5000 Engineering and Design Environment.

Prior to Installation

Keep the following considerations in mind before you install the Studio 5000 Engineering and Design Environment:

Installing one of the following software versions:

·       Logix Designer application v21

·       RSNetWorx v21

·       RSLinx v3.51

·       Add-On Profiles using Core 9.0

·       DeviceNet Tag Generator

will cause prior versions of RSNetWorx and the DeviceNet Tag Generator to become inoperable.

Important: During the installation of Logix Designer application, version 21.03, the installation stops and a dialog box opens if an incompatible version of RSNetWorx software is detected on the PC. Upgrade RSNetWorx software to version 21 or uninstall it from your PC, and restart the Studio 5000 Engineering and Design Environment installation.

Installing the Software

Follow these steps to install the Studio 5000 Engineering and Design Environment.

  1. Start your personal computer.
  2. Insert the Studio 5000 Engineering and Design Environment installation DVD into your DVD-ROM drive.

The DVD-ROM should auto-start. If it does not auto-start, run Setup.exe from the root of the DVD.

The Studio 5000 Engineering and Design Environment supports multiple versions of the programming software on a single personal computer. With version 10 and later of the application, you may install as many of the later major versions as needed plus one version earlier than version 10 (for example, version 8.02).

  1. Follow the directions that appear on your screen.

Note that the Studio 5000 Engineering and Design Environment version 21 may need to update several system files early in the installation process. These updates will likely require you to restart your personal computer. Be sure to close all other applications before clicking OK to initiate this reboot.

When prompted for a serial number, enter the 10-digit serial number identifying your software license; otherwise, enter any sequence of characters, not longer than 10 characters.

Important: The 10-digit serial number is used to determine what functionality to enable while in Grace Period mode. Entering an invalid serial number will result in the application operating in Service Edition mode, upload and download only, while in Grace Period mode.

  1. When prompted, click Activate Studio 5000 to complete the activation of the software.
  2. Follow the directions that appear on your screen and refer to the FactoryTalk Activation insert for additional information.

Important: When a valid activation cannot be located by the application, the application will enter a seven-day activation grace period, during which you will be able to run the application with full functionality. If this seven-day grace period ends before a valid activation has been found, you will no longer be able to start the Logix Designer application.

  1. Click Close to complete the installation.

When the setup utility finishes, an entry for the Studio 5000 Engineering and Design Environment appears in the program list in the Rockwell Software group.

  1. Remove the Studio 5000 Engineering and Design Environment DVD from the DVD-ROM drive and store it in a safe place.

Starting the Studio 5000 Engineering and Design Environment

To start the Studio 5000 Engineering and Design Environment, from the Start menu, choose All Programs>Rockwell Software>Studio 5000 from the menu.

If Studio 5000 Engineering and Design Environment does not start up or run properly, keep the following in mind:

Uninstalling the Software

Follow these steps to uninstall the software when using the default Start menu on the Windows 7 or Windows Server 2008 operating system.

  1. From the Start menu, choose Control Panel.

(for Windows 7, Windows Server 2008 R2) From the Programs category, choose Uninstall a program.

(for Windows Server 2008 – Control Panel Home) From the Programs category, choose Uninstall a program.

(for Windows Server 2008 – Classic View) Double-click Programs and Features.

  1. From this dialog box, double-click Studio 5000 Logix Designer <version>.
  2. If all Studio 5000 Logix Designer <version> applications have been uninstalled, from this dialog box, double-click Studio 5000 Launcher.

Note: This will uninstall only the Studio 5000 Engineering and Design Environment. Other components that were installed with the Studio 5000 Engineering and Design Environment (such as Start Page Media, Online Books, or RSLinx) must be uninstalled separately.

Software Requirements Product Considerations v21

System Requirements
Logix Designer 21.x
  

Software Requirements v21

System Requirements
Logix Designer 21.x

Operating system and service pack compatibility:

  1. This version of RSLogix 5000 software has been tested on the following operating systems:
  2. Microsoft Windows 7 Professional (64-bit) with Service Pack 1
  3. Microsoft Windows 7 Home Premium (64-bit) with Service Pack 1
  4. Microsoft Windows 7 Home Premium (32-bit) with Service Pack 1
  5. Microsoft Windows Server 2003 R2 Standard Edition with Service Pack 1
  6. This version of RSLogix 5000 software is expected to operate correctly on all other editions and service packs of the following operating systems, but has not been tested:
  7. Microsoft Windows 7
  8. Microsoft Windows Server 2008 R2

For operating systems that support User Account Control (UAC), this version of RSLogix 5000 software was tested with UAC set to the most restrictive level (“Always notify” for Windows 7, or “On” for Vista). This version of RSLogix 5000 software is also expected to operate correctly when UAC is configured for any less restrictive setting.
Running the Logix Designer application in conjunction with Fast-User Switching, in Safe mode, or via Remote Desktop is not supported. 

Features

This release includes the following system features.

Pre-scan of Add-On Instruction Behavior

System Feature

Firmware Revision/ Software Version 21.011

 

Catalog Numbers 1756-L71, 1756-L72, 1756-L73, 1756-L74, 1756-L75, 1756-L73XT, 1756-L71S, 1756-L72S, 1756-L73S, 1756-L7SP, 1756-L73SXT, 1756-L7SPXT

Catalog Numbers 1769-L16ER-BB1B, 1769-L18ER-BB1B, 1769-L18ERM-BB1B, 1769-L24ER-QB1B, 1769-24ER-QBFC1B, 1769-L27ERM-QBFC1B, 1769-L30ER, 1769-L30ERM, 1769-L30ER-NSE, 1769-L33ER, 1769-L33ERM, 1769-L36ERM


The Pre-scan behavior of Add-On Instructions has been enhanced. This enhancement can affect Pre-scan behavior of Add-On Instructions when indirect addressing is used.
This enhancement can improve the Add-On Instruction initialization behavior when indirect addressing is used.
For more information, see Rockwell Automation Knowledgebase document 481124.

You can access the Rockwell Automation Knowledgebase at: http://www.rockwellautomation.com/rockwellautomation/support/overview.page?

 

Corrected Anomalies in This Release

This release corrects the following anomalies.

Generating WinHlp32 Database for Find Tab (x88677)

Corrected Anomaly

RSLogix 5000 Software 16.x


If you are logged on using an account that does not have Administrator privileges, you may be unable to generate the database for the Find tab for RSLogix 5000 Online Help. An error message will be displayed indicating “Unable to display the Find tab” or “WinHlp32 has stopped working”. This error can be resolved by generating the database while logged on using an account with Administrator privileges. If RSLogix 5000 will be used by an account that does not have Administrator privileges, we suggest that the database be created as part of the installation process while still logged on using an account that has Administrator privileges.

Known Anomalies in This Release

This release has the following known anomalies.

Disable Download Project Documentation and Extended Properties Features (Lgx00135928)

Known Anomaly First Identified As Of Firmware Revision 21.011

Studio 5000 Logix Designer First Identified As Of Version 21.00


Catalog Numbers:
- 1756 ControlLogix L7
- 1756 GuardLogix L7
- 5370 CompactLogix L1
- 5370 CompactLogix L2
- 5370 CompactLogix L3


IMPORTANT: The following restrictions apply to enabling or disabling the Download Project Documentation and Extended Properties feature and should be considered collectively. Any, or none, of these restrictions might apply to your application.

Restriction #1
Storing your project comments and tag descriptions in the controller can increase upload/download times. Be aware of the following:
• If you click the Cancel dialog box during the Finalize portion of the download process, the download process continues to successful completion and you may not be able to access the controller for long as 10 minutes.
• If the Finalizing portion of the download process takes longer than 10 minutes, the controller can generate a Major Non-recoverable fault (MNRF).

To work around this restriction, clear the Download Project Documentation and Extended Properties checkbox when downloading the project.

Restriction #2

IMPORTANT: This restriction exists only in environments that use multi-workstation development.
If you are using multi-workstation development, we strongly recommend that you configure the Logix Designer project to include all project documentation and extended properties when downloading a project to the controller.
This configuration setting is the default setting.
A Logix Designer project can lose content from the text boxes for routines written in either Function Block Diagram (FBD) or Sequential Function Chart (SFC) programming languages when both of the following conditions exist:
• Multiple workstations are online with the controller.
• The project is configured such that the Download Project Documentation and Extended Properties checkbox is cleared.
When project edits are made at one workstation, the content in the text boxes of edited routines are deleted from all of the other workstations in the environment.
To work around this restriction, configure the Logix Designer project so that the Download Project Documentation and Extended Properties checkbox is checked.

IMPORTANT: Consider the following:
• This anomaly does not apply if your Logix Designer project uses Ladder Logic (LL) or Structured Text (ST) programming languages.
• A restriction applies to when you check the Download Project Documentation and Extended Properties checkbox.

Restriction #3

IMPORTANT: This restriction exists only in environments that use multi-workstation development.
If you are using multi-workstation development, we strongly recommend that you configure the Logix Designer project to include all project documentation and extended properties when downloading a project to the controller.
A Logix Designer project can temporarily lose content in the Rung Comments sections when all of the following conditions exist:
• Multiple workstations are online with the controller.
• The project is configured such that the Download Project Documentation and Extended Properties checkbox is cleared.
• The Logix Designer project uses the Ladder Logic programming language.
When project edits are made at one workstation, the content in the Rung Comments sections for the project rungs is briefly hidden in all of the other workstations in the environment.

When rung edits are finalized on the workstation that is making edits, the content in the Rung Comments sections for the project rungs reappears in the in all of the other workstations in the environment.

To work around this anomaly, configure the Logix Designer project so that the Download Project Documentation and Extended Properties checkbox is checked.
 

ALMA and ALMD Instructions in Logix Designer

CORRECTED with Firmware Revision 24.011

Studio 5000 Logix Designer Version 24.00

Known Anomaly First Identified as of Firmware Revision 21.011


Catalog Numbers:


Even though controllers that use firmware revision 21.011 or later can use ALMA and ALMD instructions, FactoryTalk View Studio SE software, versions 6 and 7, cannot connect to a Logix Designer application that uses firmware revision 21.011 or later and uses ALMA or ALMD instructions.

IMPORTANT: This anomaly applies to the use of ALMA and ALMD instructions only. Tag-based alarming systems that use FactoryTalk Alarms and Events functionality work as expected.

IMPORTANT: This anomaly applies to the use of ALMA and ALMD instruction only. Tag-based alarming systems that use FactoryTalk Alarms and Events functionality work as expected with FactoryTalk View Studio SE software, version 6.

S-curve Function Executes with Uninitialized Values

Corrected as of:

Known Anomaly First Identified as of:

When you perform a Partial Import Online (PIO) of a function block routine that contains S-curve function blocks across Logix platforms, set the Initialize bit in the backing tag control structure of all S-curve instructions. This configuration causes the S-curve instructions to reinitialize themselves.

Failure to set the Initialize bit in the backing tag control structure of all S-curve instructions, can cause the S-curve function block to execute with uninitialized values.


Corrected: Logix Firmware/Studio 5000 Software 21.011

Log On to FactoryTalk Dialog Box Displays When Launching RSLogix 5000 (00124955)

Known Anomaly First Identified as of:

When launching RSLogix™ 5000 software, the Log On to FactoryTalk® dialog box can display. This dialog box can be seen when you do not have Administrator privileges on the personal computer and the current user does not exist in the FactoryTalk directory. If this dialog box is canceled, the RSLogix 5000 software is not launched. When the dialog box is displayed, entering the credentials for a user that has Administrator privileges on the personal computer allows RSLogix 5000 software to be launched.

To avoid seeing this dialog box, you can add the current user or user group to the FactoryTalk directory. Follow these steps to add a user or user group to the FactoryTalk directory.

  1. Launch the FactoryTalk Administration Console (available from the Start menu).
  2. Select the Network directory when prompted.

(In some cases, to continue, you need to provide credentials for a user with Administrator privileges.)

  1. To allow access for a particular user, navigate to Network\System\Users and Groups\Users, right-click the Users folder and choose New>Windows Linked User.
  2. Click Add and provide the domain\logon name for the desired user.

(You can click Check Names to verify that the name was found.)

  1. To allow access for all authenticated users, navigate to Network\System\Users and Groups\User Groups, right-click the User Groups folder and choose New>Windows Linked User Group.
  2. Click Add and type the name of the user group, Authenticated Users.

The Log On to FactoryTalk dialog box can also be displayed when you are using Remote Desktop to connect to the personal computer running RSLogix 5000 software.

This dialog box appears because FactoryTalk Security does not recognize the computer name. To enable access through Remote Desktop for a specific computer, you must add the name of the computer initiating the Remote Desktop connection to the Network\System\Computers and Groups\Computers folder in the FactoryTalk Administration Console.

To allow all computers to connect, follow these steps.

  1. Open the FactoryTalk Administration Console and log in to the Network directory with your domain credentials.
  2. Navigate to Network\System\Security Policy. In the Computer Policy Settings section, set Identify terminal server clients with the name of to Server Computer.

IMPORTANT: If Use single sign-on is set to disable in FactoryTalk software, then the Log On to FactoryTalk dialog box is displayed each time RSLogix 5000 software is launched. When this is launched, proper user credentials must be entered to continue. (By default, ‘Use single sign-on’ is set to enable.)


Modification of Add-On Instruction change date containing embedded UDT (Lgx0136323)

Corrected

Studio 5000 Logix Designer 21.00

An anomaly is present for tracking the change date of an Add-On Instruction that contains a user-defined data type (UDT). In Prior releases, when this embedded UDT had a modification of the UDT name, the Add-On Instruction it was embedded in would update its change date. In this current release, this has been noted to account for changes in individual members within the UDT as well as the description or comments for each member of the UDT. Now for any modification of the embedded UDT, the Add-On Instruction change date will reflect this modification and update its change date value. This anomaly is limited to the first nested layer of a UDT only. If a nested UDT is modified, then this modification will not be captured as a change date for the Add-On Instruction at this time.

Application Notes

This release has the following application notes.

Application Notes RSLinx Software v21

Logix Designer 21.x

Data access control compatibility with RSLinx software

In version 18 and later of the application, there is an External Access tag attribute, which defines how an external application can access a tag. This functionality is fully supported by RSLinx Classic software version 2.56 and RSLinx Enterprise software version 5.21. Version 18 and later of the application can be used with earlier versions of RSLinx Classic software to go online to a controller; however, earlier versions of RSLinx Classic or RSLinx Enterprise software should not be used as a data server with a controller running firmware revision 18 or later. Unexpected results will be observed when using an earlier version of RSLinx Classic or RSLinx Enterprise software as a data server with a controller running firmware revision 18 or later.

Please see Rockwell Automation Knowledgebase Tech Note #67071 (https://rockwellautomation.custhelp.com/app/answers/list).

Configuring the Ethernet port on a CompactLogix5532E controller

You are sometimes prevented from configuring the Ethernet Port of a CompactLogix5532E controller (catalog number 1769-L32E) via Channel 0 using RSLinx software. To work around the anomaly, use the Logix Designer application to configure the port (if the 1769-L32E controller is at revision 13) or use the BootP utility (which is enabled for a 1769-L32E controller at revision 1).

RSLinx Classic software Professional activation

Beginning with RSLinx Classic software version 2.31.00, the Logix Designer application Professional activation will also enable the RSLinx Classic Professional (RSLinx Classic OEM with version 16 and higher) version features. Only one professional activation is required for both products. The Logix Designer application Professional Activation must be installed on the personal computer hard disk in order to activate RSLinx Classic Professional (RSLinx Classic OEM with version 16 and higher).

Configuring drivers for the 1756-ENET, 1756-ENBT, and 1756-EWEB modules

You configure a driver for communicating from the workstation through the 1756-ENET, 1756-ENBT, or 1756-EWEB module by selecting Configure Drivers from the RSLinx Communications menu. In the dialog box, select Ethernet devices in the list of available driver types and click the Add New button.

If you are using RSLinx software version 2.40 or later, you can use the EtherNet/IP driver. This driver will automatically browse for all EtherNet/IP-capable devices on the local or configured remote subnet. See RSLinx Help for information on this driver. Note that 1756-ENET/A and 1756-ENET/B modules will not respond to the browse commands. You must use a different driver for these modules.

Configuring DF1 drivers

For DF1 point-to-point communications, choose RS232 DF1 Devices from the list of available drivers in RSLinx software. Then choose Logix5550 Serial Port for DeviceType. Rockwell Automation recommends that you do not use the DF1 Polling Master Driver or the DF1 Slave Driver with the Logix Designer application. You may be able to download successfully, but there are anomalies accessing information from I/O modules.

Offline tag and UDT Changes causing RSLinx software to halt communication

RSLinx software maintains knowledge of the memory layout of a Logix5000 controller in order to optimize the data access performance when accessing the data in these controllers. However, changes made to an offline project that are then downloaded can result in RSLinx software attempting to access tag information that is no longer present. When this occurs, RSLinx software halts the communications to the controller.

To recover, both RSLinx software and the software requesting tags from RSLinx software must be restarted. To avoid this anomaly, use caution when making offline changes to a project and then downloading to a Logix5000 controller. In particular:

Note that RSLinx Enterprise Series software is able to accommodate these changes without requiring a restart.

Third-party software with Logix Designer application

Data access control compatibility with third-party software

Some third-party data servers use un-tested data access methods not published in the Logix5000 Data Access manual. To assure controller integrity and overall system performance and reliably, Version 18 of RSLogix 5000 software only supported documented published methods for writes. Starting in Version 21 of the Logix Designer application, Logix controllers will only support published communications methods for both reads and writes. As a result, some third party data access packages may need to re-write or re-design their drivers to use a published communications method. Please see Rockwell Automation knowledgebase technical note 67071.

  

Application Notes v21

Logix Designer 21.x

The following information is provided to help you better understand the behavior of the Logix Designer in particular applications or under certain circumstances.

Product Resiliency Improvement

This release includes enhancements intended to improve product resiliency to potentially disruptive activities. These enhancements have been verified to not affect prodcut safety, performance, expected life, configuration, or operation of the product. Rockwell Automation advises customers to follow good Industrial Control System (ICS) security practices that include regular product updates. To ensure authenticity, obtain product updates and new releases directly from Rockwell Automation. Product resiliency includes, but is not limited to, security topics related to tamper prevention and detection, intellectual property management and source protection, and user authentication and authorization. 

Offline interactions between minor versions

Starting with version 21.03, ACD projects converted to version 21.03 and later cannot be opened in prior versions. 

Onlne interactions between controller and application

Starting with version 21.03, 

Support of minor versions

The Logix Designer application only supports the installation of a single minor release of the application on a computer. Therefore, version 21.03 or later versions of the application CANNOT run on the same computer as Logix Designer application version 21.00.

In order to support a system that runs version 21.03 and version 21.00, leverage the use of separate computers or use virtualization. 

Required to re-register EDS files after upgrading to version 20 or version 21 of the application

If the product described by the EDS file is to be used in the I/O configuration using EDS AOP, any EDS files that have been registered for RSLogix 5000 software version 19 and earlier must be re-registered after the installation of RSLogix 5000 software version 20 or later.

Resources cannot be found in the Online Books section of the Start Page

The Release History and Vendor Sample Project .pdf file will not display until http://localhost is added to the list of Trusted Sites in Internet Explorer.

Application crashes after importing the 1734-IB8 module

If you import the 1734-IB8 module into version 15 and later of the application, the application crashes. The workaround is to not import the 1734-IB8 module into the application. (x122918)

OpenRSLogix5000 command generates an error when trying to select Routine name

When you select a routine using the OpenRSLogix5000 command in FactoryTalk View, an error displays that tells you that RSLogix 5000 is not installed. To fix this issue, contact Technical Support to obtain a new revision directory dll.

Opening or creating data types causes the application to crash with older version of FTA

If FactoryTalk Activation version 4.0 or earlier is installed on your computer, opening or creating data types from the Controller Organizer causes the Logix Designer application to crash. To prevent this from happening, use FactoryTalk Activation version 4.1 with Logix Designer application version 21.

Download Project Documentation and Extended Properties

Your Logix Designer application project will not download in the following conditions:

To work around this restriction, check the Download Project Documentation and Extended Properties check box when configuring the project.

Download duration is slow for certain projects

Storing your project comments and tag descriptions in the controller increases upload/download times.

Be aware of the following:

To work around this restriction, clear the Download Project Documentation and Extended Properties check box when downloading the project.

IMPORTANT: Be aware that a restriction applies to clearing the Download Project Documentation and Extended Properties check box in a multi-workstation development application. (x135928)

Fatal error occur when attempt to go online with the controller

A false time stamp in the controller caused a fatal error to occur when you attempt to go online with the controller. Additionally, the application is not processing dates that are out of range when attempting to convert them to string format, which causes the application to crash. 

Use the following workaround to correct the controller's time stamp.

  1. Open the project ACD file.
  2. Select something other than the top node in the Controller Organizer. For example, click Unscheduled Programs.
  3. Go online with the controller. 
  4. Open the Controller Properties Date/Time tab. The Date and Time will show as ??.
  5. Click Set Date, Time and Zone from Workstation.

Use the following workaround to correct the out of range dates.

  1. Perform the workaround for the controller's time stamp first (see above).

It is critical to get the controller's time fixed. Otherwise, any new faults that are generated will also have false time stamps and will cause the controller to crash.

  1. From the Communication menu, choose Clear Faults (if any).

This will clear any major faults that exist. DO NOT attempt to do this from the Major Faults tab of the Controller Properties dialog box.

  1. Purge all existing minor faults by generating new ones so that the older false times faults are dropped.

DO NOT attempt to clear minor faults from the Minor Faults tab of the Controller Properties dialog box.

  1. To create minor faults, add a new rung online to an existing running routine.
  2. Test edits on the new rung to generate several minor faults.
  3. Untest edits.
  4. Go to the Controller Properties dial box - Minor Faults tab and clear the minor faults.

At this point, the controller's time stamp should be corrected and all faults that captured false time stamps should be cleared or purged.

Note that there is also the option to remove the batteries and power cycle the controllers. This will likely reset the controller's time stamp back to Jan. 1, 1998. This solution requires you to take the controller offline.

Rockwell Automation suggests that you investigate how the controller's time is getting a false value so that the problem does not repeat itself. (x135741)

Indirect addressing within Add-On Instruction logic

If your project uses indirect addressing in an Add-On Instruction, you need to be aware of two compatibility items when using RSLogix 5000 software version 20.01 and Logix5000 controller firmware revision 20.012.

First, you should consider RSLogix 5000 software version 20.01 and Logix5000 controller firmware revision 20.012 to be lock stepped. This means that you should not use the following:

EvRSI replaced by FactoryTalk Activation Manager

Beginning with RSLogix 5000 software version 20, EvRSI activation has been replaced by the FactoryTalk Activation Manager utility. EvRSI activation will not be able to activate the Logix Designer application. If you are using EvRSI activation, please contact your local Rockwell Automation Sales office or Rockwell Automation Services & Support for information on migrating your activations to FactoryTalk Activation.

1769-L2y controllers cannot be properly configured

For 1769-L2y controller types, which were released in RSLogix 5000 software version 20, the Embedded Counters module cannot be properly configured for Pulse External Direction. This anomaly was corrected in version 20.01. 1769-L2y controllers can be properly configured by using the Logix Designer application. However, 1769-L2y projects created by using RSLogix 5000 software version 20.00 will continue to be configured incorrectly.

To correct the configuration, the controller must be recreated in the Logix Designer application. A convenient way to do this import is to use the File > Import Component feature of the Logix Designer application to import your logic from the version 20.00 project to the new version project. This affects the following controller types:

Out-of-Box CIP Axis Position Loop Gain values adjusted with Load Observer

With the introduction of the CIP Motion Load Observer enhancement in version 19 of RSLogix 5000 software, the out-of-box calculations for several CIP Axis attributes were impacted. In particular, the Position Loop Bandwidth attribute and the Position Error Tolerance attribute will be automatically adjusted when the Load Coupling is change from Rigid to Compliant and Use Load Ratio is enabled.

When a change to the Load Coupling is applied, the out-of-box Position Loop Bandwidth will be reduced by 90% and the out-of-box Position Error Tolerance will be increased by 90%. This has the effect of loosening the out-of-box Position Gains so that the Motion Load Observer loop response can be tightened.

Time Synchronization replaces CST Time Mastership

RSLogix 5000 software version 18 has replaced the concept of Coordinated System Time (CST) Mastership with the more comprehensive notion of Time Synchronization, also referred to as CIP Sync Time Coordination. The Date/Time page of the controller properties has been modified to reflect this change.

For projects created with RSLogix 5000 software version 17 or earlier, if Coordinated System Time Master (CST) is enabled, then the converted project will have the Time Synchronization setting enabled. For more information about time synchronization using CIP Sync Time Coordination, refer to the Integrated Architecture and CIP Sync Configuration Application Technique, publication IA-AT003.

Attribute Value not Settable reported using AutoFLASH from Logix firmware revision 20 to an earlier revision

When attempting to download a project by using RSLogix 5000 software version 19 or earlier, if the controller firmware is at revision 20 or later and the controller is in Remote Run mode, then the version 19 software will not be able to change the controller mode in order to AutoFLASH the controller with revision 19 firmware. In this case, the controller mode must be changed either by using the keyswitch or by using version 20 or later of the application. (x123924)

CIP Generic writes to controller objects that originate from another controller failing

In RSLogix 5000 software version 20, there are enhanced security restrictions to controller CIP objects. Because of this, some CIP Generic messages that are used to write directly to controller object attributes sometimes do not function. Any CIP generic object write that originates external to the controller sometimes fail in version 20 or later of the application. CIP Generic writes that are executed in the controller’ s own user program will operate normally.

Security permissions changed for program creation

In version 17 of RSLogix 5000 software, the FactoryTalk Security permissions required for creating scheduled programs have changed slightly. As before, to create an unscheduled program, you need permission for the Program: Create action. To create a program scheduled in a task, however, you now need permission for both the Program: Create and the Task: Modify Properties actions. To create a program scheduled in the Power-Up Handler or Controller Fault Handler, you now need permission for both the Program: Create and the Controller: Modify Properties actions. (x77816, x77817)

Testing SFC online edits no longer always requires chart to reset

With RSLogix 5000 software version 17 and earlier, when performing online editing operations in a Sequential Function Chart (SFC), switching the executing logic from the original programming to the test edits version (or vice versa) resets the chart to the initial step and resets all stored actions. Beginning with version 18.00 of RSLogix 5000 software, many SFC online edits no longer result in this reset. In general, only edits that alter the logic structure of the chart will require the SFC routine to be reset.

In cases when a reset is required, you can force the transition with the initial step to false, wait for the routine to execute to the initial step, and then perform the test/un-test operation followed by removal of the force. Also, you can leverage the SFC Reset (SFR) instruction to reposition the chart back to the desired step. (x36331, x43482)

Cannot create, view, or edit modules based on Classic Profile after McAfee QuickClean

McAfee virus software version 8.0 ships with a Quick Registry Cleaner component that cleans the registry on a periodic basis. Upon cleaning the registry, the McAfee software removes all existence of the application's classic profiles from the registry. Once this has occurred, you can no longer create, view, or edit any classic profile based module.

This anomaly will also prevent the creation and importing of projects. When this condition is encountered, it is necessary to uninstall and reinstall the application. A way to avoid the anomaly is to remove the registry cleaner from any QuickClean manual and scheduled scans or delete all scheduled QuickClean tasks from the McAfee SecurityCenter UI. (x81691)

L5X file list not filtered on Windows 7 operating system

When performing a Partial Import online, the list of files displayed on the Import dialog box is filtered to show only files of the selected component type (for example, program, routine, data type, equipment phase). This filtering is not supported by the Windows 7 operating system. The Import dialog box will therefore show all .L5X format files when running the Logix Designer application on a Windows 7 operating system. The icon and ToolTip for the component file will identify the file type. (x105789, x112515, x113267)

Adobe Reader error selecting Online Books from the Tools menu

After installing RSLogix 5000 software version 19, you may see the Tools>Online Books menu item. If this menu item is selected, Adobe Reader will report that "This file cannot be found." This error occurs when using version 19 or later of the application if RSLogix 5000 software version 18 had also been installed on the same personal computer.

The Online Books installed with version 18 software were accessed by using the Custom Tools Menu (Tools>Online Books). The Online Books installed with version 19 and later access the Online Books by using the Start Page Resource Center. With version 19 installed, the Custom Tools Menu item for version 18 Online Books remains on the Tools menu, but is no longer used. Once RSLogix 5000 software version 19 has been installed, the unused Online Books Custom Tools Menu item can be manually removed by:

  1. Choosing Tools>Custom Tools.
  1. In the Custom Tools dialog box, select Online Books.
  2. Click Delete.
  3. Click OK to apply the change and close the dialog box. (x111895)

Unknown URL attempting to access Online Books or Vendor Sample Projects from Start Page

If your personal computer is not configured as part of a domain, you sometimes receive the error message "Unknown URL" when attempting to access Online Books or Vendor Sample Projects from the Start Page. This is the result of security enhancements to the Internet Explorer browser.

If Logix Designer application was installed by using the default installation path, the Online Books can be accessed from links provided in the file C:\Program Files\Rockwell Software\RSLogix 5000\Common\<language>\Docs\top level linking.pdf or C:\Program Files (x86)\Rockwell Software\RSLogix 5000\Common\<language>\Docs\top level linking.pdf, and the Vendor Sample Projects can be accessed from links provided in the file C:\RSLogix 5000\Projects\Samples\<language>\<version>\Third Party Products\Vendor Sample Projects.pdf. Access to Online Books and Vendor Sample Projects can be allowed by adding localhost’ to the allowed Local Internet sites. (x89165)

Help from 32-bit .hlp files is not displayed

The Windows Help (WinHlp32.exe) program is used to display Help that is provided in 32-bit .hlp files. The Microsoft Corporation stopped including this 32-bit Help file viewer in Windows releases beginning with Windows Vista and Windows Server 2008 operating systems. Version 18 and later of the application display Help in HTML format and does not require this Windows Help program. However, some module profiles may continue to display Help by using 32-bit .hlp files.

To properly display Help that is provided in 32-bit .hlp files on a Windows Vista or later operating system, you need to install the Windows Help program. This application is available for download from the Microsoft Download Center. For additional information on downloading and installing the Windows Help program, refer to the Microsoft Knowledgebase article I cannot open Help files that require the Windows Help (WinHlp32.exe).

Start Pages will not work if version 16.00 is installed after other versions

If version 16.00 of RSLogix 5000 software is installed after version 17.00 or later, Start Pages will fail to load and the message "Server Startup Failure physicalPath=… " will be displayed. In order to restore Start Page functionality, it is necessary to re-install the version 17.00 or later. Note that this anomaly will not be observed for version 16.03 and later. (x76424)

Function Block Diagram (FBD) ActiveX Faceplates not compatible with Windows Vista or later

The FBD ActiveX faceplates are not compatible with Microsoft Windows Vista or later operating systems. Instead, use FactoryTalk View SE/ME FBD Global Objects, available with FactoryTalk View SE/ME software version 5.1 or later.

Overflow checking improved for Immediate Operand values

In RSLogix 5000 software version 20, overflow checking for immediate operand values has been extended to all radix formats. Earlier versions of RSLogix 5000 software checked Octal values (that is, 8#nnn) for overflow into a 32-bit integer. Starting with RSLogix 5000 software version 20, immediate operand values of any integer-type radix (Hexadecimal, Decimal, Octal, or Binary) are checked for overflow into a 32-bit integer. The overflow conditions are indicated as errors during the verification process. (x116816)

First use of Drive profile when Add-On Profiles not installed requires media access

When a drive profile is first accessed, any user other than the user who installed the Drives Add-On Profiles version 4.02 or earlier will need access to the install media. When accessing the drive profile either by importing a project or by creating a drive in the I/O configuration tree, the user will be prompted with the following: "Enter an alternate path to a folder containing the installation package „RADrives_PF7.msi ”. ” The user must then provide the path on the installation media to ...\ENU\MP\RADrives\RADrives_PF7.msi. These Add-On Profiles may have been installed either separately or as part of the installation of RSLogix 5000 software version 20.01. (x128249)

Manual Tune fields active when Servo disabled

In version 20 or later, the Manual Tune parameters are enabled and editable when online for either the On or Off setting for the Servo parameter of a CIP_AXIS_DRIVE axis type. (x122492)

Motion instruction error for Stop_All or MGS Active and Pending Motion instruction

A new motion instruction error has been incorporated in version 17 of RSLogix 5000 software: error code 78 - Not Allowed While Stopping. In addition, an expanded meaning has been incorporated for error code 7 - Shutdown State Error. These errors will now be generated whenever an MGS, MAS=All, or MCS=All is active and a second motion instruction is then executed in sequence while one of these is still active. The second instruction will now report either an error 78 or an error 7. The user must allow the initial MGS, MAS=All, or MCS=All to complete before initiating another motion instruction. (x83819, x85559)

Kinetix 6000 S0 and S1 Safety Drive with Digital Inputs configuration

The hardwired digital inputs on the Kinetix 6000 S0 Enhanced Safe Torque-off Drive and S1 Advanced Safety Drive are now populated via 4 hardwired connections representing 7 selectable inputs. With the introduction of these profiles in version 17 of RSLogix 5000 software, users must develop application logic to map these inputs. This must be done via the MSG command, Read_IDN, Write_IDN to SERCOS Identification Number P-0-52, 53, 54, and 55. This data must be rewritten at each power-up of the SERCOS Ring. The user’s application must be written to make proper use of these digital inputs within the context of the associated motion instructions.

Event task names can conflict with Microsoft Windows Event names

Creation of an event task for a SoftLogix controller will result in the creation of a Microsoft Windows event with the same name. Because Windows events are globally scoped among all applications running on the same workstation, names of the event tasks must be chosen carefully so as not to conflict with other Windows events.

Versions 18 and later require updates to Custom Motion Database

If you currently use a Custom RSLogix 5000 Motion Database in RSLogix 5000 software version 12 through 17, you will need an updated motion database to work with versions 18 or later. The following table lists the motion database revisions that are used with these application versions.

* Before a Custom Motor can be used in version 18 or later, any Custom Motor currently in a motion database file at revision 5 or earlier (Motion.db format) must be converted to the newer Motion.mdb format.

To initiate the process of getting the database updated, please email your request to raeptechsupport@ra.rockwell.com. Please include any prior tech support case number if your current database includes non-Rockwell motors.

Version of Application
Motion Database Revision

21.03 / 21.00

20.03 / 20.01

9.8.0 [ Motion.mdb format ]

8.12.0 [ Motion.mdb format ]

20.00
8.9.0 [ Motion.mdb format ]
19.01 / 19.00
7.5.0 [ Motion.mdb format ]
18.02 / 18.01 / 18.00
6.9.0 [ Motion.mdb format ]
17.01 / 17.00
5.3.0 [ *Motion.md format ]
16.04 / 16.03 / 16.00
4.2.0 [ *Motion.md format ]
15.03 / 15.02 / 15.01 / 15.00
3.24.0 [ *Motion.md format ]
14.01 / 14.00
3.12.0 [ *Motion.md format ]
13.04 / 13.03 / 13.02 / 13.01 / 13.00
3.12.0 [ *Motion.md format ]
12.06 / 12.05 / 12.04 / 12.03 / 12.02 / 12.01 / 12.00
3.3.0 [ *Motion.md format ]


Error sometimes displayed when attempting to print to Adobe PDF

When Adobe Reader 6.0 and Adobe Acrobat 6.0 or 7.0 are both installed on the same workstation, attempting to print reports from the Logix Designer application sometimes result in a dialog box being displayed with the message "Unable to find Adobe PDF resource files. Do you want to run the installer in repair mode?‟ This issue is documented in the Adobe Knowledgebase article http://helpx.adobe.com/acrobat/kb/error-unable-create-pdf-resource.html, which also describes the recommended procedure for installing Adobe Acrobat Reader 6.0 and 7.0 on the same workstation.

A temporary workaround for printing reports is:

GSV of PositionFeedback1 attribute reports verification error

In version 20 and later, the PositionFeedback1 is now an integer value. When configuring a GSV of the PositionFeedback1 attribute, a destination tag value of type DINT is now required. (x123873)

Superimposed motion shifts path

Beginning with RSLogix 5000 software version 20, the superimposed motion behavior has changed. In Absolute mode, when Superimposed mode is programmed, the path is shifted by the superimposed motion, except for moves in the following conditions: (1) Sequence of moves using any termination type other than TT0 or TT1, (2) a merge, or (3) when the queue becomes empty.

This change allows for the capability of any path that is drawn on a table moving in either the X or Y direction as a result of superimposed motion to look exactly the same as if it were drawn on a stationary table. In RSLogix 5000 software version 19, the path was not shifted when Superimposed mode is programmed and this was not achievable. (x122482)

Enhancements to Motion Planner may affect motion profiles

The performance of the Rockwell Automation Integrated Motion’ s motion planner has been improved in the controller firmware associated with version 16.03 of RSLogix 5000 software. As a consequence, there can be minor differences in the velocity profile and the path profiles in some blended and merged moves. The majority of these minor differences manifest themselves in velocity limited moves and in moves programmed using an S-curve velocity profile. There can also be minor differences in Trapezoidal velocity profiles. Please refer to the Motion Planner, Version 16.03 Application Solution, publication RA-AP031, for additional details.

Kinematics transformations, additional native geometry support compatibility issues

The Kinematics transformation motion control capabilities of ControlLogix that were introduced with firmware revision 16.20 (included with RSLogix 5000 software version 16.03) should only be used with version 16.03 or greater of the application. If RSLogix 5000 software version 16.00 is used to upload a project containing one of the four new native geometries from a controller flashed with revision 16.20 firmware or later, then any of these four non-supported geometries will be converted to the default Coordinate System Type of Cartesian. The message attribute list error will be displayed during the download attempt of an RSLogix 5000 software version 16.03 project containing one of the four new native geometries to a controller flashed with a firmware revision earlier than revision 16.20. (x75769)

Version 17 installation does not automatically uninstall version 17 Beta versions

For users who have Beta software for version 17 of RSLogix 5000 software installed on their workstation, the version 17 install will not offer to uninstall any previous installations of version 17 software. Before installing the released version 17 software, it is necessary to first uninstall the version 17 Beta software using Add/Remove Programs.

Using Security with version 16 and CPR 7 FactoryTalk Network Directory Server

This applies only if you are using security with version 16 of RSLogix 5000 software. In order for CPR 7 FactoryTalk Network Directory clients to take advantage of new security actions added in version 16 of RSLogix 5000 software, a utility needs to be run on the CPR 7 FactoryTalk Network Directory Server. This utility is automatically run when version 16 of RSLogix 5000 software is installed.

However, if you will not be installing version 16 of RSLogix 5000 software on the FactoryTalk Network Directory Server, it is strongly recommended that you run the utility manually on the server prior to installing or running version 16 of RSLogix 5000 software on other workstations. The utility, named UpdateActionsInSchema.exe, can be found in the System\SecuritySchemaUpdate\ directory on the RSLogix 5000 DVD. Note that upon execution, the utility will provide further instructions.

SFCRESTART attribute removed for GSV/SSV

In version 16, the SFCRESTART attribute has been removed from the PROGRAM class for the GSV and SSV instructions. This attribute was not used in earlier versions of Logix5000, and it will now report a verification error if present.

Migrating to FactoryTalk Security (from RSI Security Server)

Existing RSI Security Server installations can be migrated to FactoryTalk Security. The FactoryTalk Security server is provided with the FactoryTalk Services Platform, which can be found on the DVD. See the FactoryTalk Security installation instructions for further migration information.

Removal of built-in action groups for Security

In version 16, the built-in action groups have been removed from RSLogix 5000 software (for example, Full Access, Maintain Project, Go Online, and View Project). If you are upgrading to RSLogix 5000 software version 16 and continue to use RSI Security Server for Logix security rather than migrating to FactoryTalk, a set of predefined action groups can be found in the RSLogix5000Security.bak file and are for use with version 16. These new action groups for the RSI Security Server are:

 Tag Modify Properties required to update Configuration dialog boxes with Tag tab

When making changes to a configuration dialog box that contains a Tag tab, you sometimes see an error message indicating that Tag: Modify Properties is not granted. Allowed configuration changes to tabs other than the Tag tab are still committed, and this error can be ignored. (x72089)

FactoryTalk Security resource and action groups and FactoryTalk CPR 9 release

The release and update of FactoryTalk Security is independent of the release of the Logix Designer application. FactoryTalk Security in CPR 9 will support resource groups and action groups. This feature will allow you to conveniently group resources, like ControlLogix controllers, and actions, like Tag Create, for easier security administration.

Ramp/Soak (RMPS) results appear to be in error

Due to the operation of single precision floating point arithmetic processing in the controller, intermediate results shown in the Soak time left of the Ramp/Soak (RMPS) instruction may appear to be inaccurate during the execution of the instruction. This does not cause improper execution of the instruction. (x72583)

Opening pre-version 17 project with Axis and Axis Performance Verification

Some motor parameter value settings have been changed in the version 17 Motion Database for the following motor types:

A project created in a version earlier than version 17 of RSLogix 5000 software that contains an AXIS_SERVO_DRIVE type axis configured with one of these motors will have its related axis parameters converted when opened in version 17 of RSLogix 5000 software. When this occurs, the following warning message will be displayed: "Axis <tag_name> Warning: Parameters for the associated motor have changed, which may have caused changes to some axis parameters. Please verify the axis performance.”

When this warning is encountered, you should verify that the axis parameters pertaining to rated current are configured for proper axis operation. You should also validate that the axis is properly configured for your application. As an alternative, you can re-associate the motor to the axis, but in this case, all motor parameters will be reset to default motion database values, canceling any previously tuned and saved non-default axis values.

File import of Axis with MPx motors and Axis Performance Verification

In the Motion Database earlier than version 16 of RSLogix 5000 software, the Maximum Rated Current (I-rated) value for certain MPF, MPG, MPL, and TL motors were defined with settings from 1% to 7% higher than rated. If a project created in version 15 or earlier contains an AXIS_SERVE_DRIVE type axis configured with one of these motors, then when this project is imported (.L5K format project file) into RSLogix 5000 software version 16, the following warning will be generated: "Warning: During conversion of Axis <tag name> – Parameters for the associated motor have change, which may have caused changes to some axis parameters. Please verify the axis performance.‟

When this warning is encountered, you should verify that the Axis Parameters pertaining to Rated Current are configured for proper axis operation. As an alternative, you can re-associate the motor to the axis, but in this case, all motor parameters will be reset to default Motion database values, canceling many previously tuned and saved axis values.

This issue does not exist with database conversion of an .ACD format project file. The motors that are affected are:

LINT time stamp values not shown with FactoryTalk View SE Utility

A new 64-bit Long INTeger data type (LINT) was introduced in version 16 of RSLogix 5000 software. This data type is currently used only for date and time stamps for the analog and digital alarm instructions (ALMA and ALMD). In the CPR 9 release of FactoryTalk View SE, these LINT time stamp values can be seen only on the Alarm Summary, Alarm Banner, and Alarm Log. LINT time stamps cannot be seen on custom FactoryTalk View SE graphics. Support of LINT time stamp values on custom graphics will be added to a future release of FactoryTalk SE.

Controller time object changed in version 16

The Controller time object was modified in version 16 of RSLogix 5000 software to support future alarms and events functionality. Time stamps now use Universal Coordinated Time (UTC), also referred to as Greenwich Mean Time (GMT). If the logic in your application reads or sets the controller clock by using the GSV/SSV attribute DateTime, then this logic should be updated to use the new attribute LocalDateTime. You may also need to make other modifications to your application as a result of this change. (x72073, x72238)

Use new Clock Update Tool with Logix5000 version 16 and later

A Logix5000 Clock Update Tool is included on the DVD. Only revision 2.2.5 or later of this tool should be used with Logix5000 version 16 and later. Older revisions sometimes do not properly synchronize workstation time and controller time.

Firmware update required for 1734 and 1738 Ethernet Point adapters

When using a 1734-AENT or a 1738-AENT that is configured in one of the following two cases, you need to upgrade the firmware in the adapter module in order for both controllers to make a connection. The two scenarios are:

The required firmware for the 1734-AENT module is revision 2.003.4 or later, and the required firmware for the 1738-AENT module is revision 2.003.4 or later.

Non-Unicode character fonts

Rockwell Automation recommended that the Microsoft Windows operating system's Language for non-Unicode programs (System Locale) be configured to match the localized language. This is especially true for the Chinese, Japanese, and Korean editions. Not configuring the PC’ s operating system's System Locale to match the language of the application sometimes results in the inability of the application to show certain fonts.

If the Microsoft Windows operating system is not configured with the recommended System Locale, a warning will be displayed when the application is started. Clicking Change on this warning dialog box will navigate to the operating system dialog box from which you can adjust the System Locale.

The System Locale can then be changed by selecting a new Language for non-Unicode programs (System Locale) on the Advanced tab of the Regional and Language Options (accessed from Microsoft Windows Control Panel). For example, if you are running the Chinese version of the application (9324-RLD300ZHE), you should select Chinese (PRC) for the System Locale.

CTree errors opening projects with McAfee VirusScan running

With McAfee VirusScan Enterprise Edition 7.1 running, unexpected CTree errors are sometimes seen when project files are opened. This is caused by files in the temporary folders, AB_xxxx, being modified by the McAfee VirusScan software. McAfee VirusScan software should be configured to ignore the contents of the AB_xxxx folders.

Starting with RSLogix 5000 software version 14, the directory structure for temporary folders has been modified so that all AB_xxxx folders now reside within a single folder named RSLogix 5000.Temp located under the Temp directory (C:\Users\<username>\AppData\Local\Temp for Windows Server 2008 and Windows 7 operating systems.

To prevent the CTree errors from occurring, the McAfee VirusScan software settings can be configured to ignore the contents of the RSLogix5000.Temp folder. (x51417, x85503)

MOTION_INSTRUCTION data type change

The MOTION_INSTRUCTION data type changed in version 12 and later and the size increased from 12 bytes to 16 bytes. If you have created User-Defined data types that include members of type MOTION_INSTRUCTION, you will lose tag initial values when you convert your project files from earlier versions.

To work around this anomaly, export your project using a version earlier than version 12 of the application and then import the project in version 12.02 or later. If you have written logic that relies on the old 12-byte size (for example by doing a COP of a MOTION_INSTRUCTION tag) you will need to verify that your logic is still correct.

The new MOTION_INSTRUCTION data type structure is:

FLAGS
DINT
EN
BOOL
DN
BOOL
ER
BOOL
PC
BOOL
IP
BOOL
AC
BOOL
ACCEL
BOOL
DECEL
BOOL
ERR
INT
STATUS
SINT
STATE
SINT
SEGMENT
DINT
EXERR
SINT

Note the addition of a new flag AC and a new element EXERR. (x36228, x34556, x33393)

Extra digit of precision shown for REAL data type

The REAL data type now shows a 32-bit (4-byte) IEEE floating-point value with the following range:

The REAL data type also stores ±infinity, ±NAN, and -IND, but what the application shows differs based on the format.

The application also stores and shows the IEEE subnormal range:

Format:
Equivalent:
Real
+infinite
- infinite
+NAN
-NAN
-indefinite
1.$
-1.$
1.#QNAN
-1.#QNAN
-1.#IND
Exponential
+infinite
- infinite
+NAN
-NAN
-indefinite
1.#INF000e+000
-1.#INF000e+000
1.#QNAN00e+000
-1.#QNAN00e+000
-1.#IND0000e+000


Application appears to lock up when RSMACC connection broken

If RSAudit message logging is enabled and the workstation is unable to connect to the FactoryTalk AssetCentre (RSMACC) server to log messages, the Logix Designer application experiences intermittent freezes while it is waiting for the message requests to time out. This might cause the application to appear as though it has locked up, but if you wait about one minute, it will begin responding again.

To resolve this anomaly, either restore the connection to the FactoryTalk AssetCentre (RSMACC) server or disable the RSAudit message logging. Once a connection has been restored, cached messages will be logged to the server and the application will resume normal operation. (x36127)

Save sometimes results in large project .ACD file

During a file save operation, the Logix Designer application attempts to compress the contents of a project so that the resulting file (.ACD) requires less disk space. When opening a project, this process is reversed and the contents of the .ACD file are de-compressed. In some instances, the application  is not able to compress the information within the .ACD file.

In order to prevent the loss of project information, the Logix Designer application will perform the save without the compression. When this occurs, your .ACD file sometimes become abnormally large, but it is still usable. That is, you can continue to work with the file as you would normally. However, if you contact Rockwell Automation Services & Support and provide a copy of your project file, this could help the Logix Designer application development team to locate the source of the compression failure.

Activation error running multiple versions simultaneously

If you have version 10.00 or later and also an earlier version of the application installed on your computer, you will observe an activation error if you run the version 10.00 or later version first and then attempt to run the earlier version simultaneously. To work around this anomaly, always run the earlier version first and then run the 10.00 or later version.

Default project directory

Be careful when performing operations with project files that depend on the default project directory. The Windows operating system controls and retains the default directory for the Open, Save As, and New Controller dialog boxes. Be sure to check that the folder selected is the one you wish to use when performing these operations to avoid mistakenly overwriting your project files. The Project Directory setting in the Tools Options dialog box is normally used unless you navigate to a different directory within the Open, Save As, or New Controller dialog boxes. (x28475, x27886)

FBD routine localized feedback wiring errors

In releases earlier than version 10.00, if you had a Function Block Diagram routine that contained nested feedback loops (outer and inner) you could download the project to a controller but sometimes encounter an error when uploading the project. This anomaly was caused by selecting multiple localized feedback wires in the outside feedback loop. In this release, this condition will be detected as a verification error in the routine. To correct this anomaly, select a feedback wire in the inner loop to be the localized feedback wire that is not also in the outer loop. (x28963, x27712)

FBD routine order of execution for unwired blocks

If you have a Function Block Diagram routine with function blocks that are not wired together, the execution order is not deterministic. Operations such as Verify Routine or Export/Import sometimes change the execution order unexpectedly for unwired blocks. To define the execution order, you must wire function blocks together. See the Function Block Attributes Order of Execution topic in the Help or the Logix5000 Process Control Drives Instructions Reference Manual, publication no. 1756-RM006 for more information. (x28703, x28681)

Describing a full circle using the MCCM instruction

In order to describe a full circle in a system with 2 axes in a coordinate system, the Direction flag in the MCCM instruction should be programmed using a code of 2 (CWF - Clockwise Full) or 3 (CCWF - Counterclockwise Full). Due to internal round-off in the floating point calculations, using a Direction flag of 0 (CW) or 1 (CCW ) with the start and end point being equal (or nearly equal) sometimes results in a small arc of nearly 0 degrees, instead of a full circle of nearly 360 degrees. (x56812)

Motion module Servo Update Period changed

The Servo Update Period for the 1756-M02AE 2 Axis Analog/Encoder Servo module has been changed from 200 microseconds to 250 microseconds. The servo update period is displayed on the Module Properties dialog box Associated Axes tab. This change in the Servo Update Period will have no effect on the behavior of existing motion control applications or on the overall performance of the motion control system. (x28647)

Motion Group Fault no longer produces Major Fault in Program mode

In version 12.01 and later, a motion group that is configured as General Fault Type: Major Fault, will no longer produce a Major Fault in program mode but will produce a Major Fault if the controller is in Run or Remote Run mode. In versions earlier than version 12.01, the motion group could produce a major fault while the controller was in Program or Remote program mode. For example, a store to nonvolatile memory interrupts the execution of the motion planner, which produces a fault. (x36957)

Phase Loss Fault-action for AM versus IAM on Kinetix 2000 & 6000 drives

With the new Phase Loss Fault-action, added in version 16, if the Integrated Axis Module (IAM) detects a phase loss fault, the motor attached to that IAM will respond with respect to the phase loss fault action setting as configured in the application without any user logic being written. However, if you expect the motor on the AM to perform in the same manner as does the IAM, a Kinetix Axis Module (AM) on the same power rail will require logic to be written.

This logic should monitor the IAM‟ s phase loss status bit, and based on the value of this bit, cause the motor attached to the AM to respond in the same manner as the IAM in regards to axis and drive stopping action. The AM cannot have the Power Loss Fault-action configured; only the IAM can. For more detail see also Kinetix Drive Firmware Release Notes. (x71448, x71717)

Motion Axis Fault reset MAFR timing changed on Kinetix drives

The Fault Reset timing for Kinetix based SERCOS Drives has changed in Drive firmware revision 1.85. The change accommodates new checks for reset of the motor commutation angle on the reset of certain drive faults, in particular E05 (IPM), E18 (Overspeed), and E19 (Following Error). Average timing changes observed were 20ms in version 13 associated drive firmware. Now up to 400ms, in RSLogix 5000 software version 15 and later, associated drive firmware for Motion Fault Reset MAFR instruction average timing changes can be observed to complete for clearing the above listed faults. For more detail see also Kinetix Drive Firmware Release Notes. (x55240)

ControlFLASH update of Rockwell Automation SERCOS Drives via SERCOS Ring

Version 13 of RSLogix 5000 software added the capability to use either RSLinx, RSWho, or RSLogix 5000 Who Active dialog boxes to browse to Rockwell Automation SERCOS drives. In version 15, support was added to allow direct firmware update of the Rockwell Automation SERCOS drives via ControlFLASH. The SERCOS Ring must be connected and able to reach Phase 2 to use ControlFLASH for firmware update. The ControlFLASH via Sercos will 1st transition the Ring to Phase-0, then re-establish Phase-2, and finally establish Phase-5 on the drive that ControlFLASH will be updating. ControlFLASH of the drives on the Ring must be done one drive node at a time.

Specific firmware revisions must exist on both the Logix MxxSE Sercos Interface motion modules and on the Rockwell Automation SERCOS Drives to support ControlFLASH via SERCOS. The Logix MxxSE module must have at minimum revision 15.06, the Rockwell Automation Kinetix Sercos drives must have revision 1.85 or higher, and the Rockwell Automation Ultra SERCOS drives must have revision 1.50 or higher. Also required is RSLinx software version 2.42 or later, and if using a 1784-PCICS card for the communication routing, the PCICS card should have current firmware and driver version 2.7 or later. (x51766)

Updating controller firmware in a DH485 network

If you update the firmware of a controller while it is connected to a DH485 network, communications on the network sometimes stops. To prevent this, disconnect the controller from the DH-485 network before you update the firmware of the controller. (x28491)

Online disconnection after non-volatile store or load operation

When using any of the controllers with nonvolatile memory, the memory store and memory load operations will take between 30 seconds and approximately 3 minutes to complete. During these operations the Logix Designer application will be taken offline and will require you to manually reconnect.

Any other workstations connected to the controller will also be taken offline. If you performed a store operation, or a load operation where your project did not have any online changes, you will be able to go back online immediately and the project will need to be saved. If you performed a load operation, and your project included online changes that you saved since the last store operation, you will be prompted to upload or download before going online.

I/O module list appears empty

If the list of modules appears empty in the Select Module Type dialog box when you attempt to create a new module, there could be an anomaly with system DLL files on your computer. Make sure that the version of files on your computer matches the compatible version listed in the table below. (x19891, x18680, x06823)

DLL Name
Compatible Versions
Comcat.dll
4.71
5.0
Ole32.dll
4.0
4.71 or later


Configuring CRC error detection

The Logix Designer application is configured to use BCC error detection by default when using DF1 serial port communication. CRC error detection can be configured instead of BCC by following these two steps.

CRC Error Detection must be selected on the Controller Properties dialog box System Protocol tab.

The RSLinx DF1 Communications Device Driver must be Auto-Configured so that the driver's Error Checking will be set to CRC to match the Logix5000 controller. The process is simplified if non-DF1 communications is used to select CRC Error Detection in the Logix5000 controller.

To change the error detection:

  1. Open a project and establish online communications using Ethernet, ControlNet, or DF1 communications to the target Logix5000 controller.
  2. Open the Controller Properties dialog box and select the System Protocol tab.
  3. Under Error Detection, enable the CRC radio button and select Apply.

If you are using DF1 communications, there will be a short delay and then the information dialog box will display the error: "Failed to modify the DF1 Protocol configuration. Communications timed out.‟ This is expected and normal for this operation.

  1. Click OK to acknowledge the error.

The other protocols will not display the error.

  1. Start RSLinx and select the Communications menu.
  2. Select Configure Drivers.
  3. Select Configure for the desired DF1 driver, such as AB_DF1-1.
  4. Click the Auto-Configure button and the text following the list box Error Checking will change from BCC to CRC.
  5. Click OK to close the dialog box and reduce RSLinx to an icon.
  6. If you are using DF1 communications, in the Logix Designer application, select Go Online to re-establish online communications.

This DF1 driver will now communicate only with Logix5000 controllers that are set up to use CRC Error Detection.

Fatal error handling

There is a log file generated that records abnormal events and that can be delivered to Rockwell Automation Services & Support so that the anomaly can be recorded, diagnosed, and fixed. An abnormal termination of the Logix Designer application will result in a short period of program unresponsiveness followed by the appearance of a dialog box that identifies the fatal error. The dialog box contains specific details about the cause of the error. In addition, this information is appended to the file fatal error log file.

In order to more effectively address software error conditions, starting with version 14.00, the Fatal Error information will be stored in a file named RSLogix 5000 Fatal Error.Dmp. This file, containing the exact memory image at the time the error occurred, greatly extends our ability to determine the cause of the Fatal Error and to address product anomalies if those were the case. The new file will be large. If it must be sent to Rockwell Automation Services & Support, it can be either (a) copied to a CD or (b) posted onto our public FTP site (ftp://ftp.rockwellautomation.com/pub/). if it is not needed, the RSLogix 5000 Fatal Error.Dmp file can also be deleted.

Starting with RSLogix 5000 software version 17.00, these diagnostic files are located in C:\Users\Public\Public Documents\Rockwell Automation\RSLogix 5000\Logs for Windows Vista, Windows Server 2008, and Windows 7 operating systems, or in C:\Documents and Settings\All Users\Documents\Rockwell Automation\RSLogix 5000\Logs for Windows XP, Windows Server 2003, and Windows 2000 operating systems. For RSLogix 5000 software versions earlier than version 17.00, these diagnostic files are located in the directory C:\Documents and Settings\<username>\Local Settings\Temp (for all operating systems).

Destination operands for GSV commands

Caution should be used in selecting the proper data type for the destination operand of a GSV instruction. Use of mismatched operand data types sometimes result in unexpected results. Refer to the Instruction Set reference manual or the Help instructions to determine the proper data types.

Downloading controllers that use more memory than available

If a controller utilizing more memory than is available in the physical controller is downloaded, you will receive an appropriate error message. However, in some instances, the serial port will become inoperative. It is recommended that in this case, the controller memory be cleared (power turned off and the battery removed).

Multiple owners or listeners of 1756 analog modules

When using multiple owners or listeners of 1756 analog modules, set the Requested Packet Interval (RPI) for all connections to the same value. If different RPIs are used, connections sometimes will not recover correctly in a power-up situation.

Configuring the DHRIO module

When online with the controller, if the DHRIO module is configured for DH+ only, this module continuously displays Faulted as its Status on the Module Properties dialog box, even when normal communications exist. To avoid this erroneous fault condition, include the DHRIO module in the I/O configuration only if the application uses the Remote I/O features.

If the Logix5000 controller is not located in the default slot (slot 0) of the ControlLogix chassis, you must use RSLinx software version 2.20 or later, or the ControlLogix Gateway Configuration Tool (1756-GTWY) to setup a controller slot for the 1756-DHRIO module.

User disk memory utilization

If a Logix Designer application session is terminated abnormally, some large temporary files could be left on the hard drive. You should periodically delete old folders named AB_xxxx from your temporary directory. Smaller files with .SEM and .WRK suffixes could be left in your project directory after an abnormal termination and can also be deleted.

AB_xxxx folders reside within a single folder named "RSLogix 5000.Temp‟ located under the Temp directory (C:\Users\<username>\AppData\Local\Temp for Windows Vista, Windows Server 2008, and Windows 7 operating systems, or C:\Documents and Settings\<username>\Local Settings\Temp for Windows XP, Windows Server 2003, and Windows 2000 operating systems).

Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.

Copyright © 2026 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please click here.
Trademarks not belonging to Rockwell Automation are property of their respective companies.