Release Notes

( 9301-2SEx ) RSView®32™ is an integrated, component-based HMI for monitoring and controlling automation machines and processes.
Version 7.60.00 (released 10/2011)

Catalog Number RSView32 

These release notes describe version information for RSView32, version 7.60.00 (released 10/2011).

Requirements

This release has the following requirements.

What's new in RSView32 7.60.00

Highlights

For Rockwell Automation Technical Support in the U.S. call 440-646-3434.

Outside the U.S. see http://www.rockwellautomation.com/locations/

 

Copyright© 2011 Rockwell Automation Technologies, Inc. All rights reserved. v. 7.6.0 July 29, 2011

How to activate RSView32

RSView32 7.60.00 no longer ships with a physical "master disk" for activating software. Instead, it is activated by activation files, generated by Rockwell Software and distributed over the Internet.

The types of activation supported for this release of RSView32 include:

  1. Node-locked activation. Depending upon the kind of device (stand-alone computer or hardware dongle) you want to activate, you can purchase either:
  1. Concurrent activation. This type of activation is locked to an activation server computer.

To activate RSView32 using node-locked activation, perform the following steps:

  1. Install the FactoryTalk® Activation Manager available from the main screen of the Install program.
  2. Once FactoryTalk® Activation Manager gets installed, it will guide you through the steps of downloading the activation from the Internet. You can download the activation to your stand-alone computer or hardware dongle.

To activate RSView32 using concurrent activation, perform the following steps:

  1. Add concurrent activation files to an activation server computer.
  1. Enable client machines to check out concurrent activation from an activation server.

 

Upgrading RSView32

Upgrading to FactoryTalk® Services Platform 2.40

Before upgrading your automation system software from an earlier version of FactoryTalk® Services Platform to the new FactoryTalk® Services Platform v.2.40, please take note of the following key points:

Known issues

 

Windows Firewall Configuration Utility

  1. Go to Start > Settings > Control Panel.
  2. On the Control Panel page, double-click the Windows Firewall icon to open the Windows Firewall dialog box.
  3. On the General tab of the Windows Firewall dialog box, check the Off (not recommended) option.
  4. Click the Exceptions tab.
  5. On the Exceptions tab, click Add Program, to open the Add a program dialog box.  
  6. Click Browse to search for the SPTDDSSV32.exe file and the MonitorRemoteProcesses.exe file. (These files are commonly located in C:\Program Files\Rockwell Software\RSView\).
  7. Once found, click Open. This adds the file to the Programs list box in the Add a Program dialog box.
  8. Repeat steps 6 and 7 to search for and add the SptFTServer.exe and sptddeex32.exe files. (These files are also commonly located in C:\Program Files\Rockwell Software\RSView\).
  9. Repeat steps 6 and 7 to search for and add the CMEOPC32.exe file. (This file is commonly located in C:\Program Files\Rockwell Software\RDM\).
  10. Repeat steps 6 and 7 to search for and add the RSViewLogServer.exe file, the RSVWHist.exe file, and RSRadMgr.exe file. (These files are commonly located in C:\Program Files\Common Files\Rockwell\).
  11. Click OK to return to Exceptions tab.
  12. On the Exceptions tab, scroll through the Programs and Services list box to verify that SPTDDSSV32, MonitorRemoteProcesses, SptFTServer, sptddeex32,  CMEOPC32, RSViewLogServer, RSVWHist, and RSRadMgr have been added to the list and are selected.
  13. If they are unchecked, click each one to select it.
  14. Click the Add Port button and then set Port Number to 135, set the Port Name to anything you want, and select the TCP type.
  15. On the Advanced tab, click Settings button for ICMP, to open the ICMP Settings dialog box.
  16. Click the following check boxes: Allow incoming echo request, Allow incoming timestamp request, Allow incoming mask request, and Allow incoming router request.
  17. Click OK to close the dialog box.
  18. In the General tab, click the On (recommended) option, and then click OK to close the dialog box.

Windows Vista/ Windows 7/ Windows Server 2008

Windows Server 2008

Windows XP Service Pack 2

Windows Internet Explorer 7

ActiveX controls

Commands

Example

gTagDb.GetTag("Tag1").Value =

“0123456789012345678901234567890123456789012345678901234567890123456789

0123456789012345678901234567890123456789012345678901234567890123456789

0123456789012345678901234567890123456789012345678901234567890123456789

0123456789012345678901234567890123456789abcde”

The AppActivate command will only bring the application forward if it is minimized. If the application is in the background, it will not bring it forward.

Communications

Data Execution Prevention

Data logging

Fast User Switching

Graphics

Graphics Import Export Wizard

Multi-processor systems

http://support.rockwellautomation.com/

ODBC Data Source

RSOPC Gateway

RSViewLogViewer

RSView32 Object Model

To avoid this problem, dimension the Tags collection at the module level (outside any procedures), rather than at the procedure level, or else use the roWait parameter.

Tag Database and Log Reports tool

User accounts

  1. Go to Start > Settings > Control Panel.
  2. On the Control Panel page, double click Administrative Tools, then Local Security Policy to open the Local Security Settings dialog box.
  3. In the console tree, click Local Policies, then Security options. In the details pane, right-click Network access: Sharing and security model for local accounts and open the Properties dialog.
  4. Select Classic – local users authenticate as themselves, then click OK to apply the changes.

Browsing for the RSView32 OPC server

You can use FactoryTalk® View Site Edition to browse the RSView32 tag database. The RSView32 OPC server appears in the list of available OPC servers when you create a new data server in FactoryTalk® View Site Edition. The OPC Server name (ProgID) is RSView32 OPC Tag Server.

Once you set up the RSView32 OPC server as a data server in FactoryTalk® View Site Edition, you can use the Tag Browser in FactoryTalk® View Site Edition to browse for tags in the RSView32 tag database.

Tips

Browsing the RSView32 tag database

Error messages appear in the RSView32 activity log when FactoryTalk® View Site Edition browses the RSView32 tag database. However, the client is still able to read the tag database.

These three error messages appear in each folder that is browsed:

You can ignore these error messages.

Using the RSView32 Object Model from an external automation controller

To provide access to the RSView32 Object Model from an external automation controller (such as Visual Basic or Visual C++), you must create a new RSView32 Application object and set a Project object to the currently loaded RSView32 project.

Example

Dim RsvApp as New RSView32.Application

Dim RsvProj as RSView32.Project 
 
Set RsvProj = RsvApp.ActiveProject 
'Continue on with code using RsvProj 

Differences in alarm event reporting between RSView32 and the RSView32 Object Model

The RSView32 alarm sub-system and the RSView32 Object Model receive alarm information from slightly different sources. The effect of this is that under certain circumstances, alarm events that show up in the Alarm Summary do not get reported by the RSView32 Object Model.

These circumstances are:

Hardware and software requirements

In the following tables, the demands your project places on the system are represented by points. Use the first table to total your points, and the second to determine your minimum hardware and software requirements.

Table 1: Points

For
If you are
Add points
RSView32 project
running displays, or editing your project using RSView32 Works
2
using more than 30,000 tags
2
using more than 5,000 tags
1
changing displays, on average, more than 5 times per minute
1
using more than 200 objects in displays
2
using ActiveX controls in displays
2
Alarms
 
monitoring more than 1,500 tags for alarms
2
monitoring more than 300 tags for alarms
1
Active Display System, or OPC Clients; simultaneously active clients
using typically more than 5 active clients
2
using at least 1 client
1
Data log or historical trends
logging less than 100 tags in 1 model
1
logging between 100 and 1000 tags in 1 model
2
logging to more than 1 model
2
Event detector, derived tags, or real-time trends
using any
1
VBA
using any
2
Add-ons
using any, for each one
1
Total points
 
Total of above points

Table 2: Minimum system configuration based on points

For this number of points
Minimum hardware you need
Minimum software you need
8 or more
Pentium II 400
128MB RAM
Windows XP Professional*
or

Windows 2000 Professional**
or

Windows Server 2003***
or

Windows Vista ****
or

Windows 7 Professional
or

Windows Server 2008 *****
6 or 7
Pentium II 300
128MB RAM
Windows XP Professional*
or

Windows 2000 Professional**
or

Windows Server 2003***
or

Windows Vista ****
or

Windows 7 Professional
or

Windows Server 2008 *****
3 to 5
Pentium 200
64MB RAM
Windows XP Professional*
or

Windows 2000 Professional**
or

Windows Server 2003***
or

Windows Vista ****
or

Windows 7 Professional
or

Windows Server 2008 *****

Important: The hardware should meet or exceed the minimum hardware requirements of the operating system you will run.

* With Service Pack 1 or later.

** With Service Pack 3 or later.

*** With Service Pack 1 or later.

**** With Service Pack 1 or later.

***** With Service Pack 2.

Tip

Software Platform\Hardware Compatibility Matrix

For the latest compatibility information for the Rockwell Automation software suite of products, consult Rockwell Automation Knowledgebase article 42682.

Requirements for using OPC on a client/server network

If you plan to use RSView32 as a remote server to networked OPC clients, the following are required:

Important

RSTools and RSView32

If you have RSTools installed on your system, you must activate RSJunctionBox before you start RSView32. If you fail to do this, an error dialog will appear.

 

  
Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.

Copyright © 2026 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please click here.
Trademarks not belonging to Rockwell Automation are property of their respective companies.