This release includes security enhancements as a part of our ongoing efforts to improve security. For information regarding Rockwell Automation's vulnerability disclosure process, please reference the Rockwell Automation Vulnerability Policy.
These anomalies are from previous releases but are still known in this release.
Mechanical Brake Delay (Lgx00113541, Lgx00107169)
Anomaly
Logix Firmware/RSLogix 5000™ Software 19.011
Catalog Numbers 1756-L61, 1756-L61S, 1756-L62, 1756-L62S, 1756-L63, 1756-L63S, 1756-L63XT, 1756-L64, 1756-L65, 1756-L72, 1756-L73, 1756-L74, 1756-L75
Logix Firmware/RSLogix 5000 Software 20.011
Catalog Numbers 1756-L71, 1756-L72S, 1756-L73S, 1756-L73XT, 1756-L73SXT
Catalog Numbers 1769-L18ERM-BB1B, 1769-L27ERM-QBFC1B, 1769-L30ERM, 1769-L33ERM, 1769-L36ERM
This anomaly occurs only in Integrated Motion on the EtherNet/IP network applications.
When you create a new CIP axis, the default value for Mechanical Brake Delay = 0. If you are using a motor with a brake on this axis and do not change the Mechanical Brake Delay value, the motor will not work properly when you attempt to execute motion.
To work around this anomaly, make sure that you set the Mechanical Brake Delay to the appropriate value before executing motion.
MSF Instruction (Lgx00113540, Lgx00108486)
Known Anomaly First Identified As Of
Catalog Numbers
- 1756-L61, 1756-L61S, 1756-L62, 1756-L62S, 1756-L63, 1756-L63S, 1756-L63XT, 1756-L64, 1756-L65, 1756-L72, 1756-L73, 1756-L74, 1756-L75 - Firmware Revision 19.011
- 1756-L71, 1756-L72S, 1756-L73S, 1756-L73XT, 1756-L73SXT - Firmware Revision 20.011
- 1769-L18ERM-BB1B, 1769-L27ERM-QBFC1B, 1769-L30ERM, 1769-L33ERM, 1769-L36ERM - Firmware Revision 20.011
This anomaly occurs only in Integrated Motion on the EtherNet/IP network applications.
Every time there is a Motion Servo Off (MSF) instruction/Motion Servo On (MSO) instruction cycle, the Position Trim value is added to the axis position. This change in axis position causes the axis to move unexpectedly by a distance equal to the Position Trim value.
Absolute Feedback Offset (Lgx00076298)
Known Anomaly First Identified as of:
Catalog Numbers:
If you issue an Absolute Feedback Offset, it results in a feedback fault. If you issue an Absolute Feedback Offset via an SSV instruction on the 1756-M02AS module, the result is a feedback fault. The feedback fault occurs regardless of whether feedback is on or off.
Logix CPU Security Tool
Known Anomaly First Identified as of Firmware Revision 20.011
RSLogix 5000™ Version 20.00
Studio 5000 Logix Designer™ First Identified as of Version 21.00
Catalog numbers:
Unconnected Timeout Time Incorrect (00171872)
Known Anomaly First Identified as of Firmware Revision 27.011
Catalog Numbers:
The unconnected timeout time can be longer for a Forward Open service than expected.
PI Function Block (Lgx00070832)
Known Anomaly First Identified as of:
For more information regarding the PI instruction, see the Logix5000™ Controllers Advanced Process Control and Drives Instructions User Manual, publication 1756-RM006.
Real Time Axis Attribute of VelocityFeedback (Lgx00107793)
Known Anomaly First Identified As Of:
Catalog Numbers 1756-L61, 1756-L61S, 1756-L62, 1756-L62S, 1756-L63, 1756-L63S, 1756-L63XT, 1756-L64, 1756-L65 Version 18.011
Catalog Numbers 1756-L72, 1756-L73, 1756-L74, 1756-L75 Version 19.011
Catalog Numbers 1756-L71, 1756-L72S, 1756-L73S, 1756-L73XT, 1756-L73SXT Version 20.011
This anomaly occurs only in SERCOS applications that use Kinetix SERCOS drives and linear motors.
Under certain conditions, it is possible that the Real Time Axis attribute VelocityFeedback contains an incorrect value. The inaccuracy is the result of incorrect scaling of that attribute.
Your program will have an incorrect value for the VelocityFeedback attribute if you follow these steps.
The VelocityFeedback attribute value is incorrect because that attribute was enabled before the program was saved, downloaded, and put online.
To work around this anomaly, do not enable the VelocityFeedback attribute until the RSLogix 5000 program is online.
Arithmetic State Flags (Lgx00122480)
Known Anomaly First Identified as of Firmware Revision 20.011
Catalog Numbers:
MAM Instruction With Merge Enabled (Lgx00078822)
Known Anomaly First Identified as of
Catalog numbers:
Under some rare occurrences, if a Motion Axis Move (MAM) instruction with Merge Enabled is activated during the deceleration segment of an active MAM instruction then the new MAM instruction may overshoot its programmed endpoint. The occurrence of the overshoot depends on the following factors:
•The original MAM instruction's remaining travel distance at the time of the merge and the new MAM instruction's remaining travel distance
•The relationship of the decel jerk of the new MAM instruction to the decel jerk of the original MAM instruction
•If the original MAM instruction is decelerating
Typically, the overshoot does not occur. If either of the following conditions exist, you will avoid the overshoot:
•The new MAM instruction is programmed with Merge Disabled. If there is no other motion active at the time of the merge, then the Merge Disable results in the same operation as the Merge Enable.
•The new MAM instruction has a slightly higher jerk (in units/seconds3) than the original MAM instruction. You should note, though, lower value of jerk in % of time results in higher value of jerk (in units/seconds3).
Excessive Velocity Error (Lgx00105360, Lgx00105595)
Known Anomaly First Identified as of:
Catalog Numbers:
IMPORTANT: This anomaly occurs only in applications that use Integrated Motion on the EtherNet/IP network.
With any coordinated move in a system that uses two or more CIP axes, if one axis is disabled using a Motion Servo Off (MSF) instruction, any remaining CIP axes will generate an Excessive Velocity Error, that is, Drive Error S55.
Accept Edits (Lgx00122528, Lgx00122622)
Known Anomaly First Identified as of Firmware Revision 20.011
Catalog Numbers:
When you accept edits in LD, ST, and FBD, the controller will log an 'Online Edit' entry in the controller log. Accepting edits in a SFC routine is done by performing a partial import, resulting in a 'Transaction Commit' entry in the controller log. This is confusing because you can select to mask both entries separately. Selecting only Online edits would cause the Audit Value to change only when FBD, ST, and LD edits are made. SFC online edits would change the Audit Value only if the 'Partial Import Online Transaction Completed' bit was set.
Anomaly
Logix Firmware/RSLogix 5000 Software 20.013, 21.011
Catalog Numbers:
● 1756-L61, 1756-L62, 1756-L63, 1756-L63XT, 1756-L64, 1756-L65
● 1756-L61S, 1756-L62S, 1756-L63S
● 1756-L71, 1756-L72, 1756-L73, 1756-L73XT, 1756-L74, 1756-L75
● 1756-L71S, 1756-L72S, 1756-L73S, 1756-L73SXT
Disable Download Project Documentation and Extended Properties Features (Lgx00135928)
Known Anomaly First Identified As Of Firmware Revision 21.011
Studio 5000 Logix Designer First Identified As Of Version 21.00
Alarm Log Content Lost at Powerup (Lgx00138163)
Known Anomaly First Identified as of Firmware Revision 24.011
Catalog Numbers:
Alarm Log content can be lost if there is a Secure Digital (SD) card in the controller that contains a project that is configured to load the project on powerup.
Controller Appears to Be Stuck in the Transition to Run Mode (Lgx00154875)
Known Anomaly First Identified as of Firmware Revision 24.011 for:
Corrected Anomaly as of Firmware Revision 1.013 for 1732E-OB8M8SR
Known Anomaly First Identified as of Firmware Revision 1.012 for 1732E-OB8M8SR
If your project uses a 1732E-OB8M8SR module, upgrade the module firmware to firmware revision 1.013 or later.
Expiration Times On a Logix Repository Record Can Differ (00171229)
Known Anomaly First Identified as of Firmware Revision 27.011
Catalog Numbers:
When the Logix Repository deletes a record, the cached value of the earliest expiration time and the actual expiration time value of the record can be different.
Incorrect Execution Schedule for Scheduled Output Module (Lgx00157174)
Known Anomaly First Identified as of Firmware Revision 24.011
Catalog Numbers:
This anomaly occurs with only 1756-OB16IEFS and 1732-OB8M8SR Scheduled Output modules.
The Scheduled Output module may schedule outputs incorrectly if the Motion Arm Output Cam (MAOC) instruction is enabled before the module’ s connection is in the RUNNING state. The following sequence must occur to observe the anomalous behavior.
To work around this anomaly, update your logic to verify that the scheduled output module is in the RUNNING state before executing the MAOC instruction.
|
Controllers
|
First Known in Firmware
Revision
|
Corrected in Firmware Revision
|
|
CompactLogix® 5370
|
20.011
|
37.011 and later
|
|
Compact GuardLogix® 5370
|
28.011
|
37.011 and later
|
|
ControlLogix® 5570
|
20.011
|
37.011 and later
|
|
GuardLogix 5570
|
20.011
|
37.011 and later
|
|
CompactLogix 5380
|
29.011
|
34.015, 35.014, 36.013, 37.011 and
later
|
|
Compact GuardLogix 5380 SIL 2
|
31.011
|
34.015, 35.014, 36.013, 37.011 and
later
|
|
Compact GuardLogix 5380 SIL 3
|
32.013
|
34.015, 35.014, 36.013, 37.011 and
later
|
|
CompactLogix 5380 Process
|
33.011
|
34.015, 35.014, 36.013, 37.011 and
later
|
|
CompactLogix 5480
|
32.011
|
34.015, 35.014, 36.013, 37.011 and
later
|
|
ControlLogix 5580
|
28.011
|
34.015, 35.014, 36.013, 37.011 and
later
|
|
GuardLogix 5580
|
31.011
|
34.015, 35.014, 36.013, 37.011 and
later
|
|
ControlLogix 5580 Process
|
33.011
|
34.015, 35.014, 36.013, 37.011 and
later
|
Axis Schedule Changes After Project Import and Download (00169297)
Known Anomaly First Identified as of Firmware Revision 27.011
Catalog Numbers:
An axis schedule can change when you import a Studio 5000 Logix Designer® application, versions 24 and 26, project into Logix Designer application, version 27.
Attribute Values Incorrect with Set System Value Instruction (00169713)
Known Anomaly First Identified as of Firmware Revision 27.011
Catalog Numbers:
When you use a Set System Variable (SSV) instruction to set the values for attributes available with the WallClockTime class, the values can be set incorrectly.
Wall Clock Value Different From Previous Value (00169756)
Known Anomaly First Identified as of Firmware Revision 27.011
Catalog Numbers:
After you set the wall clock for a controller, the actual time can be offset from the value that you set by approximately 2 seconds.
This anomaly occurs after Precision Time Protocol (PTP) is disabled in a controller that was previously synchronized with the grandmaster clock.
Motion Run Axis Tuning Instruction Gets Stuck (00172234)
Known Anomaly First Identified as of Firmware Revision 27.011
Catalog Numbers:
A Motion Run Axis Tuning (MRAT) instruction can get stuck and the .IP (In Process) stays set to 1. This anomaly can occur when the MRAT instruction is used to command a motion module to run a tuning motion profile for an axis, the instruction
Media Space Calculation Incorrect with 3rd-party Secure Digital Cards (00175295)
Known Anomaly First Identified as of Firmware Revision 28.011
Catalog Numbers:
The media space calculation that is done to determine the available memory on a Secure Digital (SD) card can be incorrect with 3rd-party SD cards that are 4 GB or greater.
This anomaly does not occur when you use SD cards available from Rockwell Automation. That is, the 1784-SD1 and 1784-SD2 cards.
We recommend that you use the SD cards available from Rockwell Automation with your controller.
While other SD cards can be used with the controller, Rockwell Automation has not tested the use of those cards with the controller. If you use an SD card other than those cards that are available from Rockwell Automation, you can experience data corruption or loss.
Motion Instruction Interference Can Prevent Axis From Being Enabled (00175334)
Known Anomaly First Identified as of Firmware Revision 27.011
Catalog Numbers:
Intermittent execution of a Motion Group Shutdown Reset (MGSR) instruction and Motion Servo On (MSO) instructions can result in an error on the MSO instruction and failure to enable an axis.
PhaseManager™ and SequenceManager™ Show Different States of Phase in Program Mode (00183769)
Known Anomaly First Identified as of Firmware Revision 28.011
Catalog Numbers:
If the controller is switched to Program mode while a sequence and phase are running, the phase state changes to idle and displays idle, while the sequence continues to show running. On transition back to Run mode, the sequence displays inactive.
|
Controllers
|
First Known in Firmware
Revision
|
Corrected in Firmware
Revision
|
|
CompactLogix™ 5370
|
20.011
|
38.011 and later
|
|
Compact GuardLogix® 5370
|
28.011
|
38.011 and later
|
|
ControlLogix® 5570
|
18.012
|
38.011 and later
|
|
GuardLogix 5570
|
20.011
|
38.011 and later
|
|
CompactLogix 5380
|
28.011
|
38.011 and later
|
|
Compact GuardLogix 5380 SIL 2
|
31.011
|
38.011 and later
|
|
Compact GuardLogix 5380 SIL 3
|
32.013
|
38.011 and later
|
|
CompactLogix 5380 Process
|
33.011
|
38.011 and later
|
|
CompactLogix 5480
|
32.011
|
38.011 and later
|
|
ControlLogix 5580
|
28.011
|
38.011 and later
|
|
GuardLogix 5580
|
31.011
|
38.011 and later
|
|
ControlLogix 5580 Process
|
33.011
|
38.011 and later
|
Work arounds to consider:
Controller Anomaly with Continuous Task, Indirect Addressing, and CONCAT or DTOS (1442602)
|
Controllers
|
First Known in
Firmware Revision
|
Corrected in Firmware
Revision
|
|
CompactLogix™ 5370
|
29.011
|
—
|
|
Compact GuardLogix® 5370
|
29.011
|
—
|
|
ControlLogix® 5570
|
29.011
|
—
|
|
GuardLogix 5570
|
29.011
|
—
|
|
ControlLogix 5570 redundant
|
30.051
|
—
|
Controller applications with a continuous task with CONCAT or DTOS instructions where indirect addressing exists may result in a controller major nonrecoverable fault/assert when additional task(s) exist. See Knowledgebase Technote 5570/5370 Controller Anomaly with Continuous Task, Indirect Addressing and CONCAT or DTOS.
SequenceManager Event Client 2.0 Can Experience Slow Performance When Using the Start Up Recovery Option (1769621)
|
Controllers
|
First Known in Firmware
Revision
|
Corrected in
Firmware Revision
|
|
CompactLogix™ 5370
|
28.011
|
36.011 and later
|
|
Compact GuardLogix® 5370
|
28.011
|
36.011 and later
|
|
ControlLogix® 5570
|
28.011
|
36.011 and later
|
|
GuardLogix 5570
|
28.011
|
36.011 and later
|
After downloading a new project, the SequenceManager™ Event Client that started with the Start Up Recovery option should stop attempting to recover events immediately. However, the Event Client can continue to attempt recovery until the maximum number of events has been reached.
Workaround: Start the SequenceManager Event Client with the Start Up Recovery option disabled.
SequenceManager Event Client 2.0 Cannot Reliably Recover Events on Startup of The Service (1766682)
|
Controllers
|
First Known in Firmware
Revision
|
Corrected in
Firmware Revision
|
|
CompactLogix™ 5370
|
28.011
|
36.011 and later
|
|
Compact GuardLogix® 5370
|
28.011
|
36.011 and later
|
|
ControlLogix® 5570
|
28.011
|
36.011 and later
|
|
GuardLogix 5570
|
28.011
|
36.011 and later
|
Starting the SequenceManager™ Event Client 2.0 service with the Start Up Recovery option enabled can result in missing data.