This release has the following requirements.
2711P-PVP7 Performance 12.104 works within the system requirements of all Rockwell Automation® software products. For the latest compatibility information, refer to the Product Compatibility and Download Center.
Hardware requirements
2711P-PVP7 Performance 12.104 requires the following hardware:
Component revisions
The following table identifies the new component revision information after 2711P-PVP7 Performance 12.104 is installed.
|
Components
|
Revisions
|
|
FactoryTalk View ME
|
12.00.77
|
|
FactoryTalk ViewPoint
|
12.00.05
|
|
FactoryTalk Services Platform
|
6.20.16
|
|
FactoryTalk Linx
|
6.20.35
|
|
Operating system
|
Windows 10 IoT Core Services 1809
v10.0.17763.1757
|
|
Platform revision
|
3.04.00
|
|
Fonts
|
2.00.00
|
This release has the following requirements.
2711P-PVP7 Performance 12.105 works within the system requirements of all Rockwell Automation® software products. For the latest compatibility information, refer to the Product Compatibility and Download Center.
Hardware requirements
2711P-PVP7 Performance 12.105 requires the following hardware:
Component revisions
The following table identifies the new component revision information after 2711P-PVP7 Performance 12.105 is installed.
|
Components
|
Revisions
|
|
FactoryTalk View ME
|
12.00.78
|
|
FactoryTalk ViewPoint
|
12.00.05
|
|
FactoryTalk Services Platform
|
6.20.16
|
|
FactoryTalk Linx
|
6.20.35
|
|
Operating system
|
Windows 10 IoT Core Services 1809
v10.0.17763.1757
|
|
Platform revision
|
3.08.00
|
|
Fonts
|
2.00.00
|
This release has the following requirements.
2711P-PVP7 Performance 12.106 works within the system requirements of all Rockwell Automation® software
products. For the latest compatibility information, refer to the Product Compatibility and Download Center.
Hardware requirements
2711P-PVP7 Performance 12.106 requires the following hardware:
Component revisions
The following table identifies the new component revision information after 2711P-PVP7 Performance 12.106 is installed.
|
Components
|
Revisions
|
|
FactoryTalk View ME
|
12.00.85
|
|
FactoryTalk ViewPoint
|
12.00.05
|
|
FactoryTalk Services Platform
|
6.20.16
|
|
FactoryTalk Linx
|
6.20.38
|
|
Operating system
|
Windows 10 IoT Core Services 1809
v10.0.17763.1757
|
|
Platform revision
|
3.11.00
|
|
Fonts
|
2.00.00
|
This release includes the following system features.
OpenSSL library is upgraded to 1.1.1q to enhance the system security.
This release includes the following system features.
2711P-PVP7 Performance 12.105 has the following enhanced features.
Provides remote access capability. VNC is turned off by default. You can turn on VNC in the Control Panel with administrator privileges.
Provides the functionality to print to PDF.
This release includes the following system features.
2711P-PVP7 Performance 12.106 has the following enhanced feature.
Supports alarm notification sounds and internal beepers caused by pressing button objects.
This release corrects the following anomalies.
The list identifies the anomalies corrected in 2711P-PVP7 Performance 12.104.
This release corrects the following anomalies.
This release corrects the following anomalies.
The list identifies the anomalies corrected in 2711P-PVP7 Performance 12.106.
This release has the following known anomalies.
To show the correct date, change the system date after powering on the terminal.
To avoid this problem, use the Delete key.
There is currently no workaround for this anomaly.
There is currently no workaround for this anomaly.
This release has the following known anomalies.
To avoid this problem, set the time zone on the terminal to UTC-8 (Pacific Time) with Daylight Saving Time Enabled, and then set the time and restart the terminal.
To avoid this problem, in the Time Zone setting, change the time to a similar time zone, for example, in the Configuration mode and change the Time Zone from (UTC-05:00) Eastern Time (US & Canada) to (UTC-05:00) Indiana East, and then run the application.
There is currently no workaround for this anomaly.
There is currently no workaround for this anomaly. After the sound stops playing (for example, after acknowledging the alarm or the sound ends), CPU usage becomes normal.
There is currently no workaround for this anomaly.
These anomalies are from previous releases but are still known in this release.
There is currently no workaround for this anomaly.
To avoid this problem, download the PDF to the terminal and use the built-in PDF viewer on the terminal.
To avoid this problem, restart the terminal and try again.
There is currently no workaround for this anomaly.
To avoid this problem, save the files on the terminal or an SD card.
To avoid this problem, use the touch screen.
To avoid this problem, use a Short Date format.
To avoid this problem, close the web browser once you do not need to access the application.
To avoid this problem, skip the IP address and upgrade the firmware using a USB drive.
There is currently no workaround for this anomaly.
There is currently no workaround for this anomaly.
There is currently no workaround for this anomaly.
There is currently no workaround for this anomaly.
To avoid this problem, reset the terminal after changing the settings.
There is currently no workaround for this anomaly.
This release has the following functional changes from the previous release.
This release has the following functional changes from the previous release.
2711P-PVP7 Performance version 12.105 has no changes in functionality since the last release.
This release has the following functional changes from the previous release.
2711P-PVP7 Performance version 12.106 has no changes in functionality since the last release.
This release has the following application notes.
The following are the application notes for 2711P-PVP7 Performance 12.104.
How to get firmware updates?
Firmware Upgrade Packages are available from the Product Compatibility and Download Center. After signing in, a selection of updates will become available for download.
To get the firmware updates
|
|
Tip: We don’t recommend using an SD card to update the firmware.
|
Rockwell Automation Knowledgebase Documents
Additional information regarding PanelView Plus 7 firmware updates can be found in Rockwell Automation Knowledgebase.
To locate pertinent documents, search using the keywords: "PanelView Plus 7", "PanelView Plus v7", "TOC", or "PVP7".
Unsupported features
The following features are not available in 2711P-PVP7 Performance 12.104:
Alternatively, use FactoryTalk® ViewPoint. Plan to support this in a future release.
There is currently no workaround. Plan to play locally stored video files through a web browser in a future release.
There is currently no workaround. Plan to support Universal Windows Platform (UWP) applications from Microsoft Store in a future release.
Alternatively, use a modern printer that supports supported IPP or AirPrint.
There is currently no workaround. Plan to support this in a future release.
ViewPoint runs, but without HTTPS. Plan to support this in a future release.
Alternatively, store data locally or on removable media.
There is currently no workaround. Plan to support the viewers with UWP applications (full-screen only).
Alternatively, modify the application in FactoryTalk View Studio to provide user access to the print screen function in the user application.
Alternatively, configure the terminal to dim the screen when it is idle in FactoryTalk View ME Station.
There is currently no workaround.
For more information about the unsupported features, see PanelView Plus 7 Performance Series B* Terminals Important Information (publication 2711p-rn005).
This release has the following application notes.
The following are the application notes for 2711P-PVP7 Performance 12.105.
How to get firmware updates?
Firmware Upgrade Packages are available from the Product Compatibility and Download Center. After signing in, a selection of updates will become available for download.
To get the firmware updates
|
|
Tip: We don’t recommend using an SD card to update the firmware.
|
Rockwell Automation Knowledgebase Documents
Additional information regarding PanelView Plus 7 firmware updates can be found in Rockwell Automation Knowledgebase.
To locate pertinent documents, search using the keywords: "PanelView Plus 7", "PanelView Plus v7", "TOC", or "PVP7".
Unsupported features
The following features are not available in 2711P-PVP7 Performance 12.105:
There is currently no workaround. Plan to play locally stored video files through a web browser in a future release.
There is currently no workaround. Plan to support Universal Windows Platform (UWP) applications from Microsoft Store in a future release.
There is currently no workaround. Plan to support this in a future release.
ViewPoint runs, but without HTTPS. Plan to support this in a future release.
Alternatively, store data locally or on removable media.
There is currently no workaround. Plan to support the viewers with UWP applications (full-screen only).
Alternatively, modify the application in FactoryTalk View Studio to provide user access to the print screen function in the user application.
Alternatively, configure the terminal to dim the screen when it is idle in FactoryTalk View ME Station.
There is currently no workaround.
For more information about the unsupported features, see PanelView Plus 7 Performance Series B* Terminals Important Information (publication 2711p-rn005).
This release has the following application notes.
The following are the application notes for 2711P-PVP7 Performance 12.106.
How to get firmware updates?
Firmware Upgrade Packages are available from the Product Compatibility and Download Center. After signing in, a selection of updates will become available for download.
To get the firmware updates
| Tip: We don’t recommend using an SD card to update the firmware. |
Rockwell Automation Knowledgebase Documents
Additional information regarding PanelView Plus 7 firmware updates can be found in Rockwell Automation Knowledgebase.
To locate pertinent documents, search using the keywords: "PanelView Plus 7", "PanelView Plus v7", "TOC", or "PVP7".
Unsupported features
The following features are not available in 2711P-PVP7 Performance 12.106:
For more information about the unsupported features, see PanelView Plus 7 Performance Series B* Terminals Important Information (publication 2711p-rn005).