Release Notes
The Network Device Library is a tested, documented, and life cycle managed object library including pre-configured status and diagnostic HMI faceplates for Stratix® Switches, Device Level Ring (DLR) & Parallel Redundancy Protocol (PRP) networks. HMI faceplates are provided for FactoryTalk View ME, FactoryTalk View SE and Studio 5000 View Designer. Use with Studio 5000 Application Code Manager for best results. Supports Stratix® 2500/5200/5400/5410/5700/5800 switch families.
Version 12.02.00 (released 12/2022)
Catalog Number Network Device Library
These release notes describe version information for Network Device Library, version 12.02.00 (released 12/2022).
Requirements
This release has the following requirements.
Network Device Library v12.02 Compatible Software
Requirement First Identified as of Software Version 12.02
- Studio 5000 Logix Designer® V30.01.00, v31.02.00, v32.04.00, v33.01.01,
v34.01.00 v312.02.00 for PAC Application Development
- Studio 5000® Application Code Manager v4.02 and later for bulk code
configuration
- Studio 5000 View Designer® v5.02 and later for PanelView™ 5000 Application
Development
- FactoryTalk® View Studio v11.00.00 and later for PanelView™ Plus and
FactoryTalk® View SE Application Development
Network Device Library v12.02 Compatible Hardware
Requirement First Identified as of Software Version 12.02
- PanelView™ 5500/5510/5310 with v5 or later firmware
- PanelView™ Plus with v11 or later firmware
- GuardLogix® 5580/GuardLogix® 5570/Compact GuardLogix® 5370/Compact
GuardLogix® 5380 controller with v30.001 or later firmware
Compatible Stratix Families for Stratix objects – recommended to use latest device firmware:
- Stratix 2500
- Stratix 5400
- Stratix 5410
- Stratix 5700
- Stratix 5800
Compatible Stratix Families for raC_Opr_NetDLR1 and raC_Opr_NetDLR1_Lite objects – recommended to use latest device firmware:
- Stratix 5200 *Note: Must use Ring #1 on CIP VLAN
- Stratix 5400
- Stratix 5700
- Stratix 5800 *Note: Must use Ring #1 on CIP VLAN
Compatible Stratix Families for raC_Opr_NetDLR3 objects – recommended to use latest device firmware:
*Note: At this time the DLR3 faceplate does not support Stratix 5200 or Stratix 5800. These may be compatible with single ring DLRs only when using Ring #1 and the ring is on the CIP VLAN.
Features
This release includes the following system features.
Network Device Library v12.02.00 – DLR3 Ring of Switches Support
Feature First Identified as of Software Version 12.02.00
DLR3 AOI previously supported a maximum of 2 switches per DLR network. New in v12.02 each DLR
network can support up to 10 switches for a “ring of switches” network.
Network Device Library v12.02.00 – Studio 5000 Application Code Manager
Support
Feature First Identified as of Software Version 12.02.00
Newly added for v12.02 is library support for Studio 5000 Application Code Manager. Studio 5000
Application Code Manager allows you to easily bulk generate project code by configuring rather than
programming. This update allows you to add Stratix modules to your project along with Stratix and
DLR AOIs and FactoryTalk View ME/SE HMI content.
A new video “How To Import and Configure Network Device Object in ACM.MP4” has also been
added to the library.
Network Device Library v12.02.00 – Updated Videos
Feature First Identified as of Software Version 12.02.00
Updated the following videos to include DLR_Lite information:
- Operational Overview of DLR Object Faceplates.mp4
- How To Configure DLR Object Components in View Designer.mp4
- How To Import and Configure DLR Object Components in FTView ME.mp4
- How To Import and Configure DLR Object Components in FTView SE.mp4
- How To Import and Configure Single DLR Object Components in Logix Designer.mp4
Updated the following videos to include DLR3/ring of switches information:
- How To Import and Configure Three DLR Object Components in Logix Designer.mp4
Updated the following videos to include standardization updates related to revision info and
program mode:
- Operational_Overview_Stratix_Managed_Switch_ Faceplates_in_MachineEdition.mp4
- Operational_Overview_Stratix_Managed_Switch_ Faceplates_in_SiteEdition.mp4
- Operational_Overview_Stratix_Managed_Switch_Faceplates_in_ViewDesigner.mp4
- How_To_Import_and_Configure_Stratix_Switch_Device_Objects_in_FTViewME.mp4
- How_To_Import_and_Configure_Stratix_Switch_Device_Objects_in_FTViewSE.mp4
- How_To_Import_and_Configure_Stratix_Switch_Device_Objects_in_ViewDesigner.mp4
- How_To_Import_and_Configure_Stratix_Switch_Device_Objects_in_Logix_Designer.mp4
Network Device Library v12.02.00 – FTView SE Stratix Title Bar Improvement
Feature First Identified as of Software Version 12.02.00
Stratix faceplate in FTView SE updated title bar to use default windows frame for more
consistent look and feel across libraries.
Network Device Library v12.02.00 – DLR Faceplate 5069-AENTR adapter icon
updated
Feature First Identified as of Software Version 12.02.00
5069-AENTR adapter shown in DLR networks on DLR faceplates updated to newer slim
version of hardware.
Network Device Library v12.02.00 – New Graphical launch buttons
Feature First Identified as of Software Version 12.02.00
New graphical launch buttons have been added in FactoryTalk View ME/SE global
object Graphic Symbols display and Studio 5000 View Designer projects. These are
launch buttons are physical representations of Stratix Switch modules which allow you to
build out a network or schematic style diagram of your system. Use along with the IO
Device Library v5.01 and Power Device Library v3.02 for a complete system.
Network Device Library v12.02.00 – Studio 5000 View Designer TabNav Variable
Removed
Feature First Identified as of Software Version 12.02.00
TabNav variable removed from faceplate properties for all Studio 5000 View Designer
faceplates. Initial value of 11 (home tab) now set by default without the need for user
configuration.
Network Device Library v12.02.00 – AOI Parameter Standardization
Feature First Identified as of Software Version 12.02.00
Made various changes to the AOI to follow standards across other device object libraries.
Changes included:
- Added HMI_Ref Output parameter to Stratix definition
Added AOI help
Network Device Library v12.02.00 – Reset DLR AOIs if path error is active for
extended period
Feature First Identified as of Software Version 12.02.00
All DLR AOIs now automatically reset if path error is active for an extended period of time
Network Device Library v12.02.00 – Example Application
Feature First Identified as of Software Version 12.02.00
Example application files have been added to the library to demonstrate how instructions
and HMI faceplates can be configured and used in applications. It is not recommended to
copy code from these applications, but they can be used as a reference or demonstration.
Included files:
- ACM Project
- ACD File (created from ACM project, modified as required to compile)
- FTView SE APA project archive (Station Application)
- FTView ME APA project archive
ViewDesigner Project
Corrected Anomalies in This Release
This release corrects the following anomalies.
Network Device Library – Stratix Switch Anomaly – Banner and Alarm Details
Corrected Anomaly with Software Version 1.01.00
Known Anomaly First Identified as of Software Version 1.00.01
Corrected inconsistent behavior of banner & alarm detail tabs for Stratix Switch Device Objects
Network Device Library – Stratix Switch Anomaly – Port status info
Corrected Anomaly with Software Version 1.01.00
Known Anomaly First Identified as of Software Version 1.00.01
Updated Port status info for ME Stratix Switch Device Objects
Network Device Library – Stratix Switch Anomaly – Time Sync Dropdown
Corrected Anomaly with Software Version 1.01.00
Known Anomaly First Identified as of Software Version 1.00.01
Corrected Time Sync selection dropdown visibility.
Network Device Library – Stratix Switch Anomaly – View Designer Last run state
data does not warn if controller in program mode
Corrected Anomaly with Software Version 12.02.00
Known Anomaly First Identified as of Software Version 1.01.00
Unlike FTView ME and SE, View Designer Stratix Faceplates will show last run state data without a
direct warning if the Controller is placed in Program Mode. Although PV5000 top banner will show
warning icon on controller indicator.
Network Device Library – Corrupted “How-to-Configure Three DLR Object
Components into View Designer.mp4” file
Corrected Anomaly with Software Version 1.01.02
Known Anomaly First Identified as of Software Version 1.01.00
Updated the corrupted “How To - Configure Three DLR Object Components into View Designer.mp4”
file.
Network Device Library – DLR AOI can cause major controller fault when used
with more than 31 nodes
Corrected Anomaly with Software Version 1.02.00
Known Anomaly First Identified as of Software Version 1.01.03
There is a known anomaly within all versions of the raC_Opr_NetDLR1_Rung.L5X and
raC_Opr_NetDLR3_Rung.L5X of logic that can cause a major controller fault if used with DLR
Networks with more than 31 Nodes. Refer to Knowledgebase Article BF25847-DLR Faceplate AOI
generates a Major controller fault if DLR Node 32 is selected on the Faceplate Home page.
If you are updating application from previous version, make sure select “Overwrite” option for AOI and
corresponding data tag.
Network Device Library – IP Address Selector Slider Anomaly
Corrected Anomaly with Software Version 1.03.00
Known Anomaly First Identified as of Software Version 1.02.00
Corrected IP Address selector slider anomaly
Network Device Library – DLR AOI creates minor faults with 5 nodes or less and
not enabled
Corrected Anomaly with Software Version 1.04.00
Known Anomaly First Identified as of Software Version 1.03.00
AOI correction to prevent minor faults for networks with 5 or less nodes, and in Not Enabled state.
Network Device Library – DLR3 Animation for Ring Selection in Path Error State
Corrected Anomaly with Software Version 1.04.00
Known Anomaly First Identified as of Software Version 1.03.00
Corrected animation for Ring Selector in Path Error state for Three-Ring 56-node FTView SE/ME
faceplates.
Network Device Library – Stratix 5800 Missing Modules Support
Corrected Anomaly with Software Version 12.02.00
Known Anomaly First Identified as of Software Version 1.04.00
Added support in v12.02.00 for any Stratix 5800 modules that were missing and unsupported by the
Stratix AOI:
Added support in v12.02.00 for DLR AOI to support Stratix 5800 as DLR node.
Known Anomalies in This Release
This release has the following known anomalies.
Network Device Library – DLR Participant list shows addresses 0.0.0.0
Known Anomaly First Identified as of Software Version 12.02.00
For DLR3 AOI, a Stratix-only network using DLR trunking can have a supervisor with IP address
0.0.0.0. See technote
AID 1132932 for more information.
Network Device Library – Reference Manual Library Update Procedure
Corrected Anomaly with Software Version v12.03.00
Known Anomaly First Identified as of Software Version v12.02
The reference manual DEVICE-RM400 has been updated to capture potential
issues when updating to v12.03 or greater. A used UDT name has changed in
v12.02+ from raC_UDT_ItfAD_Framework_Sts udt to
raC_UDT_ItfAD_Stratix_Sts. This name changes will result in errors when
performing library updates. The solution is to manually update each existing
"Ref_Ctrl_Sts" tag's data type to raC_UDT_ItfAD_Stratix_Sts.
Network Device Library – Reference Manual Stratix 5800 Firmware Compatibility
Corrected Anomaly with Software Version v12.03.00
Known Anomaly First Identified as of Software Version v12.02
The reference manual DEVICE-RM400 displayed incorrect firmware compatibility
for the Stratix 5800. This has been corrected for Stratix 5800 rev 17.2(7)E1a or
later.
Network Device Library – Reference Manual Upgrade Procedure
Corrected Anomaly with Software Version v12.03.00
Known Anomaly First Identified as of Software Version v12.02
The reference manual DEVICE-RM400 has been updated to include
considerations for UDT name changes that occurred in v12.02 including
raC_UDT_ItfAD_Framework_Sts udt to raC_UDT_ItfAD_Stratix_Sts which may
have resulted in errors when upgrading from previous AOI versions. An extra
step has been added in the manual to address this issue.
Network Device Library – raC_Dvc_StratixAllImport Rung Ref_Module Missing
Corrected Anomaly with Software Version v12.03.00
Known Anomaly First Identified as of Software Version v12.02
When using the import rung method to add the raC_Dvc_StratixAll AOI into a project, the
Ref_Module would be incorrectly set to ‘0’. The import rung 5X file has been updated to
resolve this problem with release v12.03.00.
Network Device Library – raC_Dvc_StratixAll and raC_Opr_DLR Default Message
Path
Corrected Anomaly with Software Version v12.03.00
Known Anomaly First Identified as of Software Version v12.02
Network Device Library instructions for Stratix and DLR may be imported with incorrect
message paths. The message path should be set to 1,0 by default. This has been
resolved with release version 12.03.00.
Network Device Library – raC_Opr_NetDLR3 Minor Anomalies
Corrected Anomaly with Software Version v12.03.00
Known Anomaly First Identified as of Software Version v12.02
A number of minor anomalies related to the raC_Opr_NetDLR3 instruction have been
resolved in library release v12.03.00 including:
- Ring number drop-down had issues when used with switches that support
multiple rings but have only ring 1 enabled.
- Switch valid path indicator was not getting cleared during instruction initialization
and could have incorrectly reported as ‘1’ (valid path).
- Messages faulted if AOI Stratix switch path included a space character in the
string (e.g. “2, 192.168.1.10”).
Network Device Library – raC_Opr_NetDLR – “?” Icon showing for some devices
Corrected Anomaly with Software Version v12.03.00
Known Anomaly First Identified as of Software Version v12.02
The DLR HMI faceplates may have shown a “?” icon for some unknown devices
including the 1788-EN2FFR and 1788-EN2PAR devices. This has now be updated to
show a generic ethernet device icon.
Network Device Library – raC_Dvc_StratixALL – .Sts_ER Output Becomes Latched
Known Anomaly First Identified as of Software Version v12.02
Some users may observe an anomaly in the AOI that occurs when the switch
experiences total loss of connectivity (for example, when the switch can no longer
communicate with the primary controller). The .Sts_ER parameter is triggered and
remains true for an indefinite amount of time, even after the lost connection is restored.
The AOI will then display incorrect diagnostics info until the .Sts_ER is cleared manually
by resetting the errored Ref_GetSingleMessage MSG instruction within the AOI logic. See technote
https://rockwellautomation.custhelp.com/app/answers/answer_view/a_id/1141904 for more information.
Known Anomalies from Previous Releases
These anomalies are from previous releases but are still known in this release.
NetDLR Objects Incompatible with CompactLogix 5480 Dual Ethernet Ports
Known Anomaly First Identified as of Software Version 1.04.00
Affected Instructions: raC_Opr_NetDLR1, raC_Opr_NetDLR1_Lite, raC_Opr_NetDLR3
CompactLogix® 5480 controller uses DLR instance
#2 while DLR instance #1 is disabled. The
Device Level Ring (DLR) device objects are not compatible with the CompactLogix®
5480 Controller.
Network Device Library – DLR AOI not supported in CompactLogix 5480 Controller
Known Anomaly First Identified as of Software Version 1.01.00
CompactLogix 5480 uses DLR Ring Instance 2. The DLR Add-On Instruction scans only DLR Ring
Instance 1 which is used by all other devices. As a workaround, use a different device as a DLR
supervisor if possible. Refer to the technote
AID 1137345.
Network Device Library – raC_Dvc_Stratix AOI stops execution when 19 VLANs
used
Known Anomaly First Identified as of Software Version v12.01
raC_Dvc_Stratix AOI ver 12.1, 12.2 and 12.3 will stop execution on Step 106
(rung 64 for AOI v12.1 or rung 65 for AOI v12.2 and 12.3). The anomaly is
exposed only If Stratix switch has exactly 19 VLANs defined with numbers below
1002. Workaround: define an additional unused VLAN with the number below
1002.
Environment:
- Stratix AOI ver 12.1 (Network Device Library 1.01-1.04)
- Stratix AOI ver 12.2 (Network Device Library 12.02)
- Stratix AOI ver 12.3 (Network Device Library 12.03)
- Stratix 5200
- Stratix 5400
- Stratix 5410
- Stratix 5700
- Stratix 5800
Functional Changes
This release has the following functional changes from the previous release.
Network Device Library v12.02 Updated Documentation
Functional Change First Identified as of Software Version 12.02
A new reference manual DEVICE-RM400A-EN-P “Network Device Library” has been
created to replace and combine the previous documents “RM- raC_Opr_NetDLR1.pdf”,
“RM- raC_Opr_NetDLR3.pdf”, “RM- raC_Opr_StratixSwitch.pdf”, “QuickStart - Device
Level Ring Objects.pdf”, and “QuickStart - Stratix Switch Device Objects.pdf”
Network Device Library v12.02 – Combined Studio 5000 View Designer VPD Files
Functional Change First Identified as of Software Version 12.02
Studio 5000 View Designer files have been consolidated into two VPD project files. One
contains all DLR objects and the other contains all stratix objects.
- (raC-12_02-VD) raC_Opr_NetDLR.vpd
- (raC-12_02-VD) raC_Dvc_Stratix.vpd
Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.
Copyright © 2026 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please
click here.Trademarks not belonging to Rockwell Automation are property of their respective companies.