Release Notes

FactoryTalk® Linx Gateway permits 3rd-party OPC software to access data from FactoryTalk® Linx data server(s)
Version 6.30.00 (released 3/2022) - 6.31.00 (released 1/2023)

Catalog Number FactoryTalk Linx Gateway 

These release notes describe version information for FactoryTalk Linx Gateway, version 6.30.00 (released 3/2022) - 6.31.00 (released 1/2023).

Requirements

This release has the following requirements.

The following are the system requirements for FactoryTalk Linx Gateway version 6.30.00.

FactoryTalk Linx Gateway works within the system requirements of all Rockwell Automation® software products.

For the latest compatibility information, refer to the Product Compatibility and Download Center.

Hardware requirements

FactoryTalk Linx Gateway requires the following hardware:

graphic
Tip: When FactoryTalk Linx Gateway is operating on Windows 10 IOT Enterprise (for example, the Windows core of a CompactLogix 5480 controller), it is limited to a FactoryTalk Directory and FactoryTalk Linx data server running in the same environment (a remote directory and data server are not supported).

FactoryTalk Linx Data Bridge performance may vary depending on host computer performance, network, and application configurations.

FactoryTalk Linx Data Bridge was tested with the following hardware:

Operating systems

FactoryTalk Linx Gateway is tested on operating systems installed from original Microsoft® media only. They run on the 64-bit versions of the following Windows® operating systems:

*For additional information about Windows 10 Support for the FactoryTalk Suite of Rockwell Software products, refer to Knowledgebase Document ID: IN4493 - Windows 10 Support for the FactoryTalk Suite of Rockwell Software products

Software compatibility

FactoryTalk Linx Gateway version 6.30.00 (CPR 9 SR 13) was tested with, and is compatible with, the following Rockwell Automation products when used on the same computer:

High Resolution Display Support

Windows 10 v1803 or later is the recommended operating system if running this software with a 2K or 4K High Resolution Display with scaling up to 125%.

Rockwell Automation Test Environment

Rockwell Automation tests software products under a standard configuration of operating systems and antivirus software. For additional information, see the Knowledgebase Document ID: PN24 - Rockwell Software Products and Antivirus Software.

Supported browsers

The following web browsers have been tested and are supported for use with this release:

Security requirements

To help meet secure system design requirements, review these publications:

To learn about implementing CIP Security, see CIP Security with Rockwell Automation Products (publication SECURE-AT001).

Requirements

This release has the following requirements.

FactoryTalk Linx Gateway version 6.31.00 works within the system requirements of all Rockwell Automation® software products.

For the latest compatibility information, refer to the Product Compatibility and Download Center.

Hardware requirements

FactoryTalk Linx Gateway recommends the following hardware for applications with typical data acquisition needs:

Lower level x86-based CPUs will also work in standalone configurations with reduced data acquisition needs.

For small applications, the following configuration was also evaluated:

It is recommended to run a performance validation test on the planned computer hardware to ensure that the desired capacity and performance can be achieved.

graphic
Tip: When FactoryTalk Linx Gateway is operating on Windows® 10 IOT Enterprise (for example, the Windows core of a CompactLogix™ 5480 controller), it is limited to a FactoryTalk Directory and FactoryTalk Linx data server running in the same environment (a remote directory and data server are not supported).

Operating systems

FactoryTalk Linx Gateway was tested on the following operating systems:

*For additional information about Windows 10 Support for the FactoryTalk Suite of Rockwell Software® products, refer to Knowledgebase Document ID: IN4493 - Windows 10 Support for the FactoryTalk Suite of Rockwell Software products.

Software compatibility

FactoryTalk Linx Gateway version 6.31.00 is compatible with these Rockwell Software products:

High Resolution Display Support

Windows 10 v1803 or later is the recommended operating system if running this software with a 2K or 4K High Resolution Display with scaling up to 125%.

Rockwell Automation Test Environment

Rockwell Automation tests software products under a standard configuration of operating systems and antivirus software. For additional information, see the Knowledgebase Document ID: PN24 - Rockwell Software Products and Antivirus Software.

Supported browsers

The following web browsers have been tested and are supported for use with this release:

Security requirements

To help meet secure system design requirements, review these publications:

To learn about implementing CIP Security, see CIP Security with Rockwell Automation Products Application Technique  (publication SECURE-AT001).

Features

This release includes the following system features.

FactoryTalk Linx Gateway version 6.30.00 has the following new and enhanced features:

New features

Enhanced features

Features

This release includes the following system features.

FactoryTalk Linx Gateway version 6.31.00 has the following new features:

graphic
Note: FactoryTalk Linx and the FactoryTalk Linx OPC UA connector include new capabilities that can be utilized by external clients connected to FactoryTalk Linx Gateway. Review each product’s Release Notes and documentation to determine the full set of capabilities.

Known Anomalies in This Release

This release has the following known anomalies.

            To solve this problem, add sub-items instead of folder.

Known Anomalies in This Release

This release has the following known anomalies.

Known Anomalies from Previous Releases

These anomalies are from previous releases but are still known in this release.

Functional Changes

This release has the following functional changes from the previous release.

FactoryTalk Linx Gateway version 6.30.00 has the following changes in functionality since the last release:

Change in operating system support

Beginning in this release, the product installer prevents installation on all 32-bit versions of Windows operating systems (for example, Windows 10, 32-bit) and any Windows 7 operating system (for example, Windows 7 Professional, 64-bit).

Functional Changes

This release has the following functional changes from the previous release.

FactoryTalk Linx Gateway version 6.31.00 has no changes in functionality since the last release.

Application Notes

This release has the following application notes.

The following are the application notes for FactoryTalk Linx Gateway version 6.30.00.

Array Data Request

When an OPC UA Client makes a subsequent request to an array beyond the last element previously requested, FactoryTalk Linx Gateway’s OPC UA service will initially return a "BadIndexRangeNoData" error. If the array is defined to accommodate the requested elements, the initial error response is replaced with the appropriate array data.

Certificate

When a user regenerates a certificate in FactoryTalk Linx Gateway version 6.21.00 or later, and then uninstall it with "Keep configuration when uninstall" selected, FactoryTalk Linx Gateway installed on the same computer later may not work. To avoid this problem, delete all the files in folder <C:\ProgramData\Rockwell\FactoryTalk Linx Gateway\PKI\own>, restart FactoryTalk Linx Gateway, and then regenerate an outgoing certificate.

The following certificates are installed while installing Rockwell Automation software.

FactoryTalk Linx Gateway unsupported data types

FactoryTalk Linx Gateway natively supports most FactoryTalk data types. FactoryTalk Linx Gateway does not support accessing these types through either the DA or UA service:

Tested FactoryTalk Linx Gateway OPC DA service update rates

CPU and memory requirements for the FactoryTalk Linx Gateway OPC DA server increase as tags are set to active (up to the activation tag capacity) or as more clients connect to the server (up to the 20 connected client capacity). Rockwell Automation tests with the following update rates for a number of active tags.

Processor
Number of tags
Scan rate of all tags
Total CPU utilization
Single
70,000
All data changing value every 250 msec
75%
Dual-core
70,000
All data changing value every 250 msec
50%
Dual-core
70,000
All data changing value every 1000 msec
20%

These values are tested on a computer with a dual-core Intel® Core™ i3-2120 processor, 3.3 GHz, with 4G of RAM. The single core test is run using only one of the cores to provide a basis for comparison. FactoryTalk Linx Gateway and FactoryTalk Linx are installed and configured on the same computer for the test.

The largest impact on CPU utilization is the rate the data is changing even if the data server (in this case, FactoryTalk Linx) is local or remote to the FactoryTalk Linx Gateway.

The total amount of memory used for the runtime tests was approximately 700MB. Additional memory would be utilized if browsing occurred.

Tested FactoryTalk Linx Gateway OPC UA update rates

CPU and memory requirements for the FactoryTalk Linx Gateway OPC UA server increase as tags are set to active (up to the activation tag capacity) or as more clients connect to the server. Rockwell Automation tests with the following update rates for a number of active tags. This data is captured in FactoryTalk Linx Gateway version 6.21.00 with security disabled.

Number of Active Tags
Tested Update Rate (ms)
50,000
500
100,000
700
150,000
1000
200,000
1500
250,000
2000
300,000
2400
350,000
3000
400,000
3500
450,000
4000
500,000
4500

 

graphic
Note: This data was based on tests with the UA tag list disabled.

 

Number of Active Tags
Tested Update Rate (ms)
10,000
500
50,000
500
100,000
500
150,000
1000
200,000
2000
250,000
2000
300,000
2000
350,000
2000
400,000
2500
450,000
3000
500,000
4000

 

graphic
Note: This data was based on tests with the UA tag list enabled.

These values are tested on a computer with Win 10 enterprise 64 bit,  8G RAM, Intel® Xeon® CPU, E5-2699A v4 @ 2.40 GHz 2.39 GHz 4v CPU .

FactoryTalk Linx Gateway Security Certificate

When an OPC UA client connects to FactoryTalk Linx Gateway, FactoryTalk Linx Gateway provides a self-signed security certificate to the client as identification. Depending on the OPC UA client used in the system, you may need to manually approve the FactoryTalk Linx Gateway security certificate in the client to complete the connection.

Read service

When an OPC UA client subscription is in the process of being updated and a read request for the same item interrupts the delivery, the subscription request could deliver an older value after the results of the read request are delivered. Subsequent subscription responses will deliver updated values.

Security considerations

Service log on option

Unattended or silent install

Use command-line parameters to perform an unattended or silent installation of the software.

Installation Command-line parameters

The following table identifies the installation command-line parameters. Command-line parameters are case-insensitive. However, if a specified value includes a space, be sure to enclose the value in quotation marks (for example, "value with spaces").

Parameter
Description
/?
Displays the usage options for installation parameters.
/Q
Silent Install, install runs in a quiet mode without any user interface.
This parameter is recommended when deploying the software installation using an IT tool or script, and don’t expect any error or restart messages. When using this parameter, check the error codes, and respond as needed. For example, if the installation returns error code 1641, then the IT tool or script should restart the computer and relaunch the installation after restart.
This parameter is required if /QS is not specified.
/QS
Unattended Install, install runs in a quiet simple mode and shows progress through the UI, it does not accept any input but still shows errors or restart messages.
When using this parameter, the installation will stop and display a prompt if there are errors or restart messages. For example, if an immediate restart is required to complete the install, a restart message will be displayed to confirm the restart. The installation resumes automatically from the point of interruption after restart.
This parameter is required if /Q is not specified.
/IAcceptAllLicenseTerms
Acknowledges acceptance of the license terms.
This parameter is required for /Q or /QS parameters.
/AutoRestart
Automatically restarts the computer after the installation is complete. Used when a restart is required to complete the installation.
This parameter is optional. If this parameter is not used silent install (/Q) will return either error code 1641 or 3010 if a restart is required, and unattended install (/QS) will result in a confirmation prompt that must be agreed to before the installation is completed.
/Record
Records the installation options chosen to a recording file.
This parameter is optional.
/Playback
Plays back a recording file to specify the installation options.
This parameter is optional.
/SetupLanguage="value"
Specifies which language will be displayed during install process.
The value must be one of the following:
  • ENU
  • CHS
  • DEU
  • ESP
  • FRA
  • ITA
  • JPN
  • KOR
  • PTB
This parameter is optional. If this parameter is not used, the default language is the current user or operating system user interface language.
/IgnoreWarning
Specifies that the setup ignores warnings and continues.
This parameter is optional. If it is not specified, the setup exits when a warning occurs.
/ftsp-s
Specifies the FactoryTalk directory scope for restore. Only "Global" and "Local" scopes are supported.
This parameter is optional.
/ftsp-bak
Specifies the location where the restore file can be found.
This parameter is optional.
/ftsp-pp
Specifies the plain text used to decrypt the backup file.
This parameter is optional.
/ftsp-value=enable/disable
Specifies to enable or disable the option Require computer accounts for all client machines in Security Policy. The option is used to determine whether or not a client computer account must exist in the directory to login.
This parameter is optional.
/DirectoryServer
Specifies the directory server name.
This parameter is optional.
/Repair
Runs a repair operation on the installed products.
This parameter is optional.
/InstallDrive="value"
Specifies the install drive.
This parameter is optional. If this parameter is not used, the default install location is "C:\Program Files (x86)\Rockwell Software".
Some software restricts the installer to only change the drive the software is installed on. Use /? to determine which parameter is supported.
/Uninstall
Use to uninstall the product. This parameter is optional.
/Product
Specifies which sub-products will be installed.
  • Setup.exe /Product="Gateway"
Equal to Setup.exe /Product="Gateway Server OPC UA and DA (local or remote DA clients)". Both will install “Gateway Server OPC UA and DA (local or remote DA clients)”.
  • Setup.exe /Product="Gateway-L"
Equal to Setup.exe /Product="Gateway Server OPC UA and DA (only local DA clients)". Both will install "Gateway Server OPC UA and DA (only local DA clients)".
  • Setup.exe /Product="Remote Gateway"
Equal to Setup.exe /Product="Remote Gateway (DA Client remote configuration)". Both will install “Remote Gateway (DA Client remote configuration)”.

Examples

The following examples show how to use the installation commands.

Error codes

The following table identifies the error codes that can be returned by an installation.

Error Code
Value
Description
ERROR_SUCCESS
0
The installation completed successfully.
ERROR_INVALID_PARAMETER
87
One of the parameters was invalid.
ERROR_INSTALL_USEREXIT
1602
The installation was cancelled by the user.
ERROR_INSTALL_FAILURE
1603
A fatal error occurred during installation.
ERROR_BAD_CONFIGURATION
1610
The configuration data for this product is corrupt. Contact your support personnel.
ERROR_REBOOT_CONTINUE
1641
A restart is required to continue the installation.
ERROR_SUCCESS_REBOOT_REQUIRED
3010
A restart is required to complete the installation. After restarting, the product is successfully installed.
ERROR_REBOOT_PENDING
3012
Restart is pending. Restart the computer to continue the installation.
ERROR_SUCCESS_NOT_APPLICABLE
3013
The installation cannot proceed because the products are already installed.
ERROR_SUCCESS_WARNING_REBOOT
3014
The installation succeeded with warnings. Check the installation log file for details. To complete the installation, restart the computer.

VeriSign Universal Root Certification Authority certificate

If the VeriSign Universal Root Certification Authority certificate does not exist on the local computer, the certificate is installed while installing Rockwell Automation software. Use Microsoft Management Console (MMC) to view the certificate in Console Root > Certificates (Local Computer) > Trusted Root Certification Authorities > Certificates.

Mitigation for Microsoft DCOM Hardening patch

In response to Microsoft Distributed Component Object Model (DCOM) Hardening patch (MS KB5004442), the minimum DCOM authentication level used by Rockwell Automation products was raised to Packet Integrity.

IMPORTANT
Installing this product’s latest version with earlier unpatched versions of other FactoryTalk products or products using Classic OPC DA connections may cause a loss of connectivity due to the difference in DCOM authentication level used. For additional information, see the Knowledgebase Document ID: IN39461 - Microsoft DCOM Hardening Information TOC.

Microsoft releases the DCOM Hardening patch in response to CVE-2021-26414. This patch elevates the minimum DCOM authentication level that is required to establish a DCOM connection. DCOM is used by many Rockwell Automation products and may be affected by the change that is made by the Microsoft patch. For additional information about the affected Rockwell Automation products, see the Knowledgebase Document ID: PN1581 - Product Notification 2022-01-001 - Rockwell Automation products unable to establish proper DCOM connection after installing Microsoft DCOM Hardening patch (MS KB5004442).

"Meltdown" and "Spectre" Vulnerabilities

On January 3, 2018, a set of new hardware kernel level vulnerabilities, named "Meltdown" and "Spectre", were announced by researchers. Both Spectre and Meltdown are vulnerabilities that affect modern microprocessors allowing malicious processes to access the contents of restricted memory and therefore affect multiple generations of Central Processing Units (CPUs).

For an up-to-date briefing on how Meltdown and Spectre affect Rockwell Automation products, see Rockwell Automation Knowledgebase Document ID: PN1011 - Rockwell Automation Briefing on "Meltdown" and "Spectre" vulnerabilities.

Application Notes

This release has the following application notes.

The following are the application notes for FactoryTalk Linx Gateway version 6.31.00.

Tag’s data type limitation in Custom Namespace

If you do not use the Tag Browser to add or edit a tag in the Custom UA Namespace or Custom RTD/DDE Namespace editor, you must ensure that the tag’s data type is the same as the data source, such as the Logix controller, or OPC UA server connected via the FactoryTalk Linx OPC UA Connector.

If you change a tag’s data type in a controller, you must ensure that the tag's data type in the Custom UA Namespace or Custom RTD/DDE Namespace editor is the same as that in the controller. Otherwise, an error message “BadTypeMisMatch” appears in the UA clients.

Remote Proxy service

The Remote Proxy service does not support FactoryTalk View ME Transfer Utility.

The Remote Proxy service supports Ethernet and Backplane drivers from the FactoryTalk Linx Network Browser.

CIS Benchmarks test results

Rockwell Automation conducts tests using domain-joined computers configured according to CIS Benchmarks to help assure that software products perform as expected on computers that are hardened to industry best practices.

For more information about the guidelines and which products were tested against which CIS Benchmarks, see the Knowledgebase Document ID: QA63609 - Recommended guidelines for hardening software, computer, device, and network systems and infrastructure (CIS Benchmarks).

graphic
Note: If a product compliance with the benchmark is less than 100%, a link to a detailed spreadsheet is available. Download the spreadsheet to assist you in determining whether additional compensating controls are necessary.

FactoryTalk Linx Gateway version 6.31.00 has been tested on CIS Microsoft Windows 10 Enterprise (Release 21H1) Benchmark v1.12.0, CIS Microsoft Windows 10 Enterprise (Release 21H2) Benchmark v1.12.0, CIS Microsoft Windows Server 2019 Domain Server Benchmark v1.3.0, and CIS Microsoft Windows Server 2019 Domain Controller Benchmark v1.3.0.

Exceptions settings for FactoryTalk Linx Gateway version 6.31.00 are listed.

CIS Microsoft Windows 10 Enterprise (Release 21H1) Benchmark v1.12.0 and CIS Microsoft Windows 10 Enterprise (Release 21H2) Benchmark v1.12.0

CIS Microsoft Windows Server 2019 Domain Server Benchmark v1.3.0

CIS Microsoft Windows Server 2019 Domain Controller Benchmark v1.3.0

Array Data Request

When an OPC UA Client makes a subsequent request to an array beyond the last element previously requested, FactoryTalk Linx Gateway’s OPC UA service will initially return a "BadIndexRangeNoData" error. If the array is defined to accommodate the requested elements, the initial error response is replaced with the appropriate array data.

Certificate

When a user regenerates a certificate in FactoryTalk Linx Gateway version 6.21.00 or later, and then uninstall it with "Keep configuration when uninstall" selected, FactoryTalk Linx Gateway installed on the same computer later may not work. To avoid this problem, delete all the files in folder <C:\ProgramData\Rockwell\FactoryTalk Linx Gateway\PKI\own>, restart FactoryTalk Linx Gateway, and then regenerate an outgoing certificate.

The following certificates are installed while installing Rockwell Automation software.

FactoryTalk Linx Gateway unsupported data types

FactoryTalk Linx Gateway natively supports most but not all data types defined in a Logix controller. FactoryTalk Linx Gateway does not support accessing these types through DA, UA, DDE or RTD services:

Tested FactoryTalk Linx Gateway OPC DA service update rates

CPU and memory requirements for the FactoryTalk Linx Gateway OPC DA server increase as tags are set to active (up to the activation tag capacity) or as more clients connect to the server (up to the 20 connected client capacity). Rockwell Automation tests with the following update rates for a number of active tags.

Processor
Number of tags
Scan rate of all tags
Total CPU utilization
Single
70,000
Controller data values changing at 250 msec
75%
Dual-core
70,000
Controller data values changing at 250 msec
50%
Dual-core
70,000
Controller data values changing at 1000 msec
20%

 

graphic
Note: Many of the FactoryTalk services use change of state processing.  The high data value change rate used in this test was selected to place a high processing load on the system to evaluate the computer’s CPU impact.  Because each system has different operational requirements, testing should be performed to determine how a proposed system will operate.

These values are tested on a computer with a dual-core Intel® Core™ i3-2120 processor, 3.3 GHz, with 4G of RAM. The single core test is run using only one of the cores to provide a basis for comparison. FactoryTalk Linx Gateway and FactoryTalk Linx are installed and configured on the same computer for the test.

The largest impact on CPU utilization is the rate that the data is changing even if the data server (in this case, FactoryTalk Linx) is local or remote to the FactoryTalk Linx Gateway.

The total amount of memory used for the runtime tests was approximately 700 MB. Additional memory would be used if browsing occurred.

Tested FactoryTalk Linx Gateway OPC UA update rates

Rockwell Automation tests with the following update rates for a number of active tags. This data is captured in FactoryTalk Linx Gateway version 6.31.00 with security disabled.

CPU and memory requirements for the FactoryTalk Linx Gateway OPC UA server increase as tags are set to active (up to the activation tag capacity) or as more clients connect to the server.

Number of Active Tags
Requested Rate (s)
Achieved Update Rate (s)
50,000
0.5
0.561
100,000
0.5
0.759
150,000
0.5
1.023
200,000
0.5
1.287
250,000
0.5
1.635
300,000
0.5
1.996
350,000
0.5
2.403
400,000
0.5
2.777
450,000
0.5
3.192
500,000
0.5
3.327

 

graphic
Note: This data was based on tests with the Folder with scalar data enabled in the UA server. This data is provided as an example to show how tag quantity will impact the speed that data can be delivered. The test did not verify all value changes that were delivered. Because each system has different operational requirements, testing should be performed to determine how a proposed system will operate.
Number of Active Tags
Requested Rate (s)
Achieved Update Rate (s)
10,000
0.5
0.5
50,000
0.5
0.5
100,000
0.5
0.5
150,000
0.5
1
200,000
0.5
2
250,000
0.5
2
300,000
0.5
2
350,000
0.5
2
400,000
0.5
2.5
450,000
0.5
3
500,000
0.5
4

 

graphic
Note: This data was based on tests with the UA tag list enabled. This data is provided as an example to show how tag quantity will impact the speed that data can be delivered. The test did not verify all value changes that were delivered. Because each system has different operational requirements, testing should be performed to determine how a proposed system will operate.
Number of Active Tags
Requested Rate (s)
Achieved Update Rate (s)
10,000
0.5
0.5
50,000
0.5
0.57
100,000
0.5
1.003
150,000
0.5
1.335
200,000
0.5
1.977
250,000
0.5
2.257
300,000
0.5
2.557
350,000
0.5
2.885
400,000
0.5
2.351
450,000
0.5
3.433
500,000
0.5
4.006

 

graphic
Note: This data was based on tests with the Custom namespace enabled. This data is provided as an example to show how tag quantity will impact the speed that data can be delivered. The test did not verify all value changes that were delivered. Because each system has different operational requirements, testing should be performed to determine how a proposed system will operate.

These values are tested on a computer with Win 10 enterprise 64 bit, 8G RAM, Intel® Xeon® CPU, E5-2699A v4 @ 2.40 GHz 2.39 GHz 4v CPU.

Requestor’s subscription rate recommendation

In a FactoryTalk system, data moves from a source like a controller connected to FactoryTalk Linx to a software client when a data item’s value has changed. Once, changes are detected, the data values are transferred between multiple components or services. The services use the subscription rate from the requestor to initiate a processing thread to transfer the data to its next destination in the system. Small processing delays by components, network delivery time, a high number of values changing at once, or a heavily loaded system can cause data to be processed and delivered slower than the requested rate. If the source data value changes faster than twice the subscription rate, a newer data value could likely overwrite a previous data value as it travels between the services.

In some cases, sampling at a rate faster than half of the speed of the value changes can help to ensure that data value changes are detected by the requester. Also balancing the data subscriptions across multiple computers and services can reduce processing and delivery delays.

FactoryTalk Linx Gateway Security Certificate

When an OPC UA client connects to FactoryTalk Linx Gateway, FactoryTalk Linx Gateway provides a self-signed security certificate to the client as identification. Depending on the OPC UA client used in the system, you may need to manually approve the FactoryTalk Linx Gateway security certificate in the client to complete the connection.

Read service

When an OPC UA client subscription is in the process of being updated and a read request for the same item interrupts the delivery, the subscription request could deliver an older value after the results of the read request are delivered. Subsequent subscription responses will deliver updated values.

Security considerations

Service log on option

Unattended or silent install

Use command-line parameters to perform an unattended or silent installation of the software.

Installation Command-line parameters

The following table identifies the installation command-line parameters. Command-line parameters are case-insensitive. However, if a specified value includes a space, be sure to enclose the value in quotation marks (for example, "value with spaces").

Parameter
Description
/?
Displays the usage options for installation parameters.
/Q
Silent Install, install runs in a quiet mode without any user interface.
This parameter is recommended when deploying the software installation using an IT tool or script, and don’t expect any error or restart messages. When using this parameter, check the error codes, and respond as needed. For example, if the installation returns error code 1641, then the IT tool or script should restart the computer and relaunch the installation after restart.
This parameter is required if /QS is not specified.
/QS
Unattended Install, install runs in a quiet simple mode and shows progress through the UI, it does not accept any input but still shows errors or restart messages.
When using this parameter, the installation will stop and display a prompt if there are errors or restart messages. For example, if an immediate restart is required to complete the install, a restart message will be displayed to confirm the restart. Installation resumes automatically from the point of interruption after restart.
This parameter is required if /Q is not specified.
/IAcceptAllLicenseTerms
Acknowledges acceptance of the license terms.
This parameter is required for /Q or /QS parameters.
/AutoRestart
Automatically restarts the computer after the installation is complete. Used when a restart is required to complete the installation.
This parameter is optional. If this parameter is not used silent install (/Q) will return either error code 1641 or 3010 if a restart is required, and unattended install (/QS) will result in a confirmation prompt that must be agreed to before the installation is completed.
/Record
Records the installation options chosen to a recording file.
This parameter is optional.
/Playback
Plays back a recording file to specify the installation options.
This parameter is optional.
/SetupLanguage="value"
Specifies which language will be displayed during the install process.
The value must be one of the following:
  • ENU
  • CHS
  • DEU
  • ESP
  • FRA
  • ITA
  • JPN
  • KOR
  • PTB
This parameter is optional. If this parameter is not used, the default language is the current user or operating system user interface language.
/IgnoreWarning
Specifies that the setup ignores warnings and continues.
This parameter is optional. If it is not specified, the setup exits when a warning occurs.
/ftsp-s
Specifies the FactoryTalk directory scope for restore. Only "Global" and "Local" scopes are supported.
This parameter is optional.
/ftsp-bak
Specifies the location where the restore file can be found.
This parameter is optional.
/ftsp-pp
Specifies the plain text used to decrypt the backup file.
This parameter is optional.
/ftsp-value=enable/disable
Specifies to enable or disable the option Require computer accounts for all client machines in Security Policy. The option is used to determine whether or not a client computer account must exist in the directory to log in.
This parameter is optional.
/FTSPWebAuth="value"
Specifies that the installation includes the FactoryTalk Web Authentication Server.
This parameter is optional.
The value must be one of the following:
  • Yes
If the value is Yes, the FactoryTalk Web Authentication Server will be installed. The FactoryTalk Reverse Proxy will also be installed as it is required for operation of the FactoryTalk Web Authentication Server.
  • No
If the value is No, the FactoryTalk Web Authentication Server will not be installed.
/ReverseProxy="value"
Specifies that the installation includes the FactoryTalk Reverse Proxy.
This parameter is optional.
The value must be one of the following:
  • Yes
If the value is Yes, the FactoryTalk Reverse Proxy will be installed.
  • No
If the value is No, the FactoryTalk Reverse Proxy will not be installed.
/FTSPWebEventServer="value"
Specifies that the installation includes the FactoryTalk Web Event Server.
This parameter is optional.
The value must be one of the following:
  • Yes
If the value is Yes, the FactoryTalk Web Event Server will be installed.
  • No
If the value is No, the FactoryTalk Web Event Server will not be installed.
/DirectoryServer
Specifies the directory server name.
This parameter is optional. If it is not specified, the setup turns on HTTPS for communication, and a TLS certificate must be configured after installation.
/NoHTTPS
Specifies that the setup turns off HTTPS.
This parameter is optional. If it is not specified, the setup turns on HTTPS for communication, and a TLS certificate must be configured after installation.
/Repair
Runs a repair operation on the installed products.
This parameter is optional.
/InstallDrive="value"
Specifies the install drive.
This parameter is optional. If this parameter is not used, the default install location is "C:\Program Files (x86)\Rockwell Software".
Some software restricts the installer to only change the drive the software is installed on. Use /? to determine which parameter is supported.
/Uninstall
Use to uninstall the product. This parameter is optional.

Examples

The following examples show how to use the installation commands.

Error codes

The following table identifies the error codes that can be returned by an installation.

Error Code
Value
Description
ERROR_SUCCESS
0
The installation completed successfully.
ERROR_INVALID_PARAMETER
87
One of the parameters was invalid.
ERROR_INSTALL_USEREXIT
1602
The installation was canceled by the user.
ERROR_INSTALL_FAILURE
1603
A fatal error occurred during installation.
ERROR_BAD_CONFIGURATION
1610
The configuration data for this product is corrupt. Contact your support personnel.
ERROR_REBOOT_CONTINUE
1641
A restart is required to continue the installation.
ERROR_SUCCESS_REBOOT_REQUIRED
3010
A restart is required to complete the installation. After restarting, the product is successfully installed.
ERROR_REBOOT_PENDING
3012
Restart is pending. Restart the computer to continue the installation.
ERROR_SUCCESS_NOT_APPLICABLE
3013
The installation cannot proceed because the products are already installed.
ERROR_SUCCESS_WARNING_REBOOT
3014
The installation succeeded with warnings. Check the installation log file for details. To complete the installation, restart the computer.

VeriSign Universal Root Certification Authority certificate

If the VeriSign Universal Root Certification Authority certificate does not exist on the local computer, the certificate is installed while installing Rockwell Automation software. Use Microsoft Management Console (MMC) to view the certificate in Console Root > Certificates (Local Computer) > Trusted Root Certification Authorities > Certificates.

Mitigation for Microsoft DCOM Hardening patch

In response to Microsoft Distributed Component Object Model (DCOM) Hardening patch (MS KB5004442), the minimum DCOM authentication level used by Rockwell Automation products was raised to Packet Integrity.

IMPORTANT
Installing this product’s latest version with earlier unpatched versions of other FactoryTalk products or products using Classic OPC DA connections may cause a loss of connectivity due to the difference in DCOM authentication level used. For additional information, see the Knowledgebase Document ID: IN39461 - Microsoft DCOM Hardening Information TOC.

Microsoft releases the DCOM Hardening patch in response to CVE-2021-26414. This patch elevates the minimum DCOM authentication level that is required to establish a DCOM connection. DCOM is used by many Rockwell Automation products and may be affected by the change that is made by the Microsoft patch. For additional information about the affected Rockwell Automation products, see the Knowledgebase Document ID: PN1581 - Product Notification 2022-01-001 - Rockwell Automation products unable to establish proper DCOM connection after installing Microsoft DCOM Hardening patch (MS KB5004442).

"Meltdown" and "Spectre" Vulnerabilities

On January 3, 2018, a set of new hardware kernel-level vulnerabilities, named "Meltdown" and "Spectre", were announced by researchers. Both Spectre and Meltdown are vulnerabilities that affect modern microprocessors allowing malicious processes to access the contents of restricted memory and therefore affect multiple generations of Central Processing Units (CPUs).

For an up-to-date briefing on how Meltdown and Spectre affect Rockwell Automation products, see Rockwell Automation Knowledgebase Document ID: PN1011 - Rockwell Automation Briefing on "Meltdown" and "Spectre" vulnerabilities.

Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.

Copyright © 2026 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please click here.
Trademarks not belonging to Rockwell Automation are property of their respective companies.