This release has the following requirements.
The following are the system requirements for FactoryTalk View SE version 13.00.00 (CPR 9 SR 13).
Hardware requirements
The following is a sample specification of computer hardware to run FactoryTalk View SE applications aligned with the hardware used in product development testing.
|
Type
|
Description
|
CPU
|
RAM
|
|
Operator Workstation
|
FactoryTalk View SE Client
or
FactoryTalk View SE Station
|
Intel® Core™ i5 Standard
Power processor
|
4 GB
|
|
Engineering Workstation
|
FactoryTalk View Studio Enterprise
FactoryTalk Linx
Studio 5000
|
Intel Core i5 Standard Power
processor
|
8 GB
|
|
Application Server
|
FactoryTalk View SE server
FactoryTalk View Studio Enterprise
FactoryTalk Alarms and Events
tag-based server
FactoryTalk Linx data server with
FactoryTalk Alarms and Events
enabled
|
Smaller systems:
Intel Core i5 Standard Power
processor
|
4 GB
|
| Medium to larger systems:
Quad core Intel Core Xeon
family processor
|
8 GB
|
Software requirements
Operating systems
FactoryTalk View SE is tested on the following operating systems:
* For more information, see Rockwell Automation Knowledgebase Document ID: IN4493 - Windows 10 Support for the FactoryTalk Suite of Rockwell Software products and IN4718 - Windows Server 2016 Support for the FactoryTalk Suite of Rockwell Software products.
** This operating system is supported with the Allen-Bradley® 61xx family of industrial computers and CompactLogix™ 5480 family of controllers.
Domain controller requirements
The following operating systems are supported for use as domain controllers for FactoryTalk View SE client computers. Using a domain is recommended for applications that include more than 10 computers. If your application includes 10 or fewer computers, they can be organized in a workgroup.
Rockwell Automation Test Environment
Rockwell Automation tests software products under a standard configuration of operating systems and antivirus software. For additional information, see the Knowledgebase Document ID: PN24 - Rockwell Software Products and Antivirus Software.
Supported browsers
The following web browsers have been tested and are supported for use with this release:
Security requirements
To help meet secure system design requirements, review these publications:
To learn about implementing CIP Security, see CIP Security with Rockwell Automation Products (publication SECURE-AT001).
This release includes the following system features.
FactoryTalk View SE version 13.00.00 has the following new and enhanced features.
New features
Enhanced features
This release corrects the following anomalies.
The following list identifies the anomalies corrected in FactoryTalk View SE version 13.00.00.
This release has the following known anomalies.
These anomalies are from previous releases but are still known in this release.
Datalogoff <name of datalog> and then the command
Datalogon <name of datalog>.Pause 5 command between the launch of each SE client file. This will allow the start of each SE client to be offset from each other.HKEY_USERS\.DEFAULT\Software\Rockwell Software\RSView Enterprise\Data Log
HKEY_USERS\S-1-5-18\Software\Rockwell Software\RSView Enterprise\Data Log
This issue occurs due to the unintended handling of temporary files created when displays are opened in either FactoryTalk View SE client or FactoryTalk View Studio, especially within the Windows Remote Desktop Server (RDS) environment. For specific causes and associated solutions, see Knowledgebase Document ID: BF27588 - FactoryTalk View SE - No longer able to open displays in FactoryTalk View Studio or FactoryTalk View SE Client.
This release has the following functional changes from the previous release.
FactoryTalk View SE version 13.00.00 has the following changes in functionality since the last release.
HTTPS enabled by default
If you install Studio Enterprise, Site Edition Server, or FactoryTalk ViewPoint SE on a computer with no FactoryTalk View component installed, the installation enables HTTPS by default.
If HTTPS is enabled, you must configure a TLS certificate after installation. If you do not configure the certificate, there will be unexpected errors when operating FactoryTalk View SE components. For details on configuring a TLS certificate, see FactoryTalk View Site Edition Installation Guide.
This release has the following application notes.
The following are the application notes for FactoryTalk View SE version 13.00.00.
Impact of Microsoft deprecating VBScript
Microsoft announced the phased deprecation of VBScript in 2024. VBScript is now an optional feature beginning in Windows 11 24H2 and Windows Server 2025. Many FactoryTalk software products released before September 1, 2026, use VBScript during installation.
FactoryTalk View SE versions 16.00.00 and earlier require VBScript for installation. Installation will fail if VBScript is not enabled.
To mitigate the problem, enable VBScript manually. For more information, see the Knowledgebase Document ID: IN41397 - Impact of Microsoft deprecating VBScript. FactoryTalk software products released after September 1, 2026, no longer rely on VBScript.
HTTPS enabled by default
If you install Studio Enterprise, Site Edition Server, or FactoryTalk ViewPoint SE on a computer with no FactoryTalk View component installed, the installation enables HTTPS by default.
If HTTPS is enabled, you must configure a TLS certificate after installation. If you do not configure the certificate, there will be unexpected errors when operating FactoryTalk View SE components. For details on configuring a TLS certificate, see FactoryTalk View Site Edition Installation Guide.
Mitigation for Microsoft DCOM Hardening patch
In response to Microsoft Distributed Component Object Model (DCOM) Hardening patch (MS KB5004442), the minimum DCOM authentication level used by Rockwell Automation products was raised to Packet Integrity.
|
IMPORTANT
|
Installing this product’s latest version with earlier unpatched
versions of other FactoryTalk products or products using Classic
OPC DA connections may cause a loss of connectivity due to the
difference in DCOM authentication level used. For additional
information, see the Knowledgebase Document ID: IN39461 -
Microsoft DCOM Hardening Information TOC.
|
Microsoft releases the DCOM Hardening patch in response to CVE-2021-26414. This patch elevates the minimum DCOM authentication level that is required to establish a DCOM connection. DCOM is used by many Rockwell Automation products and may be affected by the change that is made by the Microsoft patch. For additional information about the affected Rockwell Automation products, see the Knowledgebase Document ID: PN1581 - Product Notification 2022-01-001 - Rockwell Automation products unable to establish proper DCOM connection after installing Microsoft DCOM Hardening patch (MS KB5004442).
Change in operating system support
Beginning in this release, the product installer prevents installation on all 32-bit versions of Windows operating systems (for example, Windows 10, 32-bit) and any Windows 7 operating system (for example, Windows 7 Professional, 64-bit).
Considerations for application server host computers
In a network application, it is possible for a single server computer that meets the recommended requirements to host all of the following components:
If a network application requires multiple HMI servers, data servers, or alarm servers, to distribute the load, it is recommended that you install the necessary software and run the servers on multiple host computers.
For information about setting up redundant FactoryTalk View SE servers, see FactoryTalk View Site Edition User’s Guide.
FactoryTalk Diagnostics
FactoryTalk Diagnostics cannot log to a remote database using Microsoft Access. You can only log to a local database using Microsoft Access.
Find and Replace
If an HMI server at the root node of an SE Network distributed application has the same name as the application itself, the Find and Replace feature search results might include the application name even though you performed the search at the HMI server level.
Floating-point operations
Floating-point numbers may not precisely represent all real numbers. Floating points only has six digits of precision. As a result, expressions based on floating-point arithmetic operations may not evaluate as expected. This is a side effect of how the CPU represents the floating-point data. For this reason, in certain cases you may experience loss of precision and get unexpected results of floating-point operations.
KEPServer
If you are using KEPServer Enterprise as an OPC server with FactoryTalk View version 9.00.00 or later and using an HMI tag to connect to a third-party device, you will not be able to access the tag value. The cause is that the security enhancements in FactoryTalk View version 9.00.00 or later affect the communications with third-party devices. To access the tag value, additional Distributed Component Object Model (DCOM) configuration is required for KEPServer Enterprise on the computers.
For more information about the configuration, see Appendix, "Troubleshoot KEPServer Enterprise" in the FactoryTalk View SE Installation Guide.
Pre-installation configuration
Before you install FactoryTalk View SE, there are a number of steps required to set up the installation environment. This will help ensure that the installation proceeds smoothly and that your new or upgraded FactoryTalk system operates as expected. For detailed information about pre-requisites before installation, see Chapter 3, Pre-installation configuration of FactoryTalk View Site Edition Installation Guide.
Security requirements
For information on the security considerations when using Rockwell Automation products, including
System sizing recommendations
When you design and set up a FactoryTalk system, we recommend using the following guidelines. If you find that your system needs to expand beyond these guidelines, contact your Rockwell Automation sales or distributor representative to discuss your application design.
|
Component
|
Recommended guidelines
|
|
FactoryTalk Alarms and Events
|
|
|
FactoryTalk Alarms and Events servers per FactoryTalk Directory
|
10 non-redundant servers or 10 redundant server pairs1
|
|
FactoryTalk tag-based alarms per server
|
20,0002
|
|
Logix device-based alarms per server
|
10,0003
|
|
Total alarms per FactoryTalk Directory
|
100,0004
|
|
FactoryTalk Linx
|
|
|
FactoryTalk Linx data servers per FactoryTalk Directory
|
10 non-redundant servers or 10 redundant server pairs1
|
|
Total device tags per FactoryTalk Directory
|
1,000,0005
|
|
Tags per FactoryTalk Linx data server
|
100,0005
|
|
FactoryTalk View SE
|
|
|
HMI servers per FactoryTalk Directory
|
10 non-redundant servers or 10 redundant server pairs1
|
|
HMI tags per HMI server
|
40,0006
|
|
Total data logged tags per HMI server (1 second scan rate)
|
5,000
|
|
FactoryTalk View SE client sessions simultaneously connected to
the application
|
1205
|
|
FactoryTalk ViewPoint SE servers per application
|
4
|
|
FactoryTalk ViewPoint SE concurrent clients per ViewPoint server
|
50
|
| |
Tag Browser
If you rename an HMI server while you are deploying an application, you may need to restart the computer in order to have the HMI tags show up in the Tag Browser.
Tools and utilities
Trend objects
The Trend objects cannot get the oldest data from FactoryTalk Historian server when you click the Oldest Data button.
TrendPro objects
UAC support
Turning off User Account Control (UAC) is not recommended.
|
This action
|
Prompts for authentication or confirmation before running this
program
|
|
Configuring Internet Information Services (IIS)
|
RSViewWebManager.exe
CustomWebSite.exe
|
|
Updating Samples application directory
information
|
RefreshSampleApplication.exe
|
|
End processes
|
VSClean.exe
|
|
DeskLock
|
DeskLock2000.exe
|
|
Legacy Tag Database Conversion
|
LegacyTagDBConvertTool.exe
|
VeriSign Universal Root Certification Authority certificate
If the VeriSign Universal Root Certification Authority certificate does not exist on the local computer, the certificate is installed while installing Rockwell Automation software. Use Microsoft Management Console (MMC) to view the certificate in Console Root > Certificates (Local Computer) > Trusted Root Certification Authorities > Certificates.
Unattended installation
Use command-line parameters to perform an unattended or silent installation of the software.
Command-line parameters
The following table identifies the installation command-line parameters. Command-line parameters are case-insensitive. However, if a specified value includes a space, be sure to enclose the value in quotation marks (for example, "value with spaces").
|
Parameter
|
Description
|
|
/?
|
Displays the usage options for installation parameters.
|
|
/Q
|
Silent Install, install runs in a quiet mode without any user interface.
This parameter is recommended when deploying the software installation
using an IT tool or script, and don’t expect any error or restart messages.
When using this parameter, check the error codes, and respond as needed.
For example, if the installation returns error code 1641, then the IT tool or
script should restart the computer and relaunch the installation after restart.
This parameter is required if /QS is not specified.
|
|
/QS
|
Unattended Install, install runs in a quiet simple mode and shows progress
through the UI, it does not accept any input but still shows error or restart
messages.
When using this parameter, the installation will stop and display a prompt if
there are error or restart messages. For example, if an immediate restart is
required to complete the install, a restart message will be displayed to confirm
the restart. Installation resumes automatically from the point of interruption
after restart.
This parameter is required if /Q is not specified.
|
|
/IAcceptAllLicenseTerms
|
Acknowledges acceptance of the license terms.
This parameter is required for /Q or /QS parameters.
|
|
/AutoRestart
|
Automatically restarts the computer after the installation is complete. Used
when a restart is required to complete the installation.
This parameter is optional. If this parameter is not used, silent install (/Q) will
return either error code 1641 or 3010 if a restart is required, and unattended
install (/QS) will result in a confirmation prompt that must be agreed to before
the installation is completed.
|
|
/Record
|
Records the installation options chosen to a recording file.
This parameter is optional.
|
|
/Playback
|
Plays back a recording file to specify the installation options.
This parameter is optional.
|
|
/Repair
|
Runs a repair operation on the installed products.
This parameter is optional.
|
|
/Uninstall
|
Uninstalls the product.
|
|
/SetupLanguage="value"
|
Specifies which language will be displayed during install process.
The value must be the one of the following:
This parameter is optional. If this parameter is not used, the default language
is the current user or operating system user interface language.
|
|
/Product="value"
|
Specifies which sub-products will be installed.
This parameter is required.
For FactoryTalk View ME, the value must be one of the following:
For FactoryTalk View SE, the value must be one of the following:
|
|
/ProductLanguage="value"
|
Specifies the language version of the software being installed.
The value must be one of the following:
This parameter is optional. If this parameter is not used, the default language
is the same as the setup language.
If the software does not support multiple languages, this parameter is not
available.
|
|
/InstallDrive="value"
|
Specifies the installation drive.
This parameter is optional. If this parameter is not used, the default install
drive is C:.
|
|
/IgnoreWarning
|
Specifies that the setup ignores warnings and continues.
This parameter is optional. If it is not specified, the setup exits when a
warning occurs.
|
|
/SerialNumber="value"
|
Specifies the serial number of the software being installed. This is used to
activate the software during installation.
This parameter is optional. If it is not specified, the software must be activated
manually after installation if activation is required.
Some software does not require activation. If activation is not required, this
parameter is not available.
|
|
/ProductKey="value"
|
Specifies the product key used to get activation keys during installation.
This parameter is optional. If it is not specified, the software must be activated
manually after installation if activation is required.
Some software does not require activation. If activation is not required, this
parameter is not available.
|
|
/Version="value"
|
Specifies the version of the software to activate, which corresponds to the
product version associated with the SerialNumber and ProductKey.
This parameter is optional. If it is not specified, the installer will use the most
recent product version available.
Some software does not require activation. If activation is not required, this
parameter is not available.
|
|
/DirectoryServer="value"
|
Specifies the FactoryTalk network directory if you are using a distributed
system.
This parameter is optional. If it is not specified, the software will use its current
computer as the FactoryTalk Directory server.
The value must be the host name of the FactoryTalk Directory server.
|
|
/NoHTTPS
|
Specifies that the setup turns off HTTPS.
This parameter is optional. If it is not specified, the setup turns on HTTPS for
communication, and a TLS certificate must be configured after installation.
|
Error codes
The following table identifies the error codes that can be returned by an installation.
|
Error Code
|
Value
|
Description
|
|
ERROR_SUCCESS
|
0
|
The installation completed successfully.
|
|
ERROR_INVALID_PARAMETER
|
87
|
One of the parameters was invalid.
|
|
ERROR_INSTALL_USEREXIT
|
1602
|
The installation was canceled by the user.
|
|
ERROR_INSTALL_FAILURE
|
1603
|
A fatal error occurred during installation.
|
|
ERROR_BAD_CONFIGURATION
|
1610
|
The configuration data for this product is corrupt. Contact your
support personnel.
|
|
ERROR_SUCCESS_REBOOT_INITIATED
|
1641
|
The installer has initiated a restart. After restart, the installation
will continue.
|
|
ERROR_SUCCESS_REBOOT_REQUIRED
|
3010
|
A restart is required to complete the installation. After restart,
the product is successfully installed.
|
|
ERROR_REBOOT_PENDING
|
3012
|
Restart pending. Restart the computer for the installation to
continue.
|
|
ERROR_SUCCESS_NOT_APPLICABLE
|
3013
|
The installation cannot proceed because the products are
already installed.
|
|
ERROR_SUCCESS_WARNING_REBOOT
|
3014
|
The installation succeeded with warnings. Check the installation
log file for details. To complete the installation, restart the
computer.
|