Release Notes

More information: PowerFlex® 525 Site
Version 7.001 (released 12/2020)

Catalog Number PowerFlex 525 (series A)

These release notes describe version information for PowerFlex 525, version 7.001 (released 12/2020).

Features

This release includes the following system features.

PowerFlex 525 Synchronous Reluctance Motor Control

System Feature first identified as of PowerFlex® 525 Drive Firmware Revision 7.001

Catalog Number: 25B

This firmware introduces the Synchronous Reluctance Motor control within PF525 drive by adding Synchronous Reluctance Motor algorithm and code optimization.

A new option 5: SynRm is added to parameter P039 [Torque Perf Mode] to enable the use of SynRm control.

For more information on the related and new parameters, see the PowerFlex 520-Series Adjustable Frequency AC Drive user manual, publication 520-UM001.

Corrected Anomalies in This Release

This release corrects the following anomalies.

PowerFlex 525 issues with F114 faults (PCBANOM-1452)

Corrected Anomaly with Firmware Revision 7.001

Catalog Number: 25B

Enhanced with PowerFlex® 525 drive Firmware Revision 7.001 to strengthen the immunity of the module towards F114 faults.

PowerFlex 525 with onboard NIC using BOOTP does not receive reply from Stratix 2500 (PCBANOM-2790)

Corrected Anomaly with Firmware Revision 7.001

Catalog Number: 25B

The communication issue between PowerFlex® 525 and Stratix® 2500 is corrected with PowerFlex 525 firmware revision 7.001 and later.

USB connection is unresponsive on Windows 8 and 10 (PCBANOM-1471)

Corrected Anomaly with Firmware Revision 7.001

Known Anomaly first identified as of Firmware Revision 4.001

Catalog Number: 25B

PowerFlex® 525 with firmware revision 7.001 and later supports the USB application with Windows® 8 and 10.

  

Application Notes

This release has the following application notes.

Use ControlFLASH and ControlFLASH Plus to Update Your Firmware

For instructions on how to install ControlFLASH™ and ControlFLASH Plus software and upgrade your drive firmware by using these software tools, see these publications:

Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.

Copyright © 2026 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please click here.
Trademarks not belonging to Rockwell Automation are property of their respective companies.