Release Notes
RA Library of Process Objects, Application Templates, Application Code Manager Library, Tools & Utilities, and Integration with
Version 3.50.11 (released 10/2018)
Catalog Number Process Library
These release notes describe version information for Process Library, version 3.50.11 (released 10/2018).
Known Anomalies from Previous Releases
These anomalies are from previous releases but are still known in this release.
Corrected Anomaly with PlantPAx Process Library version 4.00.02
P_ValveSO Handling of Simultaneous Commands
Known Anomaly First Identified as of PlantPAx® Process Library version 1.00.00
When P_ValveSO receives simultaneous Open and Close commands, it alternates
between closing and opening, with the output toggling.
How Corrected: Logic was modified so that in the event of simultaneous commands, the
command for the de-energized (fail) state is the one accepted.
Corrected Anomaly with PlantPAx Process Library version 4.00.02
Read from Online Configuration Spreadsheet
Known Anomaly First Identified as of PlantPAx® Process Library version 3.00.00
Attempt to read configuration data from a controller fails with the following error
message:
Click OK for the following message:
By clicking OK, subsequent messages appear about location of cells which failed to read
and overall failure of the function.
However, the ‘Send To CLX’ function works properly, and once you do a successful
‘Send To CLX’, then the ‘Read From CLX’ function begins to work properly.
This only affects the Premier Integration Online Configuration Tool spreadsheet. The
Process Library Online Configuration Tool spreadsheet works correctly.
The spreadsheet’s Visual Basic for Applications (VBA) code associated with the Read
From CLX function was corrected to remove an improper VAR initialization.
Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.
Copyright © 2024 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please
click here.Trademarks not belonging to Rockwell Automation are property of their respective companies.