Release Notes

Connected Components Workbench (CCW) Developer Edition single software to program, simulate, configure, and visualize.
Version 11.00.00 (released 3/2018)

Catalog Number Connected Components Workbench - Dev Ed 

These release notes describe version information for Connected Components Workbench - Dev Ed, version 11.00.00 (released 3/2018).

Requirements

This release has the following requirements.

The following are the system requirements for Connected Components Workbench version 11.00.00.

Hardware requirements

To use this release of Connected Components Workbench software effectively, your personal computer should meet the following minimum hardware requirements. Using a computer exceeding the recommended characteristics will improve performance.

Software requirements

This release is supported on the following operating systems:

Important:
Attempting to install Connected Components Workbench on a computer running Windows 7 without Service Pack 1 or later will fail.

Connected Components Workbench software has dependencies upon the following software components. These components will be installed with the Connected Components Workbench software if they are not already present and updated if required.

Important:
Uninstalling the Connected Components Workbench software does not remove these components. After verifying that other software is not relying on them, they can be removed manually.

Features

This release includes the following system features.

Connected Components Workbench version 11.00.00 software has the following new and enhanced features:

New features

The following new features are introduced in this release:

Enhanced features
The following features are modified in this release to improve performance or usability:

    For controller project version 11.00.00 and later, the fault diagnostic view is upgraded to show the last seven recoverable and last seven non-recoverable faults with the POU locations if available.

    Build error will not occur if create more than 128 UDFB/UDF local variables. The number of UDFB/UDF local variables are not limited.

Corrected Anomalies in This Release

This release corrects the following anomalies.

The following list identifies the anomalies corrected in Connected Components Workbench version 11.00.00.

    In this release, the Current Program Updater checking cycle changed to 30 days. The dependency is Connected Components Workbench 11.00.00 is the first Rockwell Automation product with Current Program Updater installed. If other Rockwell Automation products or Connected Components Workbench earlier version has been installed, the 24 hours update checking cycle will not change.
    For newly created projects using Connected Components Workbench 11.00.00 and later, ladder logic branch execution will not depend on the order of parallel branches, which is the same as MicroLogix controllers.

Known Anomalies in This Release

This release has the following known anomalies.

Functional Changes

This release has the following functional changes from the previous release.

Connected Components Workbench version 11.00.00 has the following changes in functionality since the last release:

    The Adobe® Acrobat® Reader® is removed from Connected Components Workbench installation media and may need to be installed manually from the Adobe website https://get.adobe.com/reader/.

    When updating the existing installation, by default, the products are selected if they have been installed. Clear the product you want to uninstall, or select the product you want to install, and click Install.
    By default, the cross reference data will not be loaded when opening the project. The data will be loaded when opening the Cross Reference Browser or Unused Variable Browser.

Application Notes

This release has the following application notes.

The following are the application notes for Connected Components Workbench 11.00.00.

Restarts during install of Connected Components Workbench software

Some Microsoft components may require a restart before the full Connected Components Workbench software installation is complete. If the Connected Components Workbench software does not install completely, restart the computer, the Connected Components Workbench software automatically continues installing.

Install of Connected Components Workbench version 11.00.00 software

If you have a previous version of Connected Components Workbench software installed, it is recommended to :

To install the Connected Components Workbench software:

  1. Download the current version of Connected Components Workbench software (Standard or Developer Edition).
  2. Launch Setup.exe.
  3. You must manually install .NET Framework 3.5 SP1 if you are using Windows 8, Windows 8.1, Windows 10, Windows Server 2012, Windows Server 2012 R2, or Windows Server 2016.
  4. On the Connected Components Workbench Setup dialog box, select the products which you want to install, or specify a different drive where you want to install the software, and then click Next. By default all products are selected and installed with the Connected Components Workbench software. To remove a product or language from the current installation, clear the check box.
  5. (optional) If installing the Developer Edition, enter the product serial number when prompted, and click Install.
  6. On the End-User License Agreements dialog box, read the agreements, and click Accept all to continue the installation, or click Decline to return to the previous page.
  7. (optional) If there are multiple Ethernet adapters in the computer, select one as the default from the popup window. Silent install mode will not provide the selection during installing, configure it in RSLinx Classic after installation completes.
  8. When prompted to restart your computer during the installation, click Restart now to restart your computer and continue the installation, or Restart later to suspend and exit the installation.
  9. On the That's it! dialog box, click Close to exit the installation. Meanwhile, you can also:

  1. The Connected Components Workbench installation is complete.

To upgrade an existing installation:

  1. Stop your current version of Connected Components Workbench.
  1. Perform the installation steps in the order presented on the screen.
  2. Modify the products you want to install or uninstall.

  1. Click Install.
  2. Restart your computer to complete the update.

Unattended or silent install

Use command-line parameters to perform an unattended or silent installation of the software.

Command-line parameters

The following table identifies the installation command-line parameters. Command-line parameters are case-insensitive. However, if a specified value includes a space, be sure to enclose the value in quotation marks (for example, "value with spaces").

tr>
Parameter
Description
/?
Displays the usage options for installation parameters.
/Q
Silent Install, install runs in a quiet mode without any user interface.
This parameter is recommended when deploying the software installation using an IT tool or script, and don’t expect any error or restart messages. When using this parameter, check the error codes, and respond as needed. For example, if the installation returns error code 1641, then the IT tool or script should restart the computer and relaunch the installation after restart.
This parameter is required if /QS is not specified.
/QS
Unattended Install, install runs in a quiet simple mode and shows progress through the UI, it does not accept any input but still shows error or restart messages.
When using this parameter, the installation will stop and display a prompt if there are error or restart messages. For example, if an immediate restart is required to complete the install, a restart message will be displayed to confirm the restart. Installation resumes automatically from the point of interruption after restart.
This parameter is required if /Q is not specified.
/IAcceptAllLicenseTerms
Acknowledges acceptance of the license terms.
This parameter is required for /Q or /QS parameters.
/AutoRestart
Automatically restarts the computer after the installation is complete. Used when a restart is required to complete the installation.
This parameter is optional. If this parameter is not used silent install (/Q) will return either error code 1641 or 3010 if a restart is required, and unattended install (/QS) will result in a confirmation prompt that must be agreed to before the installation is completed.
/SetupLanguage="value"
Specifies which language will be displayed during install process.
The value must be the one of the following:
  • ENU
  • CHS
  • DEU
  • ESP
  • FRA
  • ITA
  • JPN
  • KOR
  • PTB
This parameter is optional. If this parameter is not used, the default language is the current user or operating system user interface language.
/Product="value"
Specifies which sub-products will be installed.
Only required if sub-products are included with the install package.
If the software does not include sub-products this parameter is not available.
/ProductLanguage="value"
Specifies the language version of the software being installed.
The value must be one of the following:
  • ENU
  • CHS
  • DEU
  • ESP
  • FRA
  • ITA
  • PTB
This parameter is optional. If this parameter is not used, the default language is the same as the setup language.
If the software does not support multiple languages this parameter is not available.
/InstallLocation="value"
Or
/InstallDrive="value"
Specifies the install location or install drive respectively.
This parameter is optional. If this parameter is not used, the default install location is "C:\Program Files (x86)\Rockwell Software".
Some software restricts the installer to only change the drive the software is installed on. Use /? to determine which parameter is supported.
/SerialNumber="value"
Specifies the serial number of the software being installed. This is used to activate the software during installation.
This parameter is optional. If it is not specified the software must be activated manually after installation if activation is required.
Some software does not require activation. If activation is not required this parameter is not available.
/ProductKey="value"
Specifies the product key used to get activation keys during installation.
This parameter is optional. If it is not specified the software must be activated manually after installation if activation is required.
Some software does not require activation. If activation is not required this parameter is not available.
/Version="value"
Specifies the version of the software to activate which corresponds to the product version associated with the SerialNumber and ProductKey.
This parameter is optional. If it is not specified the installer will use the most recent product version available.
Some software does not require activation. If activation is not required this parameter is not available.

Examples

The following examples show how to use the installation commands.

              Setup.exe /Q /IAcceptAllLicenseTerms

              Setup.exe /QS /IAcceptAllLicenseTerms /AutoRestart /SetupLanguage=CHS /InstallDrive=D:

Error codes

The following table identifies the error codes that can be returned by an installation.

Error Code
Value
Description
ERROR_SUCCESS
0
The installation completed successfully.
ERROR_INVALID_PARAMETER
87
One of the parameters was invalid.
ERROR_INSTALL_USEREXIT
1602
The installation was cancelled by the user.
ERROR_INSTALL_FAILURE
1603
A fatal error occurred during installation.
ERROR_BAD_CONFIGURATION
1610
The configuration data for this product is corrupt. Contact your support personnel.
ERROR_SUCCESS_REBOOT_INITIATED
1641
The installer has initiated a restart. After restart installation will continue.
ERROR_SUCCESS_REBOOT_REQUIRED
3010
A restart is required to complete the installation. After restart the product is successfully installed.
ERROR_SUCCESS_RELAUNCH_REQUIRED
3011
Restart of setup needed before installation can continue.

VeriSign Universal Root Certification Authority certificate

If the VeriSign Universal Root Certification Authority certificate does not exist on the local computer, the certificate is installed while installing Rockwell Automation software. Use Microsoft Management Console (MMC) to view the certificate in Console Root > Certificates (Local Computer) > Trusted Root Certification Authorities > Certificates.

Convert an existing project to the current release

To use the most current features on projects created in previous versions of Connected Components Workbench software, convert the project to the current release by opening the project in the latest Connected Components Workbench software. This will automatically convert the project’s databases to the current release.

An existing project that is converted to the current release, opened and saved in the current release, or downloaded to a Micro800 controller cannot be opened in a previous release. If a project is shared, all users must upgrade to the current release of the Connected Components Workbench software to continue using the project.

When you open a project created in a previous release of the Connected Components Workbench software, the project database automatically updates to the current release, which allows access to the latest Connected Components Workbench features. However, to use new device specific features in the current release, you may also need to use the device's upgrade feature to upgrade the device. For example, for Micro800 use the Change Controller feature to update the controller firmware revision to the latest revision to make use of newly added instructions.

User account types for Connected Components Workbench software

When you create new projects or open existing projects, we recommend you do not use the default Guest user account, and that you use the same type of account you used when you installed the Connected Components Workbench software. That is, if you were logged in under an administrator account when you installed the Connected Components Workbench software, you should log in with an account that has administrator privileges when you use the Connected Components Workbench software.

To change to an administrator account:

  1. Navigate to: \\Program Files > Rockwell Automation > Connected Components Workbench.
  1. Right-click CCW.Shell.exe, select Run as, select Administrator user.
  2. Click OK.

File Extensions and locations

Connected Components Workbench software creates and uses the file extension .ccwsln for user-created projects.

By default, the product-managed files are saved to:

c:\Users\<user>\Documents\CCW\<Project#>\<project#>.ccswln

Connecting to a Micro800 controller on a virtual machine

If you install RSLinx Classic on a virtual machine (for example, VMware®), make sure to disable RSLinx Classic on the host computer before you plug the USB cable that is attached to your Micro800 controller into the host computer. If you ignore this step, the host computer will obtain the driver for the Micro800 controller, and the virtual machine may not be able to detect the Micro800 controller.

Connecting to a Device using Ethernet

Using the default EtherNet/IP driver to connect to a device

If you use Ethernet instead of a USB to connect to the controller, the Ethernet/IP driver is installed by default in RSLinx and you can connect to devices which are on the same subnet as the PC. If a DHCP server is available, in most cases your computer and the device (such as, Micro850 controller which defaults to DHCP) will be assigned IP addresses that will allow them to communicate using this Ethernet/IP driver. The Ethernet/IP driver will browse for all devices on the subnet.

In cases where the device is not on the same subnet as the PC or you do not wish to view all devices on the subnet, it is recommended to install the Ethernet Devices driver which requires manually entering the IP address of the device. 

To add the Ethernet Devices driver to connect to a device

Note: Be sure to select the correct port (it may not be the Windows default).

  1. Click Communications > Configure to open the Configure Drivers dialog box.
  1. In Available Driver Types, select Ethernet Devices.
  2. Click Add New, and type a name for the driver or accept the default name.
  3. If prompted, enter the Ethernet adapter selection. Be sure to select the correct port (it may not be the Windows default).
  4. For each device enter the IP address (or Host Name if DNS is supported) under Host Name. It is recommended to append ":EIP" to the IP address for better performance by avoiding the older CSPv4 port 2222. Click Add New as necessary. Click OK, then Close when finished.
  5. For the device, click Connect to open the Connection Browser.
  6. Expand the Ethernet Devices driver you previously added.
  7. Select the controller that you want to connect to from your project and then click OK.

Security considerations

Connected Components Workbench software and its included software components require running system services and network access to communicate with controllers, drives, graphic terminals, and other devices. You may need to enable system services or configure firewall rules in order for Connected Components Workbench software to function properly. However, Connected Components Workbench software does not require endpoint firewall rules because it is not a server product that allows remote clients.

For a list of services that require network access, as well as detailed information on security concerns, see Security considerations when using Rockwell Automation Software Products (Knowledgebase Answer ID 609492).

For a list of TCP/UDP ports used by Rockwell Automation products, see TCP/UDP Ports Used by Rockwell Automation Products (Knowledgebase Answer ID 898270).

View Connected Components Workbench 11.00.00 Help with Help Viewer 2.1

The Help Viewer 2.1 Filter is designed to keep the search list compact and manageable. Titles appear in the filtered table of contents (TOC) list only if they contain the root of the term used in the filter and the empty TOC levels are collapsed with an ellipsis (…).

For example, if you specify "troubleshooting" as a filter, only titles that contain "troubleshoot" or "troubleshooting" appear. Nodes whose titles do not contain the term are collapsed to a single node with an ellipsis (...).

In the filtered TOC you can do the following:

Internet Explorer security settings

Internet Explorer® high security settings can prevent some help features from working as expected.

To view Connected Components Workbench Help in Help Viewer 2.1

  1. Open Internet Explorer.
  1. On the Tools menu, click Internet Options, then click the Security tab.
  2. Select the Internet zone, then click Custom level and change the following settings:
  1. After changing the Internet Explorer security settings, open Connected Components Workbench and verify the help displays in Help Viewer 2.1.

Current Program Updater

In order for the Current Program Updater to work seamlessly, run the Current Program Updater software at least once after installation. The Current Program Updater only updates permissions on directories of applications that are being updated. Applications not related to the Current Program Updater are not affected.

To configure the Current Program Updater:

  1. If your user account is an administrator account, close Current Program Updater, and then right-click the Current Program Updater shortcut and choose Run as administrator.
  1. Run the Current Program Updater as you normally would. The Current Program Updater automatically corrects any missing permissions. The next time you run the Current Program Updater revert back to running the standard way.

VMware compatibility

Compatibility with VMware has not been formally tested, but it has been used extensively with Connected Components Workbench.

Manually connecting a virtual machine to a USB device

Downloading available firmware

The only firmware files installed with Connected Components Workbench 10.00.00 and later are the two most recent firmware versions for the Micro800 controllers. Additional firmware files (.dmk) are available for download from the Rockwell Automation Compatibility and Downloads web page.

Downloading sample code

If upgrade Connected Components Workbench from earlier version to 11.00.00, the Sample Code and Device Manuals of the earlier version should be downloaded manually. The latest Sample Code and Device Manuals are available for download from the Rockwell Automation Compatibility and Downloads web page.

Activation and grace period

If the Connected Components Workbench Developer Edition is unable to connect to the FactoryTalk Activation server, it enters a seven-day grace period.  Once the grace period expires, Connected Components Workbench will run as Standard Edition.

Installing language package

If a German or Italian Connected Components Workbench version is installed in Windows 8 or Windows Server 2012 and later with different language version, install the German or Italian Language Pack on your operating system.

Spectrum Controls module configuration tool

For the Spectrum Controls module configuration tool, it is installed to ‘C:\Program Files (x86)\Rockwell Automation\CCW\SpectrumTool\ModuleConfigConverter.exe’.  This launch path can be configured as part of the module’s profile.

Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.

Copyright © 2025 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please click here.
Trademarks not belonging to Rockwell Automation are property of their respective companies.