Release Notes

( 9324-RL0x ) RSLogix 500 supports the Allen-Bradley SLC™ 500 and MicroLogix™ families of processors.
Version 11.00.00 (released 2/2017)

Catalog Number RSLogix 500 

These release notes describe version information for RSLogix 500, version 11.00.00 (released 2/2017).

Requirements

This release has the following requirements.

RSLogix 500® works within the system requirements of all Rockwell Automation® software products.

For the latest information regarding software platform support, refer to http://www.rockwellautomation.com/compatibility/#/scenarios.

Hardware requirements

Your personal computer must meet the following hardware requirements:

Software requirements

Operating systems

RSLogix 500 runs on either the 32-bit or the 64-bit versions of the following Windows or Windows Server® operating systems:

Required software and versions

The following software is required to use RSLogix 500:

Features

This release includes the following system features.

New features

·         Introduction of new processor type MicroLogix 1400 Series B (Enhanced Password Security)

Unlike the MicroLogix 1400 Series B processor with three passwords, the MicroLogix 1400 Series B security processor contains two passwords, the Password and the Subroutine Protection Password. The password is not stored in the project, instead it will be set and authenticated to the controller directly, which helps enhance password security.

Enhanced features

·         Support for Windows 10 operating systems.

Corrected Anomalies in This Release

This release corrects the following anomalies.

·         RSLogix 500 file parser buffer overflow

When opening a specifically modified .RSS project file, RSLogix 500 may stop responding and may lead to a buffer overflow vulnerability. First identified in RSLogix 500 version 8.40.00. [362310]

In this release, RSLogix 500 can successfully open the project file and the associated risk is addressed. For more information, see Answer ID 898582 in the Rockwell Automation Knowledgebase (logon may be required).

Known Anomalies in This Release

This release has the following known anomalies.

·         Poor response time of ladder editor when connecting a project with many complex instructions

Selecting Cross Reference for an address in the ladder editor is slow when online with a SLC 5/05 processor with a project containing many complex instructions such as EEM, DEM, CEM, and MSG. First identified in RSLogix 500 version 8.10.00. [262714]

There is currently no work around for this anomaly.

·         Unable to edit a rung with an LBL instruction online in remote run mode

Online editing of a rung with an LBL instruction fails on an SLC 500 processor in remote run mode if the matching JMP instruction exists in the project and UNTEST is selected.First identified in RSLogix 500 version 5.50.00. [80585]

To resolve this problem, put the LBL instruction on its own rung.

·         Unable to verify the MicroLogix 1200 or MicroLogix 1500 project

In a MicroLogix 1200 or MicroLogix 1500 project, if a CLR instruction with an HSC:0.ACC or HSC:1.ACC operand exists in the rung with a nested branch (for example:BST XIC B3:0/0 CLR HSC:1.ACC NXB ADD 0 N12:1 N7:0 BND), the project verification will fail and a compiler error will be displayed. First identified in RSLogix 500 version 7.00.00. [82259]

There is currently no work around for this anomaly.

·         The broadcast message destination node 1 is not accepted

With a MicroLogix 1500 LRP Series C Channel 1 Radio modem, the broadcast message destination node 1 is not accepted when verifying the project. The error message invalid local DH-485 Station Number (0-254) displays even though 1 is a valid local DH-485 station number when Channel 1 is set for DF1 Radio modem and a broadcast message is requested. First identified in RSLogix 500 version 7.20.00. [77766]

There is currently no work around for this anomaly.

·         RSLogix 500 may stop responding when changing DNP3 Data Set configuration

When changing DNP3 Data Set configuration from Data Element (DAEL) to Prototype (PTYP) several times, RSLogix 500 may stop responding. First identified in RSLogix 500 version 10.00.00. [355325]

To resolve this problem, restart RSLogix 500.

·         Unable to go online with MicroLogix 1400 Series B security project with password

If an MicroLogix 1400 Series B security project's password is set using RSLogix 500 version 11, an error messages shows and cannot be closed as you try to upload and go online with the project using RSLogix 500 version 10 or earlier. First identified in RSLogix 500 version 11.00.00. [363763, 362682, 364135]

There is currently no work around for this anomaly.

·         Cannot restore the SMTP settings from EEPROM

If the MicroLogix 1400 program is saved to EEPROM memory module with status bits set to Load Memory Module Always or Load Memory Module on Memory Error, the MicroLogix 1400 Chan 1 - SMTP settings cannot be restored from the EEPROM memory module at power up after changing the SMTP settings. First identified in RSLogix 500 version 8.40.00. [272814]

There is currently no work around for this anomaly.

·         Unable to save online edits of MicroLogix 1400 Series B controllers

In rare cases, during the online editing of a MicroLogix 1400 Series B controller that is online and in Run mode, an error messages may show when saving the edits. First identified in RSLogix 500 version 8.00.00. [360390]

There is currently no work around for this anomaly.

·         Unable to go online with SLC 5/01, SLC 5/02, and MicroLogix controllers

If the project file for SLC 5/01, SLC 5/02, or MicroLogix is password protected, after going offline with the project, going online with it will fail even if the correct password is entered. First identified in RSLogix 500 version 9.05.00. [356265]

To resolve this problem, clear the CPU before accessing it again.

Application Notes

This release has the following application notes.

Installing RSLogix 500

You can only install one version or edition of RSLogix 500 within a Windows operating system.

Upgrading or downgrading RSLogix 500

You can install a newer version (version 6.3x or later) of RSLogix 500 without uninstalling the old version first. To install an older version of RSLogix 500 over a newer version, you must first uninstall the newer version by using Add/Remove Programs in the Windows Control Panel.

Need Administrator privilege to execute certain tasks

If User Account Control (UAC) is enabled, you may be prompted to confirm your Administrator privileges when executing certain tasks (like import/export). To execute these tasks, make sure you have Administrative privileges. If not, contact your System Administrator.

Unable to import the database or process the native Import A.I. Database file when opening an .ACH file

When opening an .ACH file with Database or native Import A.I. Database file functions, you must open the file as an Administrator. Otherwise, the database in the .ACH file cannot be imported or the native Import A.I. Database file process will fail.

Errors occur when performing online saves with the Excel database editor opened

If the Excel database editor (Pro only) opens, performing online saves causes errors in the .RSS file. Make sure the Excel database editor is closed before performing online saves.

Download to processors with DDE communications may fail

If you are using RSLinx to perform DDE communications with a processor and you download a project to the same processor, the download may fail. If this occurs, the processor loads its default program. To avoid this situation, cease DDE communications to your target processor when you plan to download a project to the same processor.

Online and offline images of the project file (projectname.RSS) are not synchronized

The project file (projectname.RSS) contains both an online and offline image of your project. This speeds the process of connecting to a processor. These images can become unsynchronized; this occurs if you do not save your changes when going from online to offline. To synchronize the images, you must download, upload, or save the project while online.

Make the database file available when sharing the database information of the project file (projectname.RSS)

The project file (projectname.RSS) contains all database- and project-related files. If you need to share a project with someone, provide them with the projectname.RSS file and they will receive all project-related information. When sharing RSLogix™ database information with other Rockwell Automation Software programs, like RSView®32, you must use the Save database as external file check box on the File>Save As dialog box to make the database file available to that program.

Unable to print ladder report as a text file

RSLogix 500 prints ladder logic reports as graphic files. The ladder report cannot be printed as a text file. Other RSLogix 500 reports can be printed as a text file using the Windows text-only printer driver.

The Floating Point constant is not supported in an SCP instruction

RSLogix 500 does not allow the use of a Floating Point constant in an SCP instruction.

Compatibility issues occur when using an older version of RSLogix 500 with the MicroLogix 1100 Series B controller

To support the MicroLogix 1100 Series B controller, RSLogix 500 handles PTO and PWM frequencies (PTO.OF, PTO.OFS, PTO.JF, PWM.OF, and PWM.OFS) as unsigned 16-bit integers (0 - 65535) for MicroLogix 1100 Series B. If you are using an older version of RSLogix 500 (version 7.0 and version 7.10) with the MicroLogix 1100 Series B controller, there will be compatibility issues. These include:

To avoid this problem, copy PTO/PWM frequencies to long integer before manipulation. For greater detail refer to Appendix F: How to use 40kHz PTO/PWM of MicroLogix 1100 Series B Controller, publication 1763-RM001.

Unable to update the Trend applet description once the address description in a data file is changed

If the address description in a data file is changed, the description in the Trend applet cannot be updated.

Certain symbol characters cannot be used

The following characters cannot be used in RSLogix 500 symbols, `~!@#$%^&*()-+={}[]|\\:;""'<>?,./ . If you have used these characters in a previous release of RSLogix 500, the symbols will appear in your ladder views and reports; however, you cannot modify the symbol.

We recommend that you export the database to the ASCII CSV format to help locate illegal symbol characters.

Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.

Copyright © 2026 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please click here.
Trademarks not belonging to Rockwell Automation are property of their respective companies.