Release Notes

PlantPAx Process Library with Application Templates, Application Code Manager Library, Tools & Utilities, and Integration with E
Version 3.50.05 (released 1/2017)

Catalog Number Process Library 

These release notes describe version information for Process Library, version 3.50.05 (released 1/2017).

Features

This release includes the following system features.

Logix CPU Utilization for Logix Version 24 and Later  (L_CPU_24_up)

Feature First Identified as of PlantPAx Process Library Version 3.50.05

The L_CPU_24 (Logix CPU Utilization for Version 24 of Logix) instruction is replaced with a new Add-On Instruction for Version 24 and Later: L_CPU_24_up.  This instruction works with Version 24 and Later (24, 26, 27, 28, 29 and 30) major firmware versions of the CompactLogix 5370 and ControlLogix 5570 controllers:
IMPORTANT: This instruction cannot get CPU utilization and other information from the following controllers:
To install this instruction in place of L_CPU_24 in existing version 24 applications, perform the following steps:
  1. Open the existing application in Studio 5000 Logix Designer.
  2. Navigate to the existing L_CPU_24 instance in the application code. (A convenient way to do this is to find the L_CPU_24 Add-On Instruction in the Controller Organizer, then right-click and select “Cross Reference”. In the Cross Reference dialog, double-click on the instance to go to that rung.)
  3. Select the existing L_CPU_24 rung, then right-click and select “Import Rung(s)”.

graphic

  1. Select the  L_CPU_24_up_3_5-05_RUNG.L5X  file from the Library download in folder
  2. …\Files\Logix Diagnostic Objects Library\Logix Add-On Instructions.
  3. In the Import Configuration window, note the red flag next to the “Tags” item in the tree. Select this item.  In the first tag (L_CPU), change the Operation from “Use Existing” to “Overwrite”.  Click OK to begin the import.

graphic

  1. The rung will be inserted AFTER the existing L_CPU_24 rung, and that rung will have error marks (because the type of the L_CPU backing tag changed). Note (or select and copy) the existing MOV and GSV (or CLR) instructions on the upper branch.

graphic

  1. Delete the old L_CPU_24 rung. In the new L_CPU_24_up rung, modify the upper branch (paste if you copied) to restore the configuration of the Slot Number and Continuous Task Instance.

graphic

  1. Delete the (now unused) L_CPU_24 Add-On Instruction definition from the project.
  2. Verify and save the project and download to the controller.Only the Add-On Instruction definition and the backing tag type are changed. The HMI components and the other associated User-Defined Types (UDTs) and Tags are unchanged.
Alarm Builder Features (Version 5.5.5 of the Alarm Builder)

Feature First Identified as of PlantPAx Process Library Version 3.50.05

Updated ME Alarms XML Import File Builder Tool
Previous versions provided two methods for building the ME alarms XML import file:  a Quick Build that uses all Logix tags to build ME tags, and a “Long Method” where the user selects the Logix tags to use.
The new version provides a single user interface for building the ME alarms XML import file. Options are provided to use only tags from the Process Tree folders or to use all controller tags. This single user interface is consistent with the AE alarm builder interface.

graphic


New ME Alarms XML File Builder Options
New options are provided to exclude alias tags and Input/Output program parameter tags when building the ME XML file. These options are useful if alias tags are aliased to base tags with the same data type – this prevents building multiple ME tags with the same alarm triggers.
If the “Include Array Tag Elements” option is not selected, and alias tags are aliased to array tag elements, then these new exclude options should not be used. These options should also not be used if the alias tags are aliased to UDT elements and alarm definitions are not configured for the UDT.Note InOut program parameters tags are now always excluded from the export.

graphic

New options are provided for building the ME alarm messages:

graphic

Process Library Migration Tool Features (Version 1.3 of the Migration Tool)

Feature First Identified as of PlantPAx Process Library Version 3.50.05

Execution Time Reduction
Coding changes made to reduce execution time for updating ACD files. The amount of time reduction depends on the number of AOIs, IREFs and tag data changes. For some test files, conversion time is reduced by about 40% compared to the last version.

Migration Tool Options
The ACD file migration tool uses Logix Services to import AOIs and other file changes. Logix Services locks up when the importing AOIs for ACD files containing IREFs that are linked to AOI tag parameters aliased to AOI local tags. So far, this problem has only been found when converting Process Library AOIs version 3.0 and older.  As a workaround, the migration tool can check for these types of IREFs and replace them with blank references before using Logix Services to import the new AOIs.  After the AOIs are imported to the ACD file, the IREFs are restored with their original references and the ACD file updated again using Logix Services. For this version, options are added to allow the user to select when to run the workaround method. In the previous version, the workaround was hidden and always executed regardless of library version.

Startup Window Enhancements
New description added to the startup window to make clear which process library versions are supported:

graphic


PowerFlex 6000 Medium Voltage Drive Support

Feature First Identified as of PlantPAx Process Library Version 3.50.05

A new Add-On Instruction, P_PF6000, and corresponding Faceplate were added to support the PowerFlex 6000 Medium Voltage Variable Frequency Drive. Communication is via an Anybus AB7007 EtherNet/IP - Modbus Serial gateway. The AB7007 profile is supported in Logix version 20 and later software / firmware. The AOI and RUNG import files are provided in Logix version20 format and work with version 20 or later. Operation and setup are similar to the other PowerFlex drive Add-On Instructions, except that no drive datalink setup is required (or available).

The P_PF6000 instruction is supported by the updated Process Library Online Configuration Tool spreadsheet.
Along with addition of the new P_PF6000 Add-On Instruction, the following HMI displays and global objects were added or modified:
Because the 20-COMM-E (or similar) drive DPI communication adapter is not used, the drive does not support using MSG instructions to read and write parameter values. All data needed for this Add-On Instruction are contained in the Input and Output assemblies and no MSG instructions are needed. The I/O assemblies do provide an interface to read and write drive parameters from the controller, but this parameter read/write capability is NOT part of the P_PF6000 Add-On Instruction.

Known Anomalies from Previous Releases

These anomalies are from previous releases but are still known in this release.

Corrected Anomaly with PlantPAx Process Library version 4.00.02

P_ValveSO Handling of Simultaneous Commands

Known Anomaly First Identified as of PlantPAx® Process Library version 1.00.00

When P_ValveSO receives simultaneous Open and Close commands, it alternates between closing and opening, with the output toggling.

How Corrected: Logic was modified so that in the event of simultaneous commands, the command for the de-energized (fail) state is the one accepted.

Corrected Anomaly with PlantPAx Process Library version 4.00.02

Read from Online Configuration Spreadsheet

Known Anomaly First Identified as of PlantPAx® Process Library version 3.00.00

Attempt to read configuration data from a controller fails with the following error message:

graphic

Click OK for the following message:

graphic

By clicking OK, subsequent messages appear about location of cells which failed to read and overall failure of the function.

However, the ‘Send To CLX’ function works properly, and once you do a successful ‘Send To CLX’, then the ‘Read From CLX’ function begins to work properly.

This only affects the Premier Integration Online Configuration Tool spreadsheet. The Process Library Online Configuration Tool spreadsheet works correctly.

The spreadsheet’s Visual Basic for Applications (VBA) code associated with the Read From CLX function was corrected to remove an improper VAR initialization.

Functional Changes

This release has the following functional changes from the previous release.

Lead/Lag/Standby Rank Value

Functional Change First Identified as of PlantPAx Process Library Version 3.50.05

The Lead / Lag / Standby Motor Group Add-On Instruction was modified to generate an additional value, “Val_Rank”, which was added to the P_LLS_Motor User-Defined Type.

graphic

Logic was added to P_LLS so that each motor will now have its rank within the sorted motor list made available for use in application logic. A value of 1 is given to the motor assigned as Lead, a value of 2 to the first Lag, and so on, through the number of motors in the group.
Notice that this Value is provided in the “Ref_Motors” array and not as a parameter on the Add-On Instruction itself, and the array index is “zero-based”. So the rank of Motor 1 in the P_LLS instance named “MyP_LLS” would be found at the address “MyP_LLS_Motors[0].Val_Rank”  (using the required naming convention for the motor interface array tag).
Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.

Copyright © 2025 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please click here.
Trademarks not belonging to Rockwell Automation are property of their respective companies.