Release Notes

FactoryTalk View Site Edition is HMI software for monitoring and controlling applications of any size, from single computer, single user station applications to distributed server-client, multiple user applications. FACTORYTALK VIEW SE SHOULD BE DOWNLOADED USING A SERVER OR STATION SERIAL NUMBER; CLIENT SERIAL NUMBERS MAY NOT PROVIDE ACCESS TO ALL VERSIONS.
Version 9.00.00 (released 12/2016)

Catalog Number FactoryTalk View Site Edition 

These release notes describe version information for FactoryTalk View Site Edition, version 9.00.00 (released 12/2016).

Requirements

This release has the following requirements.

The following are the system requirements for FactoryTalk View SE version 9.00.00 (CPR 9 SR 9).

Hardware requirements

Operator workstations

For computers hosting FactoryTalk View SE Clients in a network application, or for a FactoryTalk View SE Client running a local station application:

Engineering workstations

For computers hosting FactoryTalk View Studio in a network application:

Application servers

For computers hosting FactoryTalk View SE HMI Server, FactoryTalk Alarms and Events Tag Server, or RSLinx Enterprise in a network application:

Software requirements

Operating systems

FactoryTalk View SE is tested on operating systems installed from original Microsoft media only. FactoryTalk View SE runs on either the 32-bit or 64-bit versions of the following Windows operating systems:

* For more information about the Windows 10 operating system support, see the Operating systems section of Anomalies.
** This operating system is supported with the Allen-Bradley® 61xx family of industrial computers and CompactLogix™ 5480 family of controllers.
^ For more information about the Windows 7 Embedded Standard operating system support, see Answer ID 619825 in the Rockwell Automation Knowledgebase.

Domain controller requirements

The following operating systems are supported for use as domain controllers for FactoryTalk View SE client computers. Using a domain is recommended for applications that include more than 10 computers. If your application includes 10 or fewer computers, they can be organized in a workgroup.

  

Features

This release includes the following system features.

FactoryTalk View SE version 9.00.00 has the following new and enhanced features.

New features

Enhanced features

  

Corrected Anomalies in This Release

This release corrects the following anomalies.

The following list identifies the anomalies corrected in FactoryTalk View SE version 9.00.00.

Known Anomalies in This Release

This release has the following known anomalies.

The following list identifies the known anomalies or limitations of FactoryTalk View SE version 9.00.00 at the time of the release.

Display client

Distributed Application Manager tool

Find and Replace

Graphic displays

Graphic objects

HMI server

Installation

Operating systems

ODBC databases

Software components

Trend objects

Trend Pro objects

  

Functional Changes

This release has the following functional changes from the previous release.

FactoryTalk View SE version 9.00.00 has the following changes in functionality since the last release.

Unattended installation syntax

The command line syntax of unattended installation has been changed to match the FactoryTalk View installation changes.

For more information, see Appendix E, "Use unattended installation" in FactoryTalk View Site Edition Installation Guide.

Adobe Acrobat Reader

The Adobe® Acrobat® Reader® is removed from FactoryTalk View installation media and will need to be installed manually from the Adobe website https://get.adobe.com/reader/ .

SQL Server installation

During the installation of FactoryTalk View, if the installer detects that there is not a compatible SQL Server available on the computer, the installer installs SQL Server 2008 R2 Express Service Pack 2 (32-bit) with a mixed authentication to store HMI tag data and adds the current Windows user to the SQL Administrators group.

Legacy Tag Database Conversion tool

To use the tool, you must run it as an administrator.

FTVIEWUSER Account Reset tool

To change or reset the password, the current Windows logged on user must be granted the sysadmin server role in SQL Server. For assistance, contact your administrators.

FactoryTalk View SE Custom Website Setup tool

FactoryTalk View SE Secure Web Site Setup tool has been renamed to FactoryTalk View SE Custom Website Setup tool.

Application Notes

This release has the following application notes.

The following are the application notes for FactoryTalk View SE version 9.00.00.

Considerations for application server host computers

In a network application, it is possible for a single server computer that meets the recommended requirements to host all of the following components:

If a network application requires multiple HMI servers, data servers, or alarm servers, to distribute the load, it is recommended that you install the necessary software and run the servers on multiple host computers.

Running more than one HMI server on a single computer is not recommended. If you plan to deploy a network application that uses more than two servers (or two pairs of redundant servers) and 20 clients, it is recommended that you contact your local Rockwell Automation Sales office for architectural assistance. For information about setting up redundant FactoryTalk View SE Servers, see Chapter 14, Setting up FactoryTalk system availability of the FactoryTalk View Site Edition User’s Guide.

Find and Replace

If an HMI server at the root node of an SE Network distributed application has the same name as the application itself, the Find and Replace feature search results might include the application name even though you performed the search at the HMI server level.

FactoryTalk Diagnostics

FactoryTalk Diagnostics cannot log to a remote database using Microsoft Access. You can only log to a local database using Microsoft Access.

HMI project folder does not replicate to secondary HMI Server

This issue can be caused by a couple of situations. One cause could be the size of the HMI project file being larger than the maximum allowable file transfer size. The other cause could be the replication taking longer than the default time limit of 20 minutes.

For complete details about this topic, see Answer ID 38407  in the Rockwell Automation Knowledgebase.

Pre-installation configuration

Before you install FactoryTalk View SE, there are a number of steps required to set up the installation environment. This will help ensure that the installation proceeds smoothly and that your new or upgraded FactoryTalk system operates as expected. For detailed information about pre-requisites before installation, see Chapter 3, Pre-installation configuration of FactoryTalk View Site Edition Installation Guide.

For information on the security considerations when using Rockwell Automation products, including:

Tag Browser

If you rename an HMI server while you are deploying an application, you may need to restart the computer in order to have the HMI tags show up in the Tag Browser.

Tools and utilities

Trend objects

The Trend objects cannot get the oldest data from FactoryTalk Historian server when you click the Oldest Data button.

Trend Pro objects

UAC support

Turning off User Account Control (UAC) is not recommended.

This action
Prompts for authentication or confirmation before running this program
Configuring Internet Information Services (IIS)
RSViewWebManager.exe
CustomWebSite.exe
Updating Samples application directory information
RefreshSampleApplication.exe
Uninstall program
UninstallAllRSI.exe
Shutdown system
RSViewReboot.exe
Terminate processes
VSClean.exe
Configuring ODBC
RSAlarmLogEd.exe
Reset FTView user account
FTViewSQLAccountReset.exe
Legacy Tag Database Conversion
LegacyTagDBConvertTool.exe

Unattended or silent install

Use command-line parameters to perform an unattended or silent installation of the software.

Command-line parameters

The following table identifies the installation command-line parameters. Command-line parameters are case-insensitive. However, if a specified value includes a space, be sure to enclose the value in quotation marks (for example, "value with spaces").

Parameter

Description

/?

Displays the usage options for installation parameters.

/Q

Silent Install, install runs in a quiet mode without any user interface.

This parameter is recommended if you are deploying the software installation using an IT tool or script, and don’t expect to see any error or restart messages. When using this parameter, your IT tool or script should check the error codes, and respond as needed. For example, if the installation returns error code 1641, then the IT too or script should restart the computer and relaunch the installation after restart.

This parameter is required if /QS is not specified.

/QS

Unattended Install, install runs in a quiet simple mode and shows progress through the UI, it does not accept any input but still shows error or restart messages.

When using this parameter, you will not have to check the error codes, and the installation will stop and display a prompt if there are error or restart messages. For example, if an immediate restart is required to complete the install, a restart message will be displayed for you to confirm the restart. Installation resumes automatically from the point of interruption after restart.

This parameter is required if /Q is not specified.

/IAcceptAllLicenseTerms

Acknowledges acceptance of the license terms.

This parameter is required for /Q or /QS parameters.

/AutoRestart

Automatically restarts the computer after the installation is complete. Used when a restart is required to complete the installation.

This parameter is optional. If this parameter is not used silent install (/Q) will return either error code 1641 or 3010 if a restart is required, and unattended install (/QS) will result in a confirmation prompt that must be agreed to before the installation is completed.

/SetupLanguage="value"

Specifies which language will be displayed during install process.

The value must be the one of the following:

  • ENU
  • CHS
  • DEU
  • ESP
  • FRA
  • ITA
  • JPN
  • KOR
  • PTB

This parameter is optional. If this parameter is not used, the default language is the current user or operating system user interface language.

/Product="value"

Specifies which sub-products will be installed.

Only required if sub-products are included with the install package.

If the software does not include sub-products this parameter is not available.

/ProductLanguage="value"

Specifies the language version of the software being installed.

The value must be the one of the following:

  • ENU
  • CHS
  • DEU
  • ESP
  • FRA
  • ITA
  • JPN
  • KOR
  • PTB

This parameter is optional. If this parameter is not used, the default language is the same as the setup language.

If the software does not support multiple languages this parameter is not available.

/InstallLocation="value"

Or

/InstallDrive="value"

Specifies the install location or install drive respectively.

This parameter is optional. If this parameter is not used, the default install location is "C:\Program Files (x86)\Rockwell Software".

Some software restricts the installer to only change the drive the software is installed on. Use /? to determine which parameter is supported.

/SerialNumber="value"

Specifies the serial number of the software being installed. This is used to activate the software during installation.

This parameter is optional. If it is not specified the software must be activated manually after installation if activation is required.

Some software does not require activation. If activation is not required this parameter is not available.

/ProductKey="value"

Specifies the product key used to get activation keys during installation.

This parameter is optional. If it is not specified the software must be activated manually after installation if activation is required.

Some software does not require activation. If activation is not required this parameter is not available.

/Version="value"

Specifies the version of the software to activate which corresponds to the product version associated with the SerialNumber and ProductKey.

This parameter is optional. If it is not specified the installer will use the most recent product version available.

Some software does not require activation. If activation is not required this parameter is not available.

Examples

The following examples show how to use the installation commands.

  • To install the software with no user interface using the default settings during the installation process. (Unattended install)

    Setup.exe /Q /IAcceptAllLicenseTerms

  • To install the Chinese language version of the software on the D: drive and display the progress, error, or complete messages during installation and restart the computer if necessary. (Silent install)

    Setup.exe /QS /IAcceptAllLicenseTerms /AutoRestart /SetupLanguage=CHS /InstallDrive=D:

Error codes

The following table identifies the error codes that can be returned by an installation.

Error Code

Value

Description

ERROR_SUCCESS

0

The installation completed successfully.

ERROR_INVALID_PARAMETER

87

One of the parameters was invalid.

ERROR_INSTALL_USEREXIT

1602

The installation was cancelled by the user.

ERROR_INSTALL_FAILURE

1603

A fatal error occurred during installation.

ERROR_BAD_CONFIGURATION

1610

The configuration data for this product is corrupt. Contact your support personnel.

ERROR_SUCCESS_REBOOT_INITIATED

1641

The installer has initiated a restart. After restart installation will continue.

ERROR_SUCCESS_REBOOT_REQUIRED

3010

A restart is required to complete the installation. After restart the product is successfully installed.

ERROR_SUCCESS_RELAUNCH_REQUIRED

3011

Restart of setup needed before installation can continue.


Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.

Copyright © 2026 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please click here.
Trademarks not belonging to Rockwell Automation are property of their respective companies.