Release Notes
Flex XT 8 Point Analog Input Module
Version A.02 (released 8/2021)
Catalog Number 1794-IF8IHNFXT (series A)
These release notes describe version information for 1794-IF8IHNFXT, version A.02 (released 8/2021).
Corrected Anomalies in This Release
This release corrects the following anomalies.
Periodic clearing of diagnostic status tag
Corrected Anomaly with Firmware Revision A.02
Known Anomaly First Identified as of Firmware Revision A.01
Catalog Numbers:
The module periodically clears the “Diagnostic Status” tag, which causes the module to
toggle between “0” and a diagnostic code that the module previously reported. This
anomaly occurs when you set the “HART OFF” bit of any channel in the output table,
and you continue to use the module without clearing the previous diagnostic condition.
Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.
Copyright © 2026 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please
click here.Trademarks not belonging to Rockwell Automation are property of their respective companies.