Release Notes

FLEX I/O ControlNet Adapter
Version C (released 3/2020)

Catalog Number 1794-APBDPV1 (series C)

These release notes describe version information for 1794-APBDPV1, version C (released 3/2020).

Requirements

This release has the following requirements.

Software Compatibility

Software Compatibility First Identified as of FLEX™ I/O PROFIBUS communications adapter, Series C


Catalog Numbers:                                  

•1794-APBDPV1


You must use RSLogix 5000® or Studio 5000 Logix Designer® application, version 20.00.00 or later, to configure the FLEX™ I/O PROFIBUS communications adapter.

  

Corrected Anomalies in This Release

This release corrects the following anomalies.

Output values go to NULL for up to 100 ms on reinsertion of PROFIBUS cable

Corrected: FLEX™ I/O PROFIBUS communications adapter, Series C


If the PROFIBUS cable is removed and reinserted, the outputs turn off briefly while the network connection re-establishes.



Slot fault status bit of input module gets set intermittently

Corrected: FLEX™ I/O PROFIBUS communications adapter, Series C


<Adapter>.I.SlotStatusBits.<Slot number of module> is set intermittently, for input modules.



Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.

Copyright © 2026 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please click here.
Trademarks not belonging to Rockwell Automation are property of their respective companies.